SteepContainment Class¶
-
class
NXOpen.CAM.
SteepContainment
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.SteepContainment
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle |
Tag | Returns the Tag for this object. |
Type | Returns or sets the steep containment type |
Methods¶
Enumerations¶
SteepContainmentTypes Enumeration | Available types for steep containment |
Property Detail¶
Angle¶
-
SteepContainment.
Angle
¶ Returns the angle
-------------------------------------
Getter Method
Signature
Angle
Returns: the valley steep angle builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
Type¶
-
SteepContainment.
Type
¶ Returns or sets the steep containment type
-------------------------------------
Getter Method
Signature
Type
Returns: the steep angle usage Return type: NXOpen.CAM.SteepContainmentTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: steepAngleUsage ( NXOpen.CAM.SteepContainmentTypes
) – the steep angle usageNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)