Interface | Description |
---|---|
AutoPoint |
This class will automatically create weld points from selected components
To create or edit an instance of this class, use AutoPointBuilder Created in NX6.0.0 |
AutoPointBuilder |
Represents a
AutoPointBuilder builder To create a new instance of this class, use WeldManager.createAutoPointBuilder(nxopen.features.Feature) Default values. |
AutoWeldSymbolsBuilder |
Represents a
AutoWeldSymbolsBuilder builder To create a new instance of this class, use WeldManager.createAutoWeldSymbolsBuilder() Created in NX8.0.0 |
CharacteristicsBuilder |
This builder allows you to define the attribute values to be set on the
output of the weld feature.
|
CharacteristicsSelectionBuilder |
This builder allows you to define the attribute values to be set on the
output of the weld feature.
|
CharacteristicsValueBuilder |
The object containing the information about the attribute to be
placed on the output of the weld feature.
|
CompoundWeld |
Represents a compound weld feature.
|
CompoundWeldBuilder |
Represents a
CompoundWeld builder. |
ConnectedFaceFinderBuilder |
Represents a builder to run the Connected Face Finder operation.
|
ConnectedPart |
Represents weld connected part to customize the retrieval of connected part information.
|
ConnectionFinderBuilder |
Represents a builder to display, manage, delete, and allow the user to
reparent face information for the weld objects.
|
CustomManager |
Represents weld interface to customize the creation of welding joint features.
|
CustomManager.DatumIconHandler |
Method called from the part navigator to define the datum surface and pin icon.
|
CustomManager.ModifyFeatureHandler |
User defined method that is called whenever a welding joints are created or edited
|
CustomManager.PipeJointSetType |
User defined method that is called whenever a welding joint is created.
|
CustomManager.PointExitHandler |
User defined method that is called whenever a welding features are created through Weld Point command.
|
CustomManager.VariableBevelHandler |
User defined method that returns the angle divisions for a variable bevel.
|
CustomManager.WeldJointHandler |
User defined method that is called whenever a welding joint is created or updated
|
DatumCommonBuilder |
Used to create or edit a
DatumSurface or DatumPin feature. |
DatumIconBuilder |
Represents a
DatumIconBuilder class used to control the part navigator icon for Datum Pin and Surface Locators. |
DatumPin |
Represents a Weld Datum Pin feature
To create or edit an instance of this class, use DatumPinBuilder Created in NX8.5.0 |
DatumPinBuilder |
Used to create or edit a
DatumPin feature. |
DatumSurface |
Represents a Weld Datum Surface feature
To create or edit an instance of this class, use DatumSurfaceBuilder Created in NX8.5.0 |
DatumSurfaceBuilder |
Used to create or edit a
DatumSurface feature. |
EasyPatternBuilder |
Represents the easy pattern builder.
|
EdgePrep |
Represents a Weld Edge Prep feature
To create or edit an instance of this class, use EdgePrepBuilder Created in NX8.0.0 |
EdgePrepBuilder |
A builder used to create or edit a
EdgePrep feature. |
EdgePrepValuesBuilder |
Used to view or edit the values used to define the welding joint and edge preparation.
|
ExportWeldBuilder |
Represents a ExportWeldBuilder class
To create a new instance of this class, use WeldManager.createExportWeldBuilder() Default values. |
ExportWeldJointBuilder |
Represents exporting weld joints.
|
Extract |
Represents a Linked Feature created in the Weld Assistant.
|
Fill |
Represents a Weld Fill feature
To create or edit an instance of this class, use WeldFillBuilder Created in NX7.5.0 |
Fillet |
Represents a Weld Fillet Feature.
|
FilletBuilder |
Represents a
Fillet builder. |
Groove |
Represents a WeldGroove feature.
|
GrooveBuilder |
Represents a Groove Weld feature
To create a new instance of this class, use WeldManager.createWeldGrooveBuilder(nxopen.features.Feature) Created in NX5.0.0 |
IFeature |
Represents a Weld Assistant or Structure Welding created feature .
|
InformationBuilder |
This class is used by "Fabrication Information" to output fabrication objects information.
|
JointExitBuilder |
Used to set custom edge preparation parameters of a
WeldJoint feaure. |
JointItemBuilder |
Used to create or edit a
Weld.WeldJoint feature. |
JointItemBuilderList |
Represents a list of objects.
|
Jointmark |
Represents a Weld Jointmark Feature.
|
JointmarkBuilder |
Represents a
Jointmark builder To create a new instance of this class, use WeldManager.createJointmarkBuilder(nxopen.weld.Jointmark) Default values. |
JointmarkElement |
Represents a Weld.JointmarkElement Feature.
|
JointmarkFaceSetsBuilder |
Used to create or edit a set of faces for Jointmark
To create a new instance of this class, use JointmarkBuilder.newFaceSets() Created in NX9.0.0 |
JointmarkFaceSetsBuilderList |
Represents a list of objects.
|
JointmarkGuideBuilder |
Used to create or edit a guide curve for Jointmark.
|
JointmarkGuideBuilderList |
Represents a list of objects.
|
JointmarkPointsBuilder |
Used to create or edit a point in the list of points for Jointmark
To create a new instance of this class, use JointmarkBuilder.newPoints() Created in NX9.0.0 |
JointmarkPointsBuilderList |
Represents a list of objects.
|
LocatorReferenceBuilder |
This class is used by "Locator Reference" to add the additional component for a weld datum DF.
|
PlugSlot |
create a PlugSlot feature for Weld
To create or edit an instance of this class, use PlugSlotBuilder Created in NX8.0.0 |
PlugSlotBuilder |
Represents a
PlugSlot builder To create a new instance of this class, use WeldManager.createPlugSlotBuilder(nxopen.features.Feature) Default values. |
PointMark |
Represents a Weld PointMark Feature.
|
PointMarkBuilder |
Used to create or edit a
PointMark feature. |
PointMarkPoint |
Represents a Weld.PointMarkPoint Feature.
|
PointMarkPointBuilder |
Used to create or edit a point in the list of points for Jointmark
To create a new instance of this class, use PointMarkBuilder.newPointsOverride() Created in NX10.0.0 |
SelectDatumPin |
Represents a single object selection.
|
SelectDatumSurface |
Represents a single object selection.
|
StructureWeldBuilder |
This class is used to create or edit the information shared among all Structure Weld builders.
|
SurfaceWeld |
Represents a surface weld feature
To create or edit an instance of this class, use SurfaceWeldBuilder Created in NX9.0.0 |
SurfaceWeldBuilder |
Use to create or edit a
SurfaceWeld feature. |
UserDefinedWeld |
Represents a User Defined Weld feature.
|
UserDefinedWeldBuilder |
Represents a
UserDefinedWeldBuilder builder. |
WeldAdvisorBuilder |
Represents a weld advisor test
To create a new instance of this class, use WeldManager.createWeldAdvisorBuilder() Created in NX7.5.0 |
WeldBead |
Represents a Weld Bead feature
To create or edit an instance of this class, use WeldBeadBuilder Created in NX7.5.0 |
WeldBeadBuilder |
Used to create or edit a
WeldBead feature. |
WeldBeadPathBuilder |
Represents the path the bead shape will be swept along.
|
WeldBeadPathBuilderList |
Represents a list of objects.
|
WeldBeadSizeBuilder |
This builder is used to define the bead shape.
|
WeldBeadSizeBuilderList |
Represents a list of objects.
|
WeldCpdUtils |
Provides methods for access a WeldCpdUtils class object in NX.
|
WeldFillBuilder |
A builder used to create or edit a
Fill feature. |
WeldFillStripBuilder |
A builder used to create or edit a single strip of the
WeldFillBuilder . |
WeldFillStripBuilderList |
Represents a list of objects.
|
WeldGroove |
Represents a Weld Groove Feature
To create or edit an instance of this class, use WeldGrooveBuilder Created in NX9.0.0 |
WeldGrooveBuilder |
Represents a
WeldGroove builder To create a new instance of this class, use WeldManager.createWeldGroove1Builder(nxopen.features.Feature) Default values. |
WeldImportBuilder |
Creates Weld features by reading a csv file
To create a new instance of this class, use WeldManager.createImportBuilder() Created in NX7.5.1 |
WeldJoint |
Represents a weld joint feature
To create or edit an instance of this class, use WeldJointBuilder Created in NX8.0.0 |
WeldJointBuilder |
Used to create or edit a
WeldJoint feature. |
WeldLabelBuilder |
Create weld labels for multiple welds and BIW locators, this builder's Commit can produce more than one object,
the GetCommittedObjects can be used to get the objects and the order of GetCommittedObject's output array is stable.
|
WeldManager |
Manages weld features and assistant tools.
|
WeldObjectBuilder |
Represents a
WeldObjectBuilder class used to collect welding objects created or edited from a command. |
WeldPmiBuilder |
Create PMI symbols for multiple structure welds, this builder's Commit can produce more than one object,
the GetCommittedObjects can be used to get the objects and the order of GetCommittedObject's output array is stable.
|
WeldPoint |
Represents a WeldPoint feature.
|
WeldPointBuilder |
Represents a Spot Weld feature
To create a new instance of this class, use WeldManager.createWeldPointBuilder(nxopen.features.Feature) Default values. |
WeldPointExitBuilder |
Represents a
WeldPointExitBuilder class used to pass welding object from the Weld Point command to a user callback. |
WeldPreferenceBuilder |
Represents a
WeldPreferenceBuilder builder To create a new instance of this class, use WeldManager.createPreferenceBuilder() Default values. |
Class | Description |
---|---|
AutoPointBuilder.InterferenceDetails |
Settings to indicate whether an interference is near an existing weld point.
|
AutoPointBuilder.Types |
Settings to indicate whether new features should be created, or if features will be reused.
|
CharacteristicsBuilder.Type |
The custom type of the datum specified for creation.
|
CharacteristicsValueBuilder.Type |
Settings to indicate the type of value contained in the attribute.
|
ConnectionFinderBuilder.FilterTypes |
Filter values to control "Save All" processing.
|
DatumCommonBuilder.ControlMethodTypes |
Settings for the method used to define the control direction.
|
DatumCommonBuilder.CreationDirectionMethods |
Settings to define the creation direction.
|
DatumCommonBuilder.CustomTypes |
The custom type of the datum specified for creation.
|
DatumCommonBuilder.SolidTypes |
Settings for defining the solid type to create for the datum object.
|
DatumSurfaceBuilder.Types |
Settings to indicate the construction type used for the datum surface.
|
EasyPatternBuilder.HemMethodTypes |
Indicates the method to use to compute the hem vector location.
|
EasyPatternBuilder.PlaneMethodTypes |
The plane to cut sections in to determine placement measurement patterns.
|
EasyPatternBuilder.SpacingMethodTypes |
Indicates whether planes should be cut a grid lines, or if a single plane should be used.
|
EasyPatternBuilder.Types |
Controls the type of pattern.
|
EdgePrepValuesBuilder.Apply |
Option to indicate how the values are to be updated.
|
EdgePrepValuesBuilder.Option |
Option to indicate how the values are to be used.
|
ExportWeldBuilder.AttributeOriginType |
the Attribute Origin enum
|
ExportWeldBuilder.OutputType |
the Output Type enum
|
FilletBuilder.EnumConstructionMethod |
the options for which construction method to use.
|
FilletBuilder.EnumContour |
the Contour enum.
|
FilletBuilder.EnumExtendEdges |
the options for populating the edge selections.
|
FilletBuilder.EnumExtensionMethod |
the Extension enum.
|
FilletBuilder.EnumSkipWeldMethod |
the Skipweld enum.
|
FilletBuilder.EnumWeldingType |
the WeldingType enum.
|
InformationBuilder.AttributeOriginType |
the Object Type enum
|
JointExitBuilder.BodySide |
Settings to indicate the side the positions should be applied to.
|
JointExitBuilder.EdgePrepValuesData |
This class holds the data returned from
JointExitBuilder.getEdgePrepValues(nxopen.weld.JointExitBuilder.Positions) |
JointExitBuilder.FilletSizes |
The structure for defining fillet weld lengths.
|
JointExitBuilder.Positions |
Settings to indicate the desired position of edge preporation thickness and angle.
|
JointmarkBuilder.ConnectedPanelTypes |
The type of sheets to create
|
JointmarkBuilder.Method |
The type of construction method for creating Jointmark
|
JointmarkBuilder.OrientationMethodTypes |
The type of orientation method for defining the default coordinate system.
|
JointmarkBuilder.ProjectionDirectionOptions |
The projection direction used to project points onto the reference sheet
|
JointmarkBuilder.ReferenceSheetTypes |
The type of sheets to create
|
JointmarkGuideBuilder.GuideCurvesData |
This class holds the data returned from
JointmarkGuideBuilder.getGuideCurves() |
JointmarkGuideBuilder.Location |
The type of guide curve
|
JointmarkGuideBuilder.SpaceMethod |
Options for Spacing Method
|
JointmarkGuideBuilder.SpaceOption |
Spacing Option
|
JointmarkPointsBuilder.PointPosition |
The point classification
|
LogInfo |
Represents entity and its log message .
|
OutputType |
Settings for output type .
|
PlugSlotBuilder.ArcProcessEnum |
arc process for the weld feature
|
PlugSlotBuilder.EnumContour |
contour type
|
PointMarkBuilder.WeldTypes |
The weld type to create.
|
SelectDatumPin.ValueData |
This class holds the data returned from
SelectDatumPin.getValue() |
SelectDatumPin.ValueWithCaeSetObjectInfoData |
This class holds the data returned from
SelectDatumPin.getValue() |
SelectDatumPin.ValueWithSnapData |
This class holds the data returned from
SelectDatumPin.getValue() |
SelectDatumSurface.ValueData |
This class holds the data returned from
SelectDatumSurface.getValue() |
SelectDatumSurface.ValueWithCaeSetObjectInfoData |
This class holds the data returned from
SelectDatumSurface.getValue() |
SelectDatumSurface.ValueWithSnapData |
This class holds the data returned from
SelectDatumSurface.getValue() |
SurfaceWeldBuilder.DestinationTypes |
The option specifying where the surface weld feature should be created.
|
UserDefinedWeldBuilder.WeldTypes |
Weld types for 4GD classes.
|
WeldAdvisorBuilder.FailedObjectsData |
This class holds the data returned from
WeldAdvisorBuilder.getFailedObjects(nxopen.weld.WeldAdvisorCheckerType) |
WeldAdvisorCheckerType |
the type of checker
|
WeldAdvisorCustomerDefault |
the customer default value types
|
WeldArcMethod |
Settings for output type
|
WeldAttribType |
the type of attribute
|
WeldBeadBuilder.BeadLocationMethod |
Settings to indicate the desired location of the bead.
|
WeldBeadBuilder.OutputTypes |
Settings to indicate the update behaviour of the bead feature
|
WeldBeadBuilder.Types |
Settings to indicate the sweep shape of the bead.
|
WeldBeadPathBuilder.OffsetMethodType |
Settings to indicate the desired offset method.
|
WeldBeadPathBuilder.UpdatePathData |
This class holds the data returned from
WeldBeadPathBuilder.updatePath() |
WeldBeadSizeBuilder.Size |
Settings to indicate which standard size to use from the customer defaults file.
|
WeldBeadSizeBuilder.TriangleMethodType |
Settings to indicate the type of method used to build a triangle shape.
|
WeldBeadSizeBuilder.TriangleTypes |
Settings to indicate the type of triangle.
|
WeldContourShape |
Top contour shape
|
WeldCreationDirection |
the type of creation direction
|
WeldCustom |
Settings for output solid type
|
WeldDatumControlDirection |
the control direction for datum
|
WeldFacesetIndex |
the index of user picked face sets
|
WeldFeatureOutput |
Feature output
|
WeldFeatureSetType |
the feature set types
|
WeldFillBuilder.BoundaryMethodType |
Defines whether the initial boundary of the fill pattern is defined
by a two point rectangle or a curve.
|
WeldFillBuilder.WidthAlongType |
Defines the direction the fill strip's length is aligned
|
WeldGrooveBuilder.Contour |
The options for Contour Type
|
WeldGrooveBuilder.Edge |
A value indicating whether the edges have been prepared
|
WeldGrooveBuilder.Prepare |
The type of edges to be prepared
|
WeldGrooveBuilder.SkipWeldMethod |
The options for creating Skip Weld
|
WeldGrooveBuilder.Taper |
The type of Taper Method
|
WeldGrooveBuilder.Types |
The types of Groove to create
|
WeldGrooveExtension |
Groove Extension Type
|
WeldGrooveShape |
Groove Weld Section type
|
WeldGrooveType |
Groove Creation Type
|
WeldGroupIdColor |
the group id color indexes
|
WeldJointBuilder.Application |
Application where joints are created.
|
WeldJointBuilder.CoordinateSystem |
Coordinate system specification.
|
WeldJointBuilder.DestinationTypes |
Where to create new joints.
|
WeldJointBuilder.JointMidPointData |
Joint evaluation information at the mid point.
|
WeldJointBuilder.MidPointInformationData |
This class holds the data returned from
WeldJointBuilder.getMidPointInformation(nxopen.weld.WeldJointBuilder.CoordinateSystem) |
WeldJointBuilder.NewlyCreatedJointsData |
This class holds the data returned from
WeldJointBuilder.getNewlyCreatedJoints() |
WeldJointBuilder.SplitTypes |
Joint splitting options.
|
WeldJointBuilder.Types |
Creation method.
|
WeldJointBuilder.WeldTypes |
Weld types.
|
WeldLabelBuilder.OrientationPlaneType |
This represents the Orientation Plane Type.
|
WeldMeasurementSizeMethod |
the size method for measurement
|
WeldObjectBuilder.CommandName |
Commands that a callback will be invoked after dialog completion.
|
WeldObjectBuilder.FeatureInfo |
Structure used to identify if each feature is newly created or edited.
|
WeldOverlapStatus |
the create status for overlap
|
WeldParasetLocation |
the index of user picked refsheet location
|
WeldPmiBuilder.OrientationPlaneType |
This represents the Orientation Plane Type.
|
WeldPointBuilder.CsysData |
This class holds the data returned from
WeldPointBuilder.getCsys() |
WeldPointBuilder.FaceSetData |
This class holds the data returned from
WeldPointBuilder.getFaceSet(int) |
WeldPointDirection |
Spot direction
|
WeldPointExitBuilder.CommandName |
The command name used for the newly created features.
|
WeldPointExitBuilder.FeatureInfo |
Structure used to identify newly created features.
|
WeldPointExitBuilder.MethodUsed |
The method use to create the features.
|
WeldPointExtendMethod |
Offset curve extend method
|
WeldPointLocation |
Settings locating spot welds using guide curves/edges
|
WeldPointMethod |
Settings for method
|
WeldPointReferenceSheetType |
Settings for the reference sheet
|
WeldPointSpacingMethod |
Guide spacing method
|
WeldPrepareEdges |
Settings for prepare edges
|
WeldProjectionMethod |
Settings project method type
|
WeldRootUpdate |
Arc process type
|
WeldSelectionType |
the type of selction
|
WeldSpacingCalcMethod |
Settings spacing method type
|
WeldTaperMethod |
Settings for groove taper method
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.