public class WeldPointMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FROM_POINTS
create fix/single/none points using existing points
|
static int |
_MIRROR
mirror existing points
|
static int |
_MULTIPLE
use guide curve(s) or edge(s) to generate spot weld points
|
static int |
_SINGLE
use point constructor to generate spot weld points
|
static int |
_TRANSLATE
translate existing points
|
static WeldPointMethod |
FROM_POINTS
create fix/single/none points using existing points
|
static WeldPointMethod |
MIRROR
mirror existing points
|
static WeldPointMethod |
MULTIPLE
use guide curve(s) or edge(s) to generate spot weld points
|
static WeldPointMethod |
SINGLE
use point constructor to generate spot weld points
|
static WeldPointMethod |
TRANSLATE
translate existing points
|
Modifier and Type | Method and Description |
---|---|
static WeldPointMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPointMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPointMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldPointMethod MULTIPLE
public static final WeldPointMethod SINGLE
public static final WeldPointMethod MIRROR
public static final WeldPointMethod TRANSLATE
public static final WeldPointMethod FROM_POINTS
public static final int _MULTIPLE
public static final int _SINGLE
public static final int _MIRROR
public static final int _TRANSLATE
public static final int _FROM_POINTS
public static WeldPointMethod valueOf(int value)
public static WeldPointMethod valueOf(String name)
public static WeldPointMethod[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.