public static class JointmarkBuilder.ConnectedPanelTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FOUR |
static int |
_THREE |
static int |
_TWO |
static JointmarkBuilder.ConnectedPanelTypes |
FOUR |
static JointmarkBuilder.ConnectedPanelTypes |
THREE |
static JointmarkBuilder.ConnectedPanelTypes |
TWO |
Modifier and Type | Method and Description |
---|---|
static JointmarkBuilder.ConnectedPanelTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JointmarkBuilder.ConnectedPanelTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JointmarkBuilder.ConnectedPanelTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final JointmarkBuilder.ConnectedPanelTypes TWO
public static final JointmarkBuilder.ConnectedPanelTypes THREE
public static final JointmarkBuilder.ConnectedPanelTypes FOUR
public static final int _TWO
public static final int _THREE
public static final int _FOUR
public static JointmarkBuilder.ConnectedPanelTypes valueOf(int value)
public static JointmarkBuilder.ConnectedPanelTypes valueOf(String name)
public static JointmarkBuilder.ConnectedPanelTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.