public static class WeldJointBuilder.Application extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ROUTING
Routing Application.
|
static int |
_STRUCTURE_WELDING
Structure Welding Application.
|
static WeldJointBuilder.Application |
ROUTING
Routing Application.
|
static WeldJointBuilder.Application |
STRUCTURE_WELDING
Structure Welding Application.
|
Modifier and Type | Method and Description |
---|---|
static WeldJointBuilder.Application |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldJointBuilder.Application |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldJointBuilder.Application[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldJointBuilder.Application STRUCTURE_WELDING
public static final WeldJointBuilder.Application ROUTING
public static final int _STRUCTURE_WELDING
public static final int _ROUTING
public static WeldJointBuilder.Application valueOf(int value)
public static WeldJointBuilder.Application valueOf(String name)
public static WeldJointBuilder.Application[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.