Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Class and Description |
---|
CustomManager
Represents weld interface to customize the creation of welding joint features.
|
WeldCpdUtils
Provides methods for access a WeldCpdUtils class object in NX.
|
Class and Description |
---|
WeldManager
Manages weld features and assistant tools.
|
Class and Description |
---|
CharacteristicsBuilder
This builder allows you to define the attribute values to be set on the
output of the weld feature.
|
Class and Description |
---|
AutoPointBuilder
Represents a
AutoPointBuilder builder To create a new instance of this class, use WeldManager.createAutoPointBuilder(nxopen.features.Feature) Default values. |
AutoPointBuilder.InterferenceDetails
Settings to indicate whether an interference is near an existing weld point.
|
AutoPointBuilder.Types
Settings to indicate whether new features should be created, or if features will be reused.
|
AutoWeldSymbolsBuilder
Represents a
AutoWeldSymbolsBuilder builder To create a new instance of this class, use WeldManager.createAutoWeldSymbolsBuilder() Created in NX8.0.0 |
CharacteristicsBuilder
This builder allows you to define the attribute values to be set on the
output of the weld feature.
|
CharacteristicsBuilder.Type
The custom type of the datum specified for creation.
|
CharacteristicsSelectionBuilder
This builder allows you to define the attribute values to be set on the
output of the weld feature.
|
CharacteristicsValueBuilder
The object containing the information about the attribute to be
placed on the output of the weld feature.
|
CharacteristicsValueBuilder.Type
Settings to indicate the type of value contained in the attribute.
|
CompoundWeld
Represents a compound weld feature.
|
CompoundWeldBuilder
Represents a
CompoundWeld builder. |
ConnectedFaceFinderBuilder
Represents a builder to run the Connected Face Finder operation.
|
ConnectedPart
Represents weld connected part to customize the retrieval of connected part information.
|
ConnectionFinderBuilder
Represents a builder to display, manage, delete, and allow the user to
reparent face information for the weld objects.
|
ConnectionFinderBuilder.FilterTypes
Filter values to control "Save All" processing.
|
CustomManager.DatumIconHandler
Method called from the part navigator to define the datum surface and pin icon.
|
CustomManager.ModifyFeatureHandler
User defined method that is called whenever a welding joints are created or edited
|
CustomManager.PipeJointSetType
User defined method that is called whenever a welding joint is created.
|
CustomManager.PointExitHandler
User defined method that is called whenever a welding features are created through Weld Point command.
|
CustomManager.VariableBevelHandler
User defined method that returns the angle divisions for a variable bevel.
|
CustomManager.WeldJointHandler
User defined method that is called whenever a welding joint is created or updated
|
DatumCommonBuilder
Used to create or edit a
DatumSurface or DatumPin feature. |
DatumCommonBuilder.ControlMethodTypes
Settings for the method used to define the control direction.
|
DatumCommonBuilder.CreationDirectionMethods
Settings to define the creation direction.
|
DatumCommonBuilder.CustomTypes
The custom type of the datum specified for creation.
|
DatumCommonBuilder.SolidTypes
Settings for defining the solid type to create for the datum object.
|
DatumIconBuilder
Represents a
DatumIconBuilder class used to control the part navigator icon for Datum Pin and Surface Locators. |
DatumPin
Represents a Weld Datum Pin feature
To create or edit an instance of this class, use DatumPinBuilder Created in NX8.5.0 |
DatumPinBuilder
Used to create or edit a
DatumPin feature. |
DatumSurface
Represents a Weld Datum Surface feature
To create or edit an instance of this class, use DatumSurfaceBuilder Created in NX8.5.0 |
DatumSurfaceBuilder
Used to create or edit a
DatumSurface feature. |
DatumSurfaceBuilder.Types
Settings to indicate the construction type used for the datum surface.
|
EasyPatternBuilder
Represents the easy pattern builder.
|
EasyPatternBuilder.HemMethodTypes
Indicates the method to use to compute the hem vector location.
|
EasyPatternBuilder.PlaneMethodTypes
The plane to cut sections in to determine placement measurement patterns.
|
EasyPatternBuilder.SpacingMethodTypes
Indicates whether planes should be cut a grid lines, or if a single plane should be used.
|
EasyPatternBuilder.Types
Controls the type of pattern.
|
EdgePrep
Represents a Weld Edge Prep feature
To create or edit an instance of this class, use EdgePrepBuilder Created in NX8.0.0 |
EdgePrepBuilder
A builder used to create or edit a
EdgePrep feature. |
EdgePrepValuesBuilder
Used to view or edit the values used to define the welding joint and edge preparation.
|
EdgePrepValuesBuilder.Apply
Option to indicate how the values are to be updated.
|
EdgePrepValuesBuilder.Option
Option to indicate how the values are to be used.
|
ExportWeldBuilder
Represents a ExportWeldBuilder class
To create a new instance of this class, use WeldManager.createExportWeldBuilder() Default values. |
ExportWeldBuilder.AttributeOriginType
the Attribute Origin enum
|
ExportWeldBuilder.OutputType
the Output Type enum
|
ExportWeldJointBuilder
Represents exporting weld joints.
|
Fill
Represents a Weld Fill feature
To create or edit an instance of this class, use WeldFillBuilder Created in NX7.5.0 |
FilletBuilder
Represents a
Fillet builder. |
FilletBuilder.EnumConstructionMethod
the options for which construction method to use.
|
FilletBuilder.EnumContour
the Contour enum.
|
FilletBuilder.EnumExtendEdges
the options for populating the edge selections.
|
FilletBuilder.EnumExtensionMethod
the Extension enum.
|
FilletBuilder.EnumSkipWeldMethod
the Skipweld enum.
|
FilletBuilder.EnumWeldingType
the WeldingType enum.
|
GrooveBuilder
Represents a Groove Weld feature
To create a new instance of this class, use WeldManager.createWeldGrooveBuilder(nxopen.features.Feature) Created in NX5.0.0 |
IFeature
Represents a Weld Assistant or Structure Welding created feature .
|
InformationBuilder
This class is used by "Fabrication Information" to output fabrication objects information.
|
InformationBuilder.AttributeOriginType
the Object Type enum
|
JointExitBuilder
Used to set custom edge preparation parameters of a
WeldJoint feaure. |
JointExitBuilder.BodySide
Settings to indicate the side the positions should be applied to.
|
JointExitBuilder.EdgePrepValuesData
This class holds the data returned from
JointExitBuilder.getEdgePrepValues(nxopen.weld.JointExitBuilder.Positions) |
JointExitBuilder.FilletSizes
The structure for defining fillet weld lengths.
|
JointExitBuilder.Positions
Settings to indicate the desired position of edge preporation thickness and angle.
|
JointItemBuilder
Used to create or edit a
Weld.WeldJoint feature. |
JointItemBuilderList
Represents a list of objects.
|
Jointmark
Represents a Weld Jointmark Feature.
|
JointmarkBuilder
Represents a
Jointmark builder To create a new instance of this class, use WeldManager.createJointmarkBuilder(nxopen.weld.Jointmark) Default values. |
JointmarkBuilder.ConnectedPanelTypes
The type of sheets to create
|
JointmarkBuilder.Method
The type of construction method for creating Jointmark
|
JointmarkBuilder.OrientationMethodTypes
The type of orientation method for defining the default coordinate system.
|
JointmarkBuilder.ProjectionDirectionOptions
The projection direction used to project points onto the reference sheet
|
JointmarkBuilder.ReferenceSheetTypes
The type of sheets to create
|
JointmarkFaceSetsBuilder
Used to create or edit a set of faces for Jointmark
To create a new instance of this class, use JointmarkBuilder.newFaceSets() Created in NX9.0.0 |
JointmarkFaceSetsBuilderList
Represents a list of objects.
|
JointmarkGuideBuilder
Used to create or edit a guide curve for Jointmark.
|
JointmarkGuideBuilder.GuideCurvesData
This class holds the data returned from
JointmarkGuideBuilder.getGuideCurves() |
JointmarkGuideBuilder.Location
The type of guide curve
|
JointmarkGuideBuilder.SpaceMethod
Options for Spacing Method
|
JointmarkGuideBuilder.SpaceOption
Spacing Option
|
JointmarkGuideBuilderList
Represents a list of objects.
|
JointmarkPointsBuilder
Used to create or edit a point in the list of points for Jointmark
To create a new instance of this class, use JointmarkBuilder.newPoints() Created in NX9.0.0 |
JointmarkPointsBuilder.PointPosition
The point classification
|
JointmarkPointsBuilderList
Represents a list of objects.
|
LocatorReferenceBuilder
This class is used by "Locator Reference" to add the additional component for a weld datum DF.
|
LogInfo
Represents entity and its log message .
|
OutputType
Settings for output type .
|
PlugSlotBuilder
Represents a
PlugSlot builder To create a new instance of this class, use WeldManager.createPlugSlotBuilder(nxopen.features.Feature) Default values. |
PlugSlotBuilder.ArcProcessEnum
arc process for the weld feature
|
PlugSlotBuilder.EnumContour
contour type
|
PointMark
Represents a Weld PointMark Feature.
|
PointMarkBuilder
Used to create or edit a
PointMark feature. |
PointMarkBuilder.WeldTypes
The weld type to create.
|
PointMarkPoint
Represents a Weld.PointMarkPoint Feature.
|
PointMarkPointBuilder
Used to create or edit a point in the list of points for Jointmark
To create a new instance of this class, use PointMarkBuilder.newPointsOverride() Created in NX10.0.0 |
SelectDatumPin
Represents a single object selection.
|
SelectDatumPin.ValueData
This class holds the data returned from
SelectDatumPin.getValue() |
SelectDatumPin.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectDatumPin.getValue() |
SelectDatumPin.ValueWithSnapData
This class holds the data returned from
SelectDatumPin.getValue() |
SelectDatumSurface
Represents a single object selection.
|
SelectDatumSurface.ValueData
This class holds the data returned from
SelectDatumSurface.getValue() |
SelectDatumSurface.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectDatumSurface.getValue() |
SelectDatumSurface.ValueWithSnapData
This class holds the data returned from
SelectDatumSurface.getValue() |
StructureWeldBuilder
This class is used to create or edit the information shared among all Structure Weld builders.
|
SurfaceWeld
Represents a surface weld feature
To create or edit an instance of this class, use SurfaceWeldBuilder Created in NX9.0.0 |
SurfaceWeldBuilder
Use to create or edit a
SurfaceWeld feature. |
SurfaceWeldBuilder.DestinationTypes
The option specifying where the surface weld feature should be created.
|
UserDefinedWeldBuilder
Represents a
UserDefinedWeldBuilder builder. |
UserDefinedWeldBuilder.WeldTypes
Weld types for 4GD classes.
|
WeldAdvisorBuilder
Represents a weld advisor test
To create a new instance of this class, use WeldManager.createWeldAdvisorBuilder() Created in NX7.5.0 |
WeldAdvisorBuilder.FailedObjectsData
This class holds the data returned from
WeldAdvisorBuilder.getFailedObjects(nxopen.weld.WeldAdvisorCheckerType) |
WeldAdvisorCheckerType
the type of checker
|
WeldAdvisorCustomerDefault
the customer default value types
|
WeldArcMethod
Settings for output type
|
WeldAttribType
the type of attribute
|
WeldBeadBuilder
Used to create or edit a
WeldBead feature. |
WeldBeadBuilder.BeadLocationMethod
Settings to indicate the desired location of the bead.
|
WeldBeadBuilder.OutputTypes
Settings to indicate the update behaviour of the bead feature
|
WeldBeadBuilder.Types
Settings to indicate the sweep shape of the bead.
|
WeldBeadPathBuilder
Represents the path the bead shape will be swept along.
|
WeldBeadPathBuilder.OffsetMethodType
Settings to indicate the desired offset method.
|
WeldBeadPathBuilder.UpdatePathData
This class holds the data returned from
WeldBeadPathBuilder.updatePath() |
WeldBeadPathBuilderList
Represents a list of objects.
|
WeldBeadSizeBuilder
This builder is used to define the bead shape.
|
WeldBeadSizeBuilder.Size
Settings to indicate which standard size to use from the customer defaults file.
|
WeldBeadSizeBuilder.TriangleMethodType
Settings to indicate the type of method used to build a triangle shape.
|
WeldBeadSizeBuilder.TriangleTypes
Settings to indicate the type of triangle.
|
WeldBeadSizeBuilderList
Represents a list of objects.
|
WeldContourShape
Top contour shape
|
WeldCreationDirection
the type of creation direction
|
WeldCustom
Settings for output solid type
|
WeldDatumControlDirection
the control direction for datum
|
WeldFacesetIndex
the index of user picked face sets
|
WeldFeatureOutput
Feature output
|
WeldFeatureSetType
the feature set types
|
WeldFillBuilder
A builder used to create or edit a
Fill feature. |
WeldFillBuilder.BoundaryMethodType
Defines whether the initial boundary of the fill pattern is defined
by a two point rectangle or a curve.
|
WeldFillBuilder.WidthAlongType
Defines the direction the fill strip's length is aligned
|
WeldFillStripBuilder
A builder used to create or edit a single strip of the
WeldFillBuilder . |
WeldFillStripBuilderList
Represents a list of objects.
|
WeldGrooveBuilder
Represents a
WeldGroove builder To create a new instance of this class, use WeldManager.createWeldGroove1Builder(nxopen.features.Feature) Default values. |
WeldGrooveBuilder.Contour
The options for Contour Type
|
WeldGrooveBuilder.Edge
A value indicating whether the edges have been prepared
|
WeldGrooveBuilder.Prepare
The type of edges to be prepared
|
WeldGrooveBuilder.SkipWeldMethod
The options for creating Skip Weld
|
WeldGrooveBuilder.Taper
The type of Taper Method
|
WeldGrooveBuilder.Types
The types of Groove to create
|
WeldGrooveExtension
Groove Extension Type
|
WeldGrooveShape
Groove Weld Section type
|
WeldGrooveType
Groove Creation Type
|
WeldGroupIdColor
the group id color indexes
|
WeldImportBuilder
Creates Weld features by reading a csv file
To create a new instance of this class, use WeldManager.createImportBuilder() Created in NX7.5.1 |
WeldJoint
Represents a weld joint feature
To create or edit an instance of this class, use WeldJointBuilder Created in NX8.0.0 |
WeldJointBuilder
Used to create or edit a
WeldJoint feature. |
WeldJointBuilder.Application
Application where joints are created.
|
WeldJointBuilder.CoordinateSystem
Coordinate system specification.
|
WeldJointBuilder.DestinationTypes
Where to create new joints.
|
WeldJointBuilder.JointMidPointData
Joint evaluation information at the mid point.
|
WeldJointBuilder.MidPointInformationData
This class holds the data returned from
WeldJointBuilder.getMidPointInformation(nxopen.weld.WeldJointBuilder.CoordinateSystem) |
WeldJointBuilder.NewlyCreatedJointsData
This class holds the data returned from
WeldJointBuilder.getNewlyCreatedJoints() |
WeldJointBuilder.SplitTypes
Joint splitting options.
|
WeldJointBuilder.Types
Creation method.
|
WeldJointBuilder.WeldTypes
Weld types.
|
WeldLabelBuilder
Create weld labels for multiple welds and BIW locators, this builder's Commit can produce more than one object,
the GetCommittedObjects can be used to get the objects and the order of GetCommittedObject's output array is stable.
|
WeldLabelBuilder.OrientationPlaneType
This represents the Orientation Plane Type.
|
WeldMeasurementSizeMethod
the size method for measurement
|
WeldObjectBuilder
Represents a
WeldObjectBuilder class used to collect welding objects created or edited from a command. |
WeldObjectBuilder.CommandName
Commands that a callback will be invoked after dialog completion.
|
WeldObjectBuilder.FeatureInfo
Structure used to identify if each feature is newly created or edited.
|
WeldOverlapStatus
the create status for overlap
|
WeldParasetLocation
the index of user picked refsheet location
|
WeldPmiBuilder
Create PMI symbols for multiple structure welds, this builder's Commit can produce more than one object,
the GetCommittedObjects can be used to get the objects and the order of GetCommittedObject's output array is stable.
|
WeldPmiBuilder.OrientationPlaneType
This represents the Orientation Plane Type.
|
WeldPointBuilder
Represents a Spot Weld feature
To create a new instance of this class, use WeldManager.createWeldPointBuilder(nxopen.features.Feature) Default values. |
WeldPointBuilder.CsysData
This class holds the data returned from
WeldPointBuilder.getCsys() |
WeldPointBuilder.FaceSetData
This class holds the data returned from
WeldPointBuilder.getFaceSet(int) |
WeldPointDirection
Spot direction
|
WeldPointExitBuilder
Represents a
WeldPointExitBuilder class used to pass welding object from the Weld Point command to a user callback. |
WeldPointExitBuilder.CommandName
The command name used for the newly created features.
|
WeldPointExitBuilder.FeatureInfo
Structure used to identify newly created features.
|
WeldPointExitBuilder.MethodUsed
The method use to create the features.
|
WeldPointExtendMethod
Offset curve extend method
|
WeldPointLocation
Settings locating spot welds using guide curves/edges
|
WeldPointMethod
Settings for method
|
WeldPointReferenceSheetType
Settings for the reference sheet
|
WeldPointSpacingMethod
Guide spacing method
|
WeldPreferenceBuilder
Represents a
WeldPreferenceBuilder builder To create a new instance of this class, use WeldManager.createPreferenceBuilder() Default values. |
WeldPrepareEdges
Settings for prepare edges
|
WeldProjectionMethod
Settings project method type
|
WeldRootUpdate
Arc process type
|
WeldSelectionType
the type of selction
|
WeldSpacingCalcMethod
Settings spacing method type
|
WeldTaperMethod
Settings for groove taper method
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.