public interface WeldObjectBuilder extends TaggedObject, IComponentBuilder
WeldObjectBuilder
class used to collect welding objects created or edited from a command.
Modifier and Type | Interface and Description |
---|---|
static class |
WeldObjectBuilder.CommandName
Commands that a callback will be invoked after dialog completion.
|
static class |
WeldObjectBuilder.FeatureInfo
Structure used to identify if each feature is newly created or edited.
|
Modifier and Type | Method and Description |
---|---|
WeldObjectBuilder.CommandName |
commandUsed()
Returns the command name that was last used to create or modify features
License requirements: None. |
WeldObjectBuilder.FeatureInfo[] |
getFeatureInformation()
Gets the created and modifed features
License requirements: None. |
printTestData, printTestData, tag, tagValue
validate
WeldObjectBuilder.CommandName commandUsed() throws NXException, RemoteException
NXException
RemoteException
WeldObjectBuilder.FeatureInfo[] getFeatureInformation() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.