EdgeBlendBuilder Class¶
-
class
NXOpen.Features.
EdgeBlendBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Edge Blend builder.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateEdgeBlendBuilder()
Default values.
Property Value TrimmingOption False New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AllInstancesOption | Returns or sets the blend all instances option |
BlendFaceContinuity | Returns or sets the Blend Face Continuity option |
BlendOrder | Returns or sets the order of blending for edge blend |
CliffEdges | Returns or sets the forced cliff edges for edge blend |
ConvexConcaveY | Returns or sets the Special blend at convex / concave Y option |
LimitFailingAreas | Returns or sets the Limit Failing Areas option |
LimitsListData | Returns the limits list |
MoveSharpEdge | Returns or sets the Maintain blend and move sharp edges option |
NonCliffEdges | Returns or sets the prohibited cliff edges for edge blend |
OverlapOption | Returns or sets the overlap resolution for edge blend |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchComplexGeometryAreas | Returns or sets the Patch Areas option |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RemoveSelfIntersection | Returns or sets the Remove self-intersection option |
RollOntoEdge | Returns or sets the Roll onto edges option |
RollOverSmoothEdge | Returns or sets the Roll over smooth edges option |
SegmentBlendFaces | Returns or sets the Segment blend to match face segments option |
SetbackOption | Returns or sets the setback option for edge blend |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance of a variable blend |
TrimmingOption | Returns or sets the trimming option |
ZeroSlopeRadiusFunctionAtChainEnds | Returns or sets the zero slope radius function at chain ends option |
Methods¶
Method | Description |
---|---|
AddChainset | Add an edge blend chainset to the edge blend @return Index of chainset, indicating which chainset we are dealing with |
AddNewStopshortData | Add an edge blend stop short data for an edge in the edge blend @return Index of where stop short data item is created. |
AddSetbackData | Add an edge blend setback data for an edge in the edge blend @return Index of where setback data item is created. |
AddStopshortData | Add an edge blend stop short data for an edge in the edge blend @return Index of where stop short data item is created. |
AddVariablePointData | Add an edge blend variable radius data for an edge in the edge blend @return Index of where variable radius data item is created |
AddVariableRadiusData | Add an edge blend variable radius data for an edge in the edge blend @return Index of where variable radius data item is created |
AddVariableRadiusDataNew | Add an edge blend variable radius data for an edge in the edge blend * Note: This ja will always create arclength parameter @return Index of where variable radius data item is created |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditVariablePointData | Edit an edge blend variable radius data for an edge in the edge blend |
EditVariableRadiusData | Edit an edge blend variable radius data for an edge in the edge blend |
EditVariableRadiusDataNew | Edit an edge blend variable radius data for an edge in the edge blend |
GetChainset | Get collector and radius for an edge blend chainset given the index of the chainset |
GetChainsetAndSectionValue | Get collector, radius and section types for an edge blend chainset given the index of the chainset |
GetChainsetAndStatus | Get collector, radius and validity status for an edge blend chainset given the index of the chainset |
GetChainsetIndex | Get the index of edge blend chainset given the collector @return Index of chainset, indicating which chainset we are dealing with |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetNewStopshortData | Get an edge blend stop short data for the index provided @return the Stopshort Data |
GetNumberOfValidChainsets | Get the number of valid chainsets @return Number of valid chainsets |
GetObject | Returns the object currently being edited by this builder. |
GetSetbackData | Get an edge blend setback data for the index provided @return Array of Edge collector tags that are used by the setback |
GetStopshortData | Get an edge blend stop short data for the index provided @return The distance for the stopshort on the edge. |
GetVariableRadiusData | Get all the variable radii data for an edge in the edge blend @return Parameter locations of points on the edge |
GetVariableRadiusDataNew | Get all the variable radii data for an edge in the edge blend |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RemoveChainset | Delete an edge blend chainset from the edge blend. |
RemoveChainsetByCollector | Delete an edge blend chainset from the edge blend. |
RemoveNewStopshortData | Remove an edge blend stop short corresponding to a BlendStopshortBuilder |
RemoveSetbackData | Remove an edge blend setback data for an edge in the edge blend |
RemoveStopshortData | Remove an edge blend stop short data for an edge |
RemoveStopshortDataByType | Remove the stop short from an edge, given its type and location |
RemoveVariableRadiusData | Remove variable radius data on an edge by the parameter value of the point on the edge |
RemoveVariableRadiusDataByIndex | Remove variable radius data on an edge by the index into the point array on the edge |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EdgeBlendBuilderConic Enumeration | This enum represents the Conic option |
EdgeBlendBuilderFaceContinuity Enumeration | The Blend Face Continuity |
EdgeBlendBuilderOrderOfBlending Enumeration | This enum represents the order of Blending |
EdgeBlendBuilderOverlap Enumeration | This enum represents the Overlap resolution options for Edge Blend |
EdgeBlendBuilderRhotype Enumeration | This enum represents the rho type for conic section blend |
EdgeBlendBuilderSection Enumeration | This enum represents the Section option |
EdgeBlendBuilderSetback Enumeration | This enum represents the Setback option |
Property Detail¶
AllInstancesOption¶
-
EdgeBlendBuilder.
AllInstancesOption
¶ Returns or sets the blend all instances option
-------------------------------------
Getter Method
Signature
AllInstancesOption()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllInstancesOption(optionValue)
Parameters: optionValue (bool) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BlendFaceContinuity¶
-
EdgeBlendBuilder.
BlendFaceContinuity
¶ Returns or sets the Blend Face Continuity option
-------------------------------------
Getter Method
Signature
BlendFaceContinuity()
Returns: Return type: NXOpen.Features.EdgeBlendBuilderFaceContinuity
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlendFaceContinuity(optionValue)
Parameters: optionValue ( NXOpen.Features.EdgeBlendBuilderFaceContinuity
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BlendOrder¶
-
EdgeBlendBuilder.
BlendOrder
¶ Returns or sets the order of blending for edge blend
-------------------------------------
Getter Method
Signature
BlendOrder()
Returns: Return type: NXOpen.Features.EdgeBlendBuilderOrderOfBlending
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlendOrder(blendOrder)
Parameters: blendOrder ( NXOpen.Features.EdgeBlendBuilderOrderOfBlending
) –New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CliffEdges¶
-
EdgeBlendBuilder.
CliffEdges
¶ Returns or sets the forced cliff edges for edge blend
-------------------------------------
Getter Method
Signature
CliffEdges()
Returns: The cliff edge collector Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CliffEdges(cliffEdgeCollector)
Parameters: cliffEdgeCollector ( NXOpen.ScCollector
) – The cliff edge collectorNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ConvexConcaveY¶
-
EdgeBlendBuilder.
ConvexConcaveY
¶ Returns or sets the Special blend at convex / concave Y option
-------------------------------------
Getter Method
Signature
ConvexConcaveY()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConvexConcaveY(optionValue)
Parameters: optionValue (bool) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
LimitFailingAreas¶
-
EdgeBlendBuilder.
LimitFailingAreas
¶ Returns or sets the Limit Failing Areas option
-------------------------------------
Getter Method
Signature
LimitFailingAreas()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitFailingAreas(optionValue)
Parameters: optionValue (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
LimitsListData¶
-
EdgeBlendBuilder.
LimitsListData
¶ Returns the limits list
-------------------------------------
Getter Method
Signature
LimitsListData()
Returns: Return type: NXOpen.GeometricUtilities.BlendLimitsData
New in version NX5.0.0.
License requirements: None.
MoveSharpEdge¶
-
EdgeBlendBuilder.
MoveSharpEdge
¶ Returns or sets the Maintain blend and move sharp edges option
-------------------------------------
Getter Method
Signature
MoveSharpEdge()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MoveSharpEdge(optionValue)
Parameters: optionValue (bool) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
NonCliffEdges¶
-
EdgeBlendBuilder.
NonCliffEdges
¶ Returns or sets the prohibited cliff edges for edge blend
-------------------------------------
Getter Method
Signature
NonCliffEdges()
Returns: The non cliff edge collector Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonCliffEdges(nonCliffEdgeCollector)
Parameters: nonCliffEdgeCollector ( NXOpen.ScCollector
) – The non cliff edge collectorNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OverlapOption¶
-
EdgeBlendBuilder.
OverlapOption
¶ Returns or sets the overlap resolution for edge blend
-------------------------------------
Getter Method
Signature
OverlapOption()
Returns: Return type: NXOpen.Features.EdgeBlendBuilderOverlap
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverlapOption(overlapOption)
Parameters: overlapOption ( NXOpen.Features.EdgeBlendBuilderOverlap
) –New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PatchComplexGeometryAreas¶
-
EdgeBlendBuilder.
PatchComplexGeometryAreas
¶ Returns or sets the Patch Areas option
-------------------------------------
Getter Method
Signature
PatchComplexGeometryAreas()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PatchComplexGeometryAreas(optionValue)
Parameters: optionValue (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveSelfIntersection¶
-
EdgeBlendBuilder.
RemoveSelfIntersection
¶ Returns or sets the Remove self-intersection option
-------------------------------------
Getter Method
Signature
RemoveSelfIntersection()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RemoveSelfIntersection(optionValue)
Parameters: optionValue (bool) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RollOntoEdge¶
-
EdgeBlendBuilder.
RollOntoEdge
¶ Returns or sets the Roll onto edges option
-------------------------------------
Getter Method
Signature
RollOntoEdge()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RollOntoEdge(optionValue)
Parameters: optionValue (bool) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RollOverSmoothEdge¶
-
EdgeBlendBuilder.
RollOverSmoothEdge
¶ Returns or sets the Roll over smooth edges option
-------------------------------------
Getter Method
Signature
RollOverSmoothEdge()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RollOverSmoothEdge(optionValue)
Parameters: optionValue (bool) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SegmentBlendFaces¶
-
EdgeBlendBuilder.
SegmentBlendFaces
¶ Returns or sets the Segment blend to match face segments option
-------------------------------------
Getter Method
Signature
SegmentBlendFaces()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SegmentBlendFaces(optionValue)
Parameters: optionValue (bool) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetbackOption¶
-
EdgeBlendBuilder.
SetbackOption
¶ Returns or sets the setback option for edge blend
-------------------------------------
Getter Method
Signature
SetbackOption()
Returns: Return type: NXOpen.Features.EdgeBlendBuilderSetback
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SetbackOption(setbackOption)
Parameters: setbackOption ( NXOpen.Features.EdgeBlendBuilderSetback
) –New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Tolerance¶
-
EdgeBlendBuilder.
Tolerance
¶ Returns or sets the tolerance of a variable blend
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TrimmingOption¶
-
EdgeBlendBuilder.
TrimmingOption
¶ Returns or sets the trimming option
-------------------------------------
Getter Method
Signature
TrimmingOption()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimmingOption(optionValue)
Parameters: optionValue (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ZeroSlopeRadiusFunctionAtChainEnds¶
-
EdgeBlendBuilder.
ZeroSlopeRadiusFunctionAtChainEnds
¶ Returns or sets the zero slope radius function at chain ends option
-------------------------------------
Getter Method
Signature
ZeroSlopeRadiusFunctionAtChainEnds()
Returns: Return type: bool New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZeroSlopeRadiusFunctionAtChainEnds(optionValue)
Parameters: optionValue (bool) – New in version NX10.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
AddChainset¶
-
EdgeBlendBuilder.
AddChainset
¶ Overloaded method AddChainset
AddChainset(collector, radius)
AddChainset(collector, sectionType, conicMethod, rhoType, radius, center, rho)
-------------------------------------
Add an edge blend chainset to the edge blend
Signature
AddChainset(collector, radius)
Parameters: - collector (
NXOpen.ScCollector
) – The collector for this edge blend chainset - radius (str) – The radius of this chain set collector
Returns: Index of chainset, indicating which chainset we are dealing with
Return type: int
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Add an edge blend chainset to the edge blend
Signature
AddChainset(collector, sectionType, conicMethod, rhoType, radius, center, rho)
Parameters: - collector (
NXOpen.ScCollector
) – The collector for this edge blend chainset - sectionType (
NXOpen.Features.EdgeBlendBuilderSection
) – Shape specifier for this chainset - conicMethod (
NXOpen.Features.EdgeBlendBuilderConic
) – Shape subtype specifier for this chainset - rhoType (
NXOpen.Features.EdgeBlendBuilderRhotype
) – rho type for this chain set - radius (str) – The radius of this chain set collector
- center (str) – The conic center value of this chain set collector if type is Conic
- rho (str) – The conic rho value of this chain set collector if type is Conic
Returns: Index of chainset, indicating which chainset we are dealing with
Return type: int
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
AddNewStopshortData¶
-
EdgeBlendBuilder.
AddNewStopshortData
¶ Add an edge blend stop short data for an edge in the edge blend
Signature
AddNewStopshortData(builder)
Parameters: builder ( NXOpen.GeometricUtilities.BlendStopshortBuilder
) – the Stopshort DataReturns: Index of where stop short data item is created. Return type: int New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
AddSetbackData¶
-
EdgeBlendBuilder.
AddSetbackData
¶ Add an edge blend setback data for an edge in the edge blend
Signature
AddSetbackData(edgeArray, fromStart, distance)
Parameters: - edgeArray (list of
NXOpen.Edge
) – Array of Edge collector tags that are used by the setback - fromStart (list of bool) – if true, then the setback is defined at the start vertex. Otherwise, it is defined at the end vertex. There is one for each input edge.
- distance (list of str) – Array of distances
Returns: Index of where setback data item is created.
Return type: int
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- edgeArray (list of
AddStopshortData¶
-
EdgeBlendBuilder.
AddStopshortData
¶ Add an edge blend stop short data for an edge in the edge blend
Signature
AddStopshortData(edge, fromStart, distance)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - fromStart (bool) – if true, then the stopshort is defined at the start vertex. Otherwise, it is defined at the end vertex.
- distance (str) – The distance for the stopshort on the edge.
Returns: Index of where stop short data item is created.
Return type: int
New in version NX4.0.0.
Deprecated since version NX5.0.0: Use
Features.EdgeBlendBuilder.AddNewStopshortData()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
- edge (
AddVariablePointData¶
-
EdgeBlendBuilder.
AddVariablePointData
¶ Add an edge blend variable radius data for an edge in the edge blend
Signature
AddVariablePointData(edge, parameter, radius, centerValue, rhoValue, smartPoint, isExternal, isArclength)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - parameter (str) – Parameter location of point on the edge
- radius (str) – The radius at this point on the edge.
- centerValue (str) – The conic center value at this point on the edge.
- rhoValue (str) – The conic rho value at this point on the edge.
- smartPoint (
NXOpen.Point
) – Smart Point defining the location of this vr - isExternal (bool) – Flag indicating whether this point is external to blend
- isArclength (bool) – Flag indicating whether parameter is arclength or not
Returns: Index of where variable radius data item is created
Return type: int
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- edge (
AddVariableRadiusData¶
-
EdgeBlendBuilder.
AddVariableRadiusData
¶ Add an edge blend variable radius data for an edge in the edge blend
Signature
AddVariableRadiusData(edge, parameter, radius, smartPoint, isExternal)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - parameter (float) – Parameter location of point on the edge
- radius (str) – The radius at this point on the edge.
- smartPoint (
NXOpen.Point
) – Smart Point defining the location of this vr - isExternal (bool) – Flag indicating whether this point is external to blend
Returns: Index of where variable radius data item is created
Return type: int
New in version NX4.0.0.
Deprecated since version NX6.0.0: Use
Features.EdgeBlendBuilder.AddVariableRadiusDataNew()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
- edge (
AddVariableRadiusDataNew¶
-
EdgeBlendBuilder.
AddVariableRadiusDataNew
¶ Overloaded method AddVariableRadiusDataNew
AddVariableRadiusDataNew(edge, parameter, radius, smartPoint, isExternal)
AddVariableRadiusDataNew(edge, parameter, radius, smartPoint, isExternal, isArclength)
-------------------------------------
Add an edge blend variable radius data for an edge in the edge blend * Note: This ja will always create arclength parameter
Signature
AddVariableRadiusDataNew(edge, parameter, radius, smartPoint, isExternal)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - parameter (str) – Parameter location of point on the edge
- radius (str) – The radius at this point on the edge.
- smartPoint (
NXOpen.Point
) – Smart Point defining the location of this vr - isExternal (bool) – Flag indicating whether this point is external to blend
Returns: Index of where variable radius data item is created
Return type: int
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Add an edge blend variable radius data for an edge in the edge blend
Signature
AddVariableRadiusDataNew(edge, parameter, radius, smartPoint, isExternal, isArclength)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - parameter (str) – Parameter location of point on the edge
- radius (str) – The radius at this point on the edge.
- smartPoint (
NXOpen.Point
) – Smart Point defining the location of this vr - isExternal (bool) – Flag indicating whether this point is external to blend
- isArclength (bool) – Flag indicating whether parameter is arclength or not
Returns: Index of where variable radius data item is created
Return type: int
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
EditVariablePointData¶
-
EdgeBlendBuilder.
EditVariablePointData
¶ Edit an edge blend variable radius data for an edge in the edge blend
Signature
EditVariablePointData(edge, vrIndex, parameter, radius, centerValue, rhoValue, smartPoint, isExternal, isArclength)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - vrIndex (int) – Index of what variable radius data item to edit
- parameter (str) – Parameter location of point on the edge
- radius (str) – The radius at this point on the edge.
- centerValue (str) – The conic center value at this point on the edge.
- rhoValue (str) – The conic center value at this point on the edge.
- smartPoint (
NXOpen.Point
) – Smart Point defining the location of this vr - isExternal (bool) – Flag indicating whether this point is external to blend
- isArclength (bool) – Flag indicating whether the parameter is arclength or not
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- edge (
EditVariableRadiusData¶
-
EdgeBlendBuilder.
EditVariableRadiusData
¶ Edit an edge blend variable radius data for an edge in the edge blend
Signature
EditVariableRadiusData(edge, vrIndex, parameter, radius, smartPoint, isExternal)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - vrIndex (int) – Index of what variable radius data item to edit
- parameter (float) – Parameter location of point on the edge
- radius (str) – The radius at this point on the edge.
- smartPoint (
NXOpen.Point
) – Smart Point defining the location of this vr - isExternal (bool) – Flag indicating whether this point is external to blend
New in version NX4.0.0.
Deprecated since version NX6.0.0: Use
Features.EdgeBlendBuilder.EditVariableRadiusDataNew()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
- edge (
EditVariableRadiusDataNew¶
-
EdgeBlendBuilder.
EditVariableRadiusDataNew
¶ Overloaded method EditVariableRadiusDataNew
EditVariableRadiusDataNew(edge, vrIndex, parameter, radius, smartPoint, isExternal)
EditVariableRadiusDataNew(edge, vrIndex, parameter, radius, smartPoint, isExternal, isArclength)
-------------------------------------
Edit an edge blend variable radius data for an edge in the edge blend
Signature
EditVariableRadiusDataNew(edge, vrIndex, parameter, radius, smartPoint, isExternal)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - vrIndex (int) – Index of what variable radius data item to edit
- parameter (str) – Parameter location of point on the edge
- radius (str) – The radius at this point on the edge.
- smartPoint (
NXOpen.Point
) – Smart Point defining the location of this vr - isExternal (bool) – Flag indicating whether this point is external to blend
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Edit an edge blend variable radius data for an edge in the edge blend
Signature
EditVariableRadiusDataNew(edge, vrIndex, parameter, radius, smartPoint, isExternal, isArclength)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - vrIndex (int) – Index of what variable radius data item to edit
- parameter (str) – Parameter location of point on the edge
- radius (str) – The radius at this point on the edge.
- smartPoint (
NXOpen.Point
) – Smart Point defining the location of this vr - isExternal (bool) – Flag indicating whether this point is external to blend
- isArclength (bool) – Flag indicating whether the parameter is arclength or not
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
GetChainset¶
-
EdgeBlendBuilder.
GetChainset
¶ Get collector and radius for an edge blend chainset given the index of the chainset
Signature
GetChainset(csIndex)
Parameters: csIndex (int) – Index of chainset, indicating which chainset we are dealing with Returns: a tuple Return type: A tuple consisting of (collector, radius). collector is a NXOpen.ScCollector
. The collector for this edge blend chainset radius is aNXOpen.Expression
. The radius of this chain set collectorNew in version NX4.0.0.
License requirements: None.
GetChainsetAndSectionValue¶
-
EdgeBlendBuilder.
GetChainsetAndSectionValue
¶ Get collector, radius and section types for an edge blend chainset given the index of the chainset
Signature
GetChainsetAndSectionValue(csIndex)
Parameters: csIndex (int) – Index of chainset Returns: a tuple Return type: A tuple consisting of (collector, sectionType, conicMethod, rhoType, radius, centerValueTAG, rhoValueTAG). collector is a NXOpen.ScCollector
. The collector for this edge blend chainset sectionType is aNXOpen.Features.EdgeBlendBuilderSection
. The section type of this chain set collector conicMethod is aNXOpen.Features.EdgeBlendBuilderConic
. The conic method of this chain set collector rhoType is aNXOpen.Features.EdgeBlendBuilderRhotype
. The rho type of this chain set collector radius is aNXOpen.Expression
. The radius of this chain set collector centerValueTAG is aNXOpen.Expression
. The conic center value expression of this chain set collector rhoValueTAG is aNXOpen.Expression
. The conic rho value expression of this chain set collectorNew in version NX10.0.3.
License requirements: None.
GetChainsetAndStatus¶
-
EdgeBlendBuilder.
GetChainsetAndStatus
¶ Get collector, radius and validity status for an edge blend chainset given the index of the chainset
Signature
GetChainsetAndStatus(csIndex)
Parameters: csIndex (int) – Index of chainset Returns: a tuple Return type: A tuple consisting of (collector, radius, isValid). collector is a NXOpen.ScCollector
. The collector for this edge blend chainset radius is aNXOpen.Expression
. The radius of this chain set collector isValid is a bool. Is the chainset alive/valid ?New in version NX5.0.0.
License requirements: None.
GetChainsetIndex¶
-
EdgeBlendBuilder.
GetChainsetIndex
¶ Get the index of edge blend chainset given the collector
Signature
GetChainsetIndex(collector)
Parameters: collector ( NXOpen.ScCollector
) – The collector for this edge blend chainsetReturns: Index of chainset, indicating which chainset we are dealing with Return type: int New in version NX4.0.0.
License requirements: None.
GetNewStopshortData¶
-
EdgeBlendBuilder.
GetNewStopshortData
¶ Get an edge blend stop short data for the index provided
Signature
GetNewStopshortData(ssIndex)
Parameters: ssIndex (int) – Index of where stop short data item is created Returns: the Stopshort Data Return type: NXOpen.GeometricUtilities.BlendStopshortBuilder
New in version NX5.0.0.
License requirements: None.
GetNumberOfValidChainsets¶
-
EdgeBlendBuilder.
GetNumberOfValidChainsets
¶ Get the number of valid chainsets
Signature
GetNumberOfValidChainsets()
Returns: Number of valid chainsets Return type: int New in version NX5.0.0.
License requirements: None.
GetSetbackData¶
-
EdgeBlendBuilder.
GetSetbackData
¶ Get an edge blend setback data for the index provided
Signature
GetSetbackData(sbIndex)
Parameters: sbIndex (int) – Index of where setback data item was created. Returns: a tuple Return type: A tuple consisting of (edgeArray, fromStart, distanceExp). edgeArray is a list of NXOpen.Edge
. Array of Edge collector tags that are used by the setback fromStart is a list of bool. if true, then the setback is defined at the start vertex. Otherwise, it is defined at the end vertex. There is one for each output edge. distanceExp is a list ofNXOpen.Expression
. The distance for the setback on each edge.New in version NX4.0.0.
License requirements: None.
GetStopshortData¶
-
EdgeBlendBuilder.
GetStopshortData
¶ Get an edge blend stop short data for the index provided
Signature
GetStopshortData(ssIndex)
Parameters: ssIndex (int) – Index of where stop short data item is created. Returns: a tuple Return type: A tuple consisting of (distanceExp, edge, fromStart). distanceExp is a NXOpen.Expression
. The distance for the stopshort on the edge. edge is aNXOpen.Edge
. Edge the stop short data is on. fromStart is a bool. if true, then the stopshort is defined at the start vertex. Otherwise, it is defined at the end vertex.New in version NX4.0.0.
Deprecated since version NX5.0.0: Use
Features.EdgeBlendBuilder.GetNewStopshortData()
instead.License requirements: None.
GetVariableRadiusData¶
-
EdgeBlendBuilder.
GetVariableRadiusData
¶ Get all the variable radii data for an edge in the edge blend
Signature
GetVariableRadiusData(edge)
Parameters: edge ( NXOpen.Edge
) – Edge to get all the varible radius data onReturns: a tuple Return type: A tuple consisting of (parameter, radiiExp, smartPoints, isExternalFlagArray). parameter is a list of float. Parameter locations of points on the edge radiiExp is a list of NXOpen.Expression
. The radius value of each point on the edge smartPoints is a list ofNXOpen.Point
. Array of smart points defining variable radius isExternalFlagArray is a list of bool. Corresponding is_external flags of the variable radius pointsNew in version NX4.0.0.
Deprecated since version NX6.0.0: Use
Features.EdgeBlendBuilder.GetVariableRadiusDataNew()
instead.License requirements: None.
GetVariableRadiusDataNew¶
-
EdgeBlendBuilder.
GetVariableRadiusDataNew
¶ Get all the variable radii data for an edge in the edge blend
Signature
GetVariableRadiusDataNew(edge)
Parameters: edge ( NXOpen.Edge
) – Edge to get all the varible radius data onReturns: a tuple Return type: A tuple consisting of (parameterExp, radiiExp, smartPoints, isExternalFlagArray). parameterExp is a list of NXOpen.Expression
. Parameter value of points on the edge radiiExp is a list ofNXOpen.Expression
. The radius value of each point on the edge smartPoints is a list ofNXOpen.Point
. Array of smart points defining variable radius isExternalFlagArray is a list of bool. Corresponding is_external flags of the variable radius pointsNew in version NX6.0.0.
License requirements: None.
RemoveChainset¶
-
EdgeBlendBuilder.
RemoveChainset
¶ Delete an edge blend chainset from the edge blend.
Signature
RemoveChainset(csIndex)
Parameters: csIndex (int) – Index of chainset, indicating which chainset we are dealing with New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveChainsetByCollector¶
-
EdgeBlendBuilder.
RemoveChainsetByCollector
¶ Delete an edge blend chainset from the edge blend.
Signature
RemoveChainsetByCollector(collector)
Parameters: collector ( NXOpen.ScCollector
) – The collector for this edge blend chainsetNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveNewStopshortData¶
-
EdgeBlendBuilder.
RemoveNewStopshortData
¶ Remove an edge blend stop short corresponding to a BlendStopshortBuilder
Signature
RemoveNewStopshortData(builder)
Parameters: builder ( NXOpen.GeometricUtilities.BlendStopshortBuilder
) – the Stopshort DataNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveSetbackData¶
-
EdgeBlendBuilder.
RemoveSetbackData
¶ Remove an edge blend setback data for an edge in the edge blend
Signature
RemoveSetbackData(sbIndex)
Parameters: sbIndex (int) – Index of where setback data item was created New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveStopshortData¶
-
EdgeBlendBuilder.
RemoveStopshortData
¶ Overloaded method RemoveStopshortData
RemoveStopshortData(edge, fromStart)
RemoveStopshortData(ssIndex)
-------------------------------------
Remove an edge blend stop short data for an edge
Signature
RemoveStopshortData(edge, fromStart)
Parameters: - edge (
NXOpen.Edge
) – Edge to remove the stopshort on - fromStart (bool) – if true, then the stopshort is defined at the start vertex. Otherwise, it is defined at the end vertex.
New in version NX4.0.0.
Deprecated since version NX5.0.0: Use
Features.EdgeBlendBuilder.RemoveNewStopshortData()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Remove an edge blend stop short data for the index indicated
Signature
RemoveStopshortData(ssIndex)
Parameters: ssIndex (int) – Index of where stop short data item is created. New in version NX4.0.0.
Deprecated since version NX5.0.0: Use
Features.EdgeBlendBuilder.RemoveNewStopshortData()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
RemoveStopshortDataByType¶
-
EdgeBlendBuilder.
RemoveStopshortDataByType
¶ Remove the stop short from an edge, given its type and location
Signature
RemoveStopshortDataByType(edge, fromStart, type)
Parameters: - edge (
NXOpen.Edge
) – Edge to remove the stopshort on - fromStart (bool) – if true, then the stopshort is defined at the start vertex. Otherwise, it is defined at the end vertex.
- type (
NXOpen.GeometricUtilities.BlendStopshortBuilderChoices
) – the type of the stopshort
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- edge (
RemoveVariableRadiusData¶
-
EdgeBlendBuilder.
RemoveVariableRadiusData
¶ Overloaded method RemoveVariableRadiusData
RemoveVariableRadiusData(edge, parameter)
RemoveVariableRadiusData(edge)
-------------------------------------
Remove variable radius data on an edge by the parameter value of the point on the edge
Signature
RemoveVariableRadiusData(edge, parameter)
Parameters: - edge (
NXOpen.Edge
) – Edge to add stop short data on - parameter (float) – Parameter location of point on the edge
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Remove all variable radius datas on an edge
Signature
RemoveVariableRadiusData(edge)
Parameters: edge ( NXOpen.Edge
) – Edge to remove all variable radius datas fromNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
RemoveVariableRadiusDataByIndex¶
-
EdgeBlendBuilder.
RemoveVariableRadiusDataByIndex
¶ Remove variable radius data on an edge by the index into the point array on the edge
Signature
RemoveVariableRadiusDataByIndex(edge, index)
Parameters: - edge (
NXOpen.Edge
) – Edge to remove variable radius data on - index (int) – Index into point array on the edge
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- edge (
Validate¶
-
EdgeBlendBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.