EdgeBlendBuilderSetback Enumeration

NXOpen.Features.EdgeBlendBuilder.Setback is an alias for NXOpen.Features.EdgeBlendBuilderSetback

class NXOpen.Features.EdgeBlendBuilderSetback

Bases: object

This enum represents the Setback option

Enum Members

Enum Member Enum Member Description
IncludeWithCorner
Include with corner
SeparateFromCorner
Separate from corner
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.