EdgeBlendBuilderSection Enumeration

NXOpen.Features.EdgeBlendBuilder.Section is an alias for NXOpen.Features.EdgeBlendBuilderSection

class NXOpen.Features.EdgeBlendBuilderSection

Bases: object

This enum represents the Section option

Enum Members

Enum Member Enum Member Description
Circular
Default option, circular shaped blends
Conic
Conical shaped blends
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.