EdgeBlendBuilderOrderOfBlending Enumeration

NXOpen.Features.EdgeBlendBuilder.OrderOfBlending is an alias for NXOpen.Features.EdgeBlendBuilderOrderOfBlending

class NXOpen.Features.EdgeBlendBuilderOrderOfBlending

Bases: object

This enum represents the order of Blending

Enum Members

Enum Member Enum Member Description
ConvexFirst
Convex first
ConcaveFirst
Concave first
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.