EdgeBlendBuilderOverlap Enumeration

NXOpen.Features.EdgeBlendBuilder.Overlap is an alias for NXOpen.Features.EdgeBlendBuilderOverlap

class NXOpen.Features.EdgeBlendBuilderOverlap

Bases: object

This enum represents the Overlap resolution options for Edge Blend

Enum Members

Enum Member Enum Member Description
MaintainAndIntersect
Maintain Blend and Intersect
DifferentConvexityRollOver
If different convexity,roll over
AnyConvexityRollOver
Any convexity,roll over
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.