InspectionToleranceOperationBuilder Class¶
-
class
NXOpen.CAM.
InspectionToleranceOperationBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
this class creates the tolerance operation
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionToleranceOperationBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CompositeToleranceValueSource | Returns or sets the GDT Composite Lower Tolerance Value Source |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
DatumPlaneFittingModeBuilder | Returns the Datum Plane Fitting Mode Builder |
Description | Returns or sets the description |
DoubleDirVecI | Returns or sets the double dir vec i |
DoubleDirVecJ | Returns or sets the double dir vec j |
DoubleDirVecK | Returns or sets the double dir vec k |
DoubleLower | Returns or sets the lower tolerance |
DoubleLowerParamOuterProfile | Returns or sets the double lower parameter outer profile |
DoubleNominal | Returns or sets the nominal tolerance |
DoubleParamExtArea | Returns or sets the double parameter extent area |
DoubleParamExtLength | Returns or sets the double parameter extent length |
DoubleParamOuterProfile | Returns or sets the double parameter outer profile |
DoubleParamTolValue | Returns or sets the double parameter tolerance value |
DoubleParamTolValue1 | Returns or sets the double parameter tolerance value1 |
DoubleUpper | Returns or sets the upper tolerance |
DoubleViewVecI | Returns or sets the double view vec i |
DoubleViewVecJ | Returns or sets the double view vec j |
DoubleViewVecK | Returns or sets the double view vec k |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
EnumPCSABS | Returns or sets the enum pcsabs |
EnumParamPriMatModifier | Returns or sets the enum parameter primary material modifier |
EnumParamPriMatModifier1 | Returns or sets the enum parameter primary material modifier1 |
EnumParamSecMatModifier | Returns or sets the enum parameter secondary material modifier |
EnumParamSecMatModifier1 | Returns or sets the enum parameter secondary material modifier1 |
EnumParamSubType | Returns or sets the enum parameter sub type |
EnumParamTerMatModifier | Returns or sets the enum parameter tertiary material modifier |
EnumParamTerMatModifier1 | Returns or sets the enum parameter tertiary material modifier1 |
EnumParamTolMatModifier | Returns or sets the enum parameter tolerance material modifier |
EnumParamTolMatModifier1 | Returns or sets the enum parameter tolerance material modifier1 |
EnumParamTolMatModifierDup | Returns or sets the enum parameter tolerance material modifier dup |
EnumParamTolZoneShape | Returns or sets the enum parameter tolerance zone shape |
EnumParamTolZoneShape1 | Returns or sets the enum parameter tolerance zone shape1 |
EnumParamXYZAxis | Returns or sets the enum parameter xyzaxis |
EnumParameterExtent | Returns or sets the enum parameter extent |
EnumTorusCharacteristic | Returns or sets the enum torus characteristic |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
IsAlignVector | Returns or sets the is Align Vector Flag |
IsComposite | Returns or sets the is composite flag |
LayoutAndLayer | Returns the Layer and Layout |
LimitsOfSizeModeBuilder | Returns the Limits of Size Mode Builder |
LowerDMS | Returns or sets the string for anglb upper DMS |
LowerSource | Returns or sets the Lower Value Source |
MotionOutputBuilder | Returns the motion output builder |
NominalDMS | Returns or sets the string for anglb nominal DMS |
NominalSource | Returns or sets the Nominal Value Source |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
ProfileDispositionModeBuilder | Returns the Profile Disposition Mode Builder |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
SelectionFeature | Returns the selection feature |
SelectionOriginFeature | Returns the selection origin feature |
SelectionPMI | Returns the PMI selection |
SelectionTolerancedFeature | Returns the selection toleranced feature |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
StringDatumFeatName | Returns or sets the string datum feat name |
StringDatumLetter | Returns or sets the string datum letter |
StringOriginFeatName | Returns or sets the string origin feat name |
StringPriDatum | Returns or sets the string primary datum |
StringPriDatum1 | Returns or sets the string primary datum1 |
StringSecDatum | Returns or sets the string secondary datum |
StringSecDatum1 | Returns or sets the string secondary datum1 |
StringTerDatum | Returns or sets the string tertiary datum |
StringTerDatum1 | Returns or sets the string tertiary datum1 |
StringTolName | Returns or sets the string tolerance name |
StringTolerancedFeat | Returns or sets the string toleranced feat |
SurfaceProfileModeBuilder | Returns the Surface Profile Mode Builder |
Tag | Returns the Tag for this object. |
TolOpType | Returns or sets the tolerance type |
ToleranceValueSource | Returns or sets the GDT Tolerance Value Source |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
UpperDMS | Returns or sets the string for anglb upper DMS |
UpperSource | Returns or sets the Upper Value Source |
UseDegMin | Returns or sets the deg/min flag for angle between |
VectorDirection | Returns or sets the vector direction |
VectorViewVec | Returns or sets the vector view vec |
XRotationDOFMode | Returns or sets the x rotation dofmode |
XRotationLowerLimit | Returns or sets the x rotation lower limit |
XRotationUpperLimit | Returns or sets the x rotation upper limit |
XTranslationDOFMode | Returns or sets the x translation dofmode |
XTranslationLowerLimit | Returns or sets the x translation lower limit |
XTranslationUpperLimit | Returns or sets the x translation upper limit |
YRotationDOFMode | Returns or sets the y rotation dofmode |
YRotationLowerLimit | Returns or sets the y rotation lower limit |
YRotationUpperLimit | Returns or sets the y rotation upper limit |
YTranslationDOFMode | Returns or sets the y translation dofmode |
YTranslationLowerLimit | Returns or sets the y translation lower limit |
YTranslationUpperLimit | Returns or sets the y translation upper limit |
ZRotationDOFMode | Returns or sets the z rotation dofmode |
ZRotationLowerLimit | Returns or sets the z rotation lower limit |
ZRotationUpperLimit | Returns or sets the z rotation upper limit |
ZTranslationDOFMode | Returns or sets the z translation dofmode |
ZTranslationLowerLimit | Returns or sets the z translation lower limit |
ZTranslationUpperLimit | Returns or sets the z translation upper limit |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateParameters | Updates Inspection tolerance parameters based on selected annotation. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
CompositeToleranceValueSource¶
-
InspectionToleranceOperationBuilder.
CompositeToleranceValueSource
¶ Returns or sets the GDT Composite Lower Tolerance Value Source
-------------------------------------
Getter Method
Signature
CompositeToleranceValueSource()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
CompositeToleranceValueSource(compositeToleranceValueSource)
Parameters: compositeToleranceValueSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DatumPlaneFittingModeBuilder¶
-
InspectionToleranceOperationBuilder.
DatumPlaneFittingModeBuilder
¶ Returns the Datum Plane Fitting Mode Builder
-------------------------------------
Getter Method
Signature
DatumPlaneFittingModeBuilder()
Returns: Return type: NXOpen.CAM.InspectionDatumPlaneFittingModeBuilder
New in version NX9.0.0.
License requirements: None.
DoubleDirVecI¶
-
InspectionToleranceOperationBuilder.
DoubleDirVecI
¶ Returns or sets the double dir vec i
-------------------------------------
Getter Method
Signature
DoubleDirVecI()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleDirVecI(doubleDirVecI)
Parameters: doubleDirVecI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleDirVecJ¶
-
InspectionToleranceOperationBuilder.
DoubleDirVecJ
¶ Returns or sets the double dir vec j
-------------------------------------
Getter Method
Signature
DoubleDirVecJ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleDirVecJ(doubleDirVecJ)
Parameters: doubleDirVecJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleDirVecK¶
-
InspectionToleranceOperationBuilder.
DoubleDirVecK
¶ Returns or sets the double dir vec k
-------------------------------------
Getter Method
Signature
DoubleDirVecK()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleDirVecK(doubleDirVecK)
Parameters: doubleDirVecK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleLower¶
-
InspectionToleranceOperationBuilder.
DoubleLower
¶ Returns or sets the lower tolerance
-------------------------------------
Getter Method
Signature
DoubleLower()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleLower(doubleLower)
Parameters: doubleLower (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleLowerParamOuterProfile¶
-
InspectionToleranceOperationBuilder.
DoubleLowerParamOuterProfile
¶ Returns or sets the double lower parameter outer profile
-------------------------------------
Getter Method
Signature
DoubleLowerParamOuterProfile()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleLowerParamOuterProfile(doubleLowerParamOuterProfile)
Parameters: doubleLowerParamOuterProfile (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleNominal¶
-
InspectionToleranceOperationBuilder.
DoubleNominal
¶ Returns or sets the nominal tolerance
-------------------------------------
Getter Method
Signature
DoubleNominal()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleNominal(doubleNominal)
Parameters: doubleNominal (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamExtArea¶
-
InspectionToleranceOperationBuilder.
DoubleParamExtArea
¶ Returns or sets the double parameter extent area
-------------------------------------
Getter Method
Signature
DoubleParamExtArea()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamExtArea(doubleParamExtArea)
Parameters: doubleParamExtArea (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamExtLength¶
-
InspectionToleranceOperationBuilder.
DoubleParamExtLength
¶ Returns or sets the double parameter extent length
-------------------------------------
Getter Method
Signature
DoubleParamExtLength()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamExtLength(doubleParamExtLength)
Parameters: doubleParamExtLength (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamOuterProfile¶
-
InspectionToleranceOperationBuilder.
DoubleParamOuterProfile
¶ Returns or sets the double parameter outer profile
-------------------------------------
Getter Method
Signature
DoubleParamOuterProfile()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamOuterProfile(doubleParamOuterProfile)
Parameters: doubleParamOuterProfile (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamTolValue¶
-
InspectionToleranceOperationBuilder.
DoubleParamTolValue
¶ Returns or sets the double parameter tolerance value
-------------------------------------
Getter Method
Signature
DoubleParamTolValue()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamTolValue(doubleParamTolValue)
Parameters: doubleParamTolValue (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamTolValue1¶
-
InspectionToleranceOperationBuilder.
DoubleParamTolValue1
¶ Returns or sets the double parameter tolerance value1
-------------------------------------
Getter Method
Signature
DoubleParamTolValue1()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamTolValue1(doubleParamTolValue1)
Parameters: doubleParamTolValue1 (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleUpper¶
-
InspectionToleranceOperationBuilder.
DoubleUpper
¶ Returns or sets the upper tolerance
-------------------------------------
Getter Method
Signature
DoubleUpper()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleUpper(doubleUpper)
Parameters: doubleUpper (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleViewVecI¶
-
InspectionToleranceOperationBuilder.
DoubleViewVecI
¶ Returns or sets the double view vec i
-------------------------------------
Getter Method
Signature
DoubleViewVecI()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleViewVecI(doubleViewVecI)
Parameters: doubleViewVecI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleViewVecJ¶
-
InspectionToleranceOperationBuilder.
DoubleViewVecJ
¶ Returns or sets the double view vec j
-------------------------------------
Getter Method
Signature
DoubleViewVecJ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleViewVecJ(doubleViewVecJ)
Parameters: doubleViewVecJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleViewVecK¶
-
InspectionToleranceOperationBuilder.
DoubleViewVecK
¶ Returns or sets the double view vec k
-------------------------------------
Getter Method
Signature
DoubleViewVecK()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleViewVecK(doubleViewVecK)
Parameters: doubleViewVecK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumPCSABS¶
-
InspectionToleranceOperationBuilder.
EnumPCSABS
¶ Returns or sets the enum pcsabs
-------------------------------------
Getter Method
Signature
EnumPCSABS()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderSirVecPCSABS
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumPCSABS(enumPCSABS)
Parameters: enumPCSABS ( NXOpen.CAM.InspectionToleranceOperationBuilderSirVecPCSABS
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamPriMatModifier¶
-
InspectionToleranceOperationBuilder.
EnumParamPriMatModifier
¶ Returns or sets the enum parameter primary material modifier
-------------------------------------
Getter Method
Signature
EnumParamPriMatModifier()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamPriMatModifier(enumParamPriMatModifier)
Parameters: enumParamPriMatModifier ( NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamPriMatModifier1¶
-
InspectionToleranceOperationBuilder.
EnumParamPriMatModifier1
¶ Returns or sets the enum parameter primary material modifier1
-------------------------------------
Getter Method
Signature
EnumParamPriMatModifier1()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamPriMatModifier1(enumParamPriMatModifier1)
Parameters: enumParamPriMatModifier1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamSecMatModifier¶
-
InspectionToleranceOperationBuilder.
EnumParamSecMatModifier
¶ Returns or sets the enum parameter secondary material modifier
-------------------------------------
Getter Method
Signature
EnumParamSecMatModifier()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamSecMatModifier(enumParamSecMatModifier)
Parameters: enumParamSecMatModifier ( NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamSecMatModifier1¶
-
InspectionToleranceOperationBuilder.
EnumParamSecMatModifier1
¶ Returns or sets the enum parameter secondary material modifier1
-------------------------------------
Getter Method
Signature
EnumParamSecMatModifier1()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamSecMatModifier1(enumParamSecMatModifier1)
Parameters: enumParamSecMatModifier1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamSubType¶
-
InspectionToleranceOperationBuilder.
EnumParamSubType
¶ Returns or sets the enum parameter sub type
-------------------------------------
Getter Method
Signature
EnumParamSubType()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamSubType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamSubType(enumParamSubType)
Parameters: enumParamSubType ( NXOpen.CAM.InspectionToleranceOperationBuilderParamSubType
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTerMatModifier¶
-
InspectionToleranceOperationBuilder.
EnumParamTerMatModifier
¶ Returns or sets the enum parameter tertiary material modifier
-------------------------------------
Getter Method
Signature
EnumParamTerMatModifier()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTerDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTerMatModifier(enumParamTerMatModifier)
Parameters: enumParamTerMatModifier ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTerDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTerMatModifier1¶
-
InspectionToleranceOperationBuilder.
EnumParamTerMatModifier1
¶ Returns or sets the enum parameter tertiary material modifier1
-------------------------------------
Getter Method
Signature
EnumParamTerMatModifier1()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTerDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTerMatModifier1(enumParamTerMatModifier1)
Parameters: enumParamTerMatModifier1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTerDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolMatModifier¶
-
InspectionToleranceOperationBuilder.
EnumParamTolMatModifier
¶ Returns or sets the enum parameter tolerance material modifier
-------------------------------------
Getter Method
Signature
EnumParamTolMatModifier()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolMatModifier(enumParamTolMatModifier)
Parameters: enumParamTolMatModifier ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolMatModifier1¶
-
InspectionToleranceOperationBuilder.
EnumParamTolMatModifier1
¶ Returns or sets the enum parameter tolerance material modifier1
-------------------------------------
Getter Method
Signature
EnumParamTolMatModifier1()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolMatModifier1(enumParamTolMatModifier1)
Parameters: enumParamTolMatModifier1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolMatModifierDup¶
-
InspectionToleranceOperationBuilder.
EnumParamTolMatModifierDup
¶ Returns or sets the enum parameter tolerance material modifier dup
-------------------------------------
Getter Method
Signature
EnumParamTolMatModifierDup()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifierDup
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolMatModifierDup(enumParamTolMatModifierDup)
Parameters: enumParamTolMatModifierDup ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifierDup
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolZoneShape¶
-
InspectionToleranceOperationBuilder.
EnumParamTolZoneShape
¶ Returns or sets the enum parameter tolerance zone shape
-------------------------------------
Getter Method
Signature
EnumParamTolZoneShape()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolZoneShape
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolZoneShape(enumParamTolZoneShape)
Parameters: enumParamTolZoneShape ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolZoneShape
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolZoneShape1¶
-
InspectionToleranceOperationBuilder.
EnumParamTolZoneShape1
¶ Returns or sets the enum parameter tolerance zone shape1
-------------------------------------
Getter Method
Signature
EnumParamTolZoneShape1()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolZoneShape
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolZoneShape1(enumParamTolZoneShape1)
Parameters: enumParamTolZoneShape1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolZoneShape
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamXYZAxis¶
-
InspectionToleranceOperationBuilder.
EnumParamXYZAxis
¶ Returns or sets the enum parameter xyzaxis
-------------------------------------
Getter Method
Signature
EnumParamXYZAxis()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamXYZAxis
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamXYZAxis(enumParamXYZAxis)
Parameters: enumParamXYZAxis ( NXOpen.CAM.InspectionToleranceOperationBuilderParamXYZAxis
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParameterExtent¶
-
InspectionToleranceOperationBuilder.
EnumParameterExtent
¶ Returns or sets the enum parameter extent
-------------------------------------
Getter Method
Signature
EnumParameterExtent()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamExtent
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParameterExtent(enumParameterExtent)
Parameters: enumParameterExtent ( NXOpen.CAM.InspectionToleranceOperationBuilderParamExtent
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumTorusCharacteristic¶
-
InspectionToleranceOperationBuilder.
EnumTorusCharacteristic
¶ Returns or sets the enum torus characteristic
-------------------------------------
Getter Method
Signature
EnumTorusCharacteristic()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamXYZAxis
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumTorusCharacteristic(enumTorusCharacteristic)
Parameters: enumTorusCharacteristic ( NXOpen.CAM.InspectionToleranceOperationBuilderParamXYZAxis
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IsAlignVector¶
-
InspectionToleranceOperationBuilder.
IsAlignVector
¶ Returns or sets the is Align Vector Flag
-------------------------------------
Getter Method
Signature
IsAlignVector()
Returns: Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsAlignVector(isAlignVector)
Parameters: isAlignVector (bool) – New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IsComposite¶
-
InspectionToleranceOperationBuilder.
IsComposite
¶ Returns or sets the is composite flag
-------------------------------------
Getter Method
Signature
IsComposite()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsComposite(isComposite)
Parameters: isComposite (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LimitsOfSizeModeBuilder¶
-
InspectionToleranceOperationBuilder.
LimitsOfSizeModeBuilder
¶ Returns the Limits of Size Mode Builder
-------------------------------------
Getter Method
Signature
LimitsOfSizeModeBuilder()
Returns: Return type: NXOpen.CAM.InspectionLimitsOfSizeModeBuilder
New in version NX9.0.0.
License requirements: None.
LowerDMS¶
-
InspectionToleranceOperationBuilder.
LowerDMS
¶ Returns or sets the string for anglb upper DMS
-------------------------------------
Getter Method
Signature
LowerDMS()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerDMS(stringLowerDMS)
Parameters: stringLowerDMS (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LowerSource¶
-
InspectionToleranceOperationBuilder.
LowerSource
¶ Returns or sets the Lower Value Source
-------------------------------------
Getter Method
Signature
LowerSource()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerSource(lowerSource)
Parameters: lowerSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NominalDMS¶
-
InspectionToleranceOperationBuilder.
NominalDMS
¶ Returns or sets the string for anglb nominal DMS
-------------------------------------
Getter Method
Signature
NominalDMS()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NominalDMS(stringNominalDMS)
Parameters: stringNominalDMS (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NominalSource¶
-
InspectionToleranceOperationBuilder.
NominalSource
¶ Returns or sets the Nominal Value Source
-------------------------------------
Getter Method
Signature
NominalSource()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
NominalSource(nominalSource)
Parameters: nominalSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProfileDispositionModeBuilder¶
-
InspectionToleranceOperationBuilder.
ProfileDispositionModeBuilder
¶ Returns the Profile Disposition Mode Builder
-------------------------------------
Getter Method
Signature
ProfileDispositionModeBuilder()
Returns: Return type: NXOpen.CAM.InspectionProfileDispositionModeBuilder
New in version NX9.0.0.
License requirements: None.
SelectionFeature¶
-
InspectionToleranceOperationBuilder.
SelectionFeature
¶ Returns the selection feature
-------------------------------------
Getter Method
Signature
SelectionFeature()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
SelectionOriginFeature¶
-
InspectionToleranceOperationBuilder.
SelectionOriginFeature
¶ Returns the selection origin feature
-------------------------------------
Getter Method
Signature
SelectionOriginFeature()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
SelectionPMI¶
-
InspectionToleranceOperationBuilder.
SelectionPMI
¶ Returns the PMI selection
-------------------------------------
Getter Method
Signature
SelectionPMI()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
SelectionTolerancedFeature¶
-
InspectionToleranceOperationBuilder.
SelectionTolerancedFeature
¶ Returns the selection toleranced feature
-------------------------------------
Getter Method
Signature
SelectionTolerancedFeature()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
StringDatumFeatName¶
-
InspectionToleranceOperationBuilder.
StringDatumFeatName
¶ Returns or sets the string datum feat name
-------------------------------------
Getter Method
Signature
StringDatumFeatName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringDatumFeatName(stringDatumFeatName)
Parameters: stringDatumFeatName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringDatumLetter¶
-
InspectionToleranceOperationBuilder.
StringDatumLetter
¶ Returns or sets the string datum letter
-------------------------------------
Getter Method
Signature
StringDatumLetter()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringDatumLetter(stringDatumLetter)
Parameters: stringDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringOriginFeatName¶
-
InspectionToleranceOperationBuilder.
StringOriginFeatName
¶ Returns or sets the string origin feat name
-------------------------------------
Getter Method
Signature
StringOriginFeatName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringOriginFeatName(stringOriginFeatName)
Parameters: stringOriginFeatName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringPriDatum¶
-
InspectionToleranceOperationBuilder.
StringPriDatum
¶ Returns or sets the string primary datum
-------------------------------------
Getter Method
Signature
StringPriDatum()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringPriDatum(stringPriDatum)
Parameters: stringPriDatum (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringPriDatum1¶
-
InspectionToleranceOperationBuilder.
StringPriDatum1
¶ Returns or sets the string primary datum1
-------------------------------------
Getter Method
Signature
StringPriDatum1()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringPriDatum1(stringPriDatum1)
Parameters: stringPriDatum1 (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringSecDatum¶
-
InspectionToleranceOperationBuilder.
StringSecDatum
¶ Returns or sets the string secondary datum
-------------------------------------
Getter Method
Signature
StringSecDatum()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringSecDatum(stringSecDatum)
Parameters: stringSecDatum (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringSecDatum1¶
-
InspectionToleranceOperationBuilder.
StringSecDatum1
¶ Returns or sets the string secondary datum1
-------------------------------------
Getter Method
Signature
StringSecDatum1()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringSecDatum1(stringSecDatum1)
Parameters: stringSecDatum1 (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringTerDatum¶
-
InspectionToleranceOperationBuilder.
StringTerDatum
¶ Returns or sets the string tertiary datum
-------------------------------------
Getter Method
Signature
StringTerDatum()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringTerDatum(stringTerDatum)
Parameters: stringTerDatum (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringTerDatum1¶
-
InspectionToleranceOperationBuilder.
StringTerDatum1
¶ Returns or sets the string tertiary datum1
-------------------------------------
Getter Method
Signature
StringTerDatum1()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringTerDatum1(stringTerDatum1)
Parameters: stringTerDatum1 (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringTolName¶
-
InspectionToleranceOperationBuilder.
StringTolName
¶ Returns or sets the string tolerance name
-------------------------------------
Getter Method
Signature
StringTolName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringTolName(stringTolName)
Parameters: stringTolName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringTolerancedFeat¶
-
InspectionToleranceOperationBuilder.
StringTolerancedFeat
¶ Returns or sets the string toleranced feat
-------------------------------------
Getter Method
Signature
StringTolerancedFeat()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringTolerancedFeat(stringTolerancedFeat)
Parameters: stringTolerancedFeat (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SurfaceProfileModeBuilder¶
-
InspectionToleranceOperationBuilder.
SurfaceProfileModeBuilder
¶ Returns the Surface Profile Mode Builder
-------------------------------------
Getter Method
Signature
SurfaceProfileModeBuilder()
Returns: Return type: NXOpen.CAM.InspectionSurfaceProfileModeBuilder
New in version NX9.0.0.
License requirements: None.
TolOpType¶
-
InspectionToleranceOperationBuilder.
TolOpType
¶ Returns or sets the tolerance type
-------------------------------------
Getter Method
Signature
TolOpType()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderTolType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolOpType(tolOpType)
Parameters: tolOpType ( NXOpen.CAM.InspectionToleranceOperationBuilderTolType
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ToleranceValueSource¶
-
InspectionToleranceOperationBuilder.
ToleranceValueSource
¶ Returns or sets the GDT Tolerance Value Source
-------------------------------------
Getter Method
Signature
ToleranceValueSource()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToleranceValueSource(toleranceValueSource)
Parameters: toleranceValueSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpperDMS¶
-
InspectionToleranceOperationBuilder.
UpperDMS
¶ Returns or sets the string for anglb upper DMS
-------------------------------------
Getter Method
Signature
UpperDMS()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperDMS(stringUpperDMS)
Parameters: stringUpperDMS (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpperSource¶
-
InspectionToleranceOperationBuilder.
UpperSource
¶ Returns or sets the Upper Value Source
-------------------------------------
Getter Method
Signature
UpperSource()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperSource(upperSource)
Parameters: upperSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UseDegMin¶
-
InspectionToleranceOperationBuilder.
UseDegMin
¶ Returns or sets the deg/min flag for angle between
-------------------------------------
Getter Method
Signature
UseDegMin()
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderAngleFormat
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseDegMin(useDegMinSec)
Parameters: useDegMinSec ( NXOpen.CAM.InspectionToleranceOperationBuilderAngleFormat
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VectorDirection¶
-
InspectionToleranceOperationBuilder.
VectorDirection
¶ Returns or sets the vector direction
-------------------------------------
Getter Method
Signature
VectorDirection()
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorDirection(vectorDirection)
Parameters: vectorDirection ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VectorViewVec¶
-
InspectionToleranceOperationBuilder.
VectorViewVec
¶ Returns or sets the vector view vec
-------------------------------------
Getter Method
Signature
VectorViewVec()
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorViewVec(vectorViewVec)
Parameters: vectorViewVec ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XRotationDOFMode¶
-
InspectionToleranceOperationBuilder.
XRotationDOFMode
¶ Returns or sets the x rotation dofmode
-------------------------------------
Getter Method
Signature
XRotationDOFMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XRotationDOFMode(xRotationDOFMode)
Parameters: xRotationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XRotationLowerLimit¶
-
InspectionToleranceOperationBuilder.
XRotationLowerLimit
¶ Returns or sets the x rotation lower limit
-------------------------------------
Getter Method
Signature
XRotationLowerLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XRotationLowerLimit(xRotationLowerLimit)
Parameters: xRotationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XRotationUpperLimit¶
-
InspectionToleranceOperationBuilder.
XRotationUpperLimit
¶ Returns or sets the x rotation upper limit
-------------------------------------
Getter Method
Signature
XRotationUpperLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XRotationUpperLimit(xRotationUpperLimit)
Parameters: xRotationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XTranslationDOFMode¶
-
InspectionToleranceOperationBuilder.
XTranslationDOFMode
¶ Returns or sets the x translation dofmode
-------------------------------------
Getter Method
Signature
XTranslationDOFMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XTranslationDOFMode(xTranslationDOFMode)
Parameters: xTranslationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XTranslationLowerLimit¶
-
InspectionToleranceOperationBuilder.
XTranslationLowerLimit
¶ Returns or sets the x translation lower limit
-------------------------------------
Getter Method
Signature
XTranslationLowerLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XTranslationLowerLimit(xTranslationLowerLimit)
Parameters: xTranslationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XTranslationUpperLimit¶
-
InspectionToleranceOperationBuilder.
XTranslationUpperLimit
¶ Returns or sets the x translation upper limit
-------------------------------------
Getter Method
Signature
XTranslationUpperLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XTranslationUpperLimit(xTranslationUpperLimit)
Parameters: xTranslationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YRotationDOFMode¶
-
InspectionToleranceOperationBuilder.
YRotationDOFMode
¶ Returns or sets the y rotation dofmode
-------------------------------------
Getter Method
Signature
YRotationDOFMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YRotationDOFMode(yRotationDOFMode)
Parameters: yRotationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YRotationLowerLimit¶
-
InspectionToleranceOperationBuilder.
YRotationLowerLimit
¶ Returns or sets the y rotation lower limit
-------------------------------------
Getter Method
Signature
YRotationLowerLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YRotationLowerLimit(yRotationLowerLimit)
Parameters: yRotationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YRotationUpperLimit¶
-
InspectionToleranceOperationBuilder.
YRotationUpperLimit
¶ Returns or sets the y rotation upper limit
-------------------------------------
Getter Method
Signature
YRotationUpperLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YRotationUpperLimit(yRotationUpperLimit)
Parameters: yRotationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YTranslationDOFMode¶
-
InspectionToleranceOperationBuilder.
YTranslationDOFMode
¶ Returns or sets the y translation dofmode
-------------------------------------
Getter Method
Signature
YTranslationDOFMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YTranslationDOFMode(yTranslationDOFMode)
Parameters: yTranslationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YTranslationLowerLimit¶
-
InspectionToleranceOperationBuilder.
YTranslationLowerLimit
¶ Returns or sets the y translation lower limit
-------------------------------------
Getter Method
Signature
YTranslationLowerLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YTranslationLowerLimit(yTranslationLowerLimit)
Parameters: yTranslationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YTranslationUpperLimit¶
-
InspectionToleranceOperationBuilder.
YTranslationUpperLimit
¶ Returns or sets the y translation upper limit
-------------------------------------
Getter Method
Signature
YTranslationUpperLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YTranslationUpperLimit(yTranslationUpperLimit)
Parameters: yTranslationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZRotationDOFMode¶
-
InspectionToleranceOperationBuilder.
ZRotationDOFMode
¶ Returns or sets the z rotation dofmode
-------------------------------------
Getter Method
Signature
ZRotationDOFMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZRotationDOFMode(zRotationDOFMode)
Parameters: zRotationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZRotationLowerLimit¶
-
InspectionToleranceOperationBuilder.
ZRotationLowerLimit
¶ Returns or sets the z rotation lower limit
-------------------------------------
Getter Method
Signature
ZRotationLowerLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZRotationLowerLimit(zRotationLowerLimit)
Parameters: zRotationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZRotationUpperLimit¶
-
InspectionToleranceOperationBuilder.
ZRotationUpperLimit
¶ Returns or sets the z rotation upper limit
-------------------------------------
Getter Method
Signature
ZRotationUpperLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZRotationUpperLimit(zRotationUpperLimit)
Parameters: zRotationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZTranslationDOFMode¶
-
InspectionToleranceOperationBuilder.
ZTranslationDOFMode
¶ Returns or sets the z translation dofmode
-------------------------------------
Getter Method
Signature
ZTranslationDOFMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZTranslationDOFMode(zTranslationDOFMode)
Parameters: zTranslationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZTranslationLowerLimit¶
-
InspectionToleranceOperationBuilder.
ZTranslationLowerLimit
¶ Returns or sets the z translation lower limit
-------------------------------------
Getter Method
Signature
ZTranslationLowerLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZTranslationLowerLimit(zTranslationLowerLimit)
Parameters: zTranslationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZTranslationUpperLimit¶
-
InspectionToleranceOperationBuilder.
ZTranslationUpperLimit
¶ Returns or sets the z translation upper limit
-------------------------------------
Getter Method
Signature
ZTranslationUpperLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZTranslationUpperLimit(zTranslationUpperLimit)
Parameters: zTranslationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
UpdateParameters¶
-
InspectionToleranceOperationBuilder.
UpdateParameters
¶ Updates Inspection tolerance parameters based on selected annotation.
Signature
UpdateParameters()
New in version NX7.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionToleranceOperationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.