InspectionToleranceOperationBuilderToleranceSource Enumeration

NXOpen.CAM.InspectionToleranceOperationBuilder.ToleranceSource is an alias for NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource

class NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource

Bases: object

Tolerance Source

Enum Members

Enum Member Enum Member Description
Unknown
Unknown Source
Pmi
PMI
CheckedGdt
Checked Gdt
Geometry
Geometry
TwoDAnnot
2D Annotation
User
User
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.