InspectionToleranceOperationBuilderTolType Enumeration¶
NXOpen.CAM.InspectionToleranceOperationBuilder.TolType is an alias for NXOpen.CAM.InspectionToleranceOperationBuilderTolType
-
class
NXOpen.CAM.
InspectionToleranceOperationBuilderTolType
¶ Bases:
object
Tolerance types
Enum Members
Enum Member Enum Member Description DistanceBetween Distance BetweenAngleBetween Angle BetweenCoordinateTolerance CoordinateDiameter DiameterRadius RadiusWidth WidthConeAngle Angle of ConeDatumDefinition Datum DefinitionFlatness FlatnessStraightness StraightnessCircularity CircularityCylindricity CylindricityLineProfile Profile of LineSurfaceProfile Profile of SurfaceAngularity AngularityParallelism ParallelismPerpendicularity PerpendicularityPosition PositionConcentricity ConcentricitySymmetry SymmetryCircularRunout Circular RunoutTotalRunout Total RunoutDatumTarget -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-