InspectionToleranceOperationBuilderParamSubType Enumeration

NXOpen.CAM.InspectionToleranceOperationBuilder.ParamSubType is an alias for NXOpen.CAM.InspectionToleranceOperationBuilderParamSubType

class NXOpen.CAM.InspectionToleranceOperationBuilderParamSubType

Bases: object

Subtypes

Enum Members

Enum Member Enum Member Description
Surface
Surface
Axis
Axis
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.