InspectionToleranceOperationBuilderParamSecDatum Enumeration

NXOpen.CAM.InspectionToleranceOperationBuilder.ParamSecDatum is an alias for NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatum

class NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatum

Bases: object

Default datum symbols

Enum Members

Enum Member Enum Member Description
A
A
B
B
C
C
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.