InspectionLimitsOfSizeModeBuilder Class

class NXOpen.CAM.InspectionLimitsOfSizeModeBuilder

Bases: NXOpen.CAM.InheritableBuilder

Represents a builder for an inheritable limits of size mode enum value

New in version NX8.5.1.

Properties

Property Description
InheritanceStatus Returns or sets the inheritance status
Tag Returns the Tag for this object.
Value Returns or sets the current limits of size mode

Methods

Property Detail

Value

InspectionLimitsOfSizeModeBuilder.Value

Returns or sets the current limits of size mode

-------------------------------------

Getter Method

Signature Value()

Returns:the current limits of size mode
Return type:NXOpen.CAM.InspectionMethodBuilderLimitsOfSizeTypes

New in version NX8.5.1.

License requirements: None.

-------------------------------------

Setter Method

Signature Value(itemValue)

Parameters:itemValue (NXOpen.CAM.InspectionMethodBuilderLimitsOfSizeTypes) – the new limits of size mode

New in version NX8.5.1.

License requirements: insp_programming (“INSPECTION PROGRAMMING”)