InheritableBuilder Class¶
-
class
NXOpen.CAM.
InheritableBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a builder for an inheritable value in of a CAM.
CAMObject .. versionadded:: NX6.0.0
Properties¶
Property | Description |
---|---|
InheritanceStatus | Returns or sets the inheritance status |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
InheritanceStatus¶
-
InheritableBuilder.
InheritanceStatus
¶ Returns or sets the inheritance status
-------------------------------------
Getter Method
Signature
InheritanceStatus()
Returns: the inheritance status Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritanceStatus(isInherited)
Parameters: isInherited (bool) – the inheritance status New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)