Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.userdefinedtemplate |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Arc
Represents an arc curve.
|
interface |
Conic
Represents a conic curve.
|
interface |
Curve
Represents a curve.
|
interface |
Edge
|
interface |
Ellipse
Represents an ellipse curve.
|
interface |
Face
Represents a face .
|
interface |
Hyperbola
Represents a hyperbola curve.
|
interface |
InfiniteLine
Represents a infinite line curve.
|
interface |
Line
Represents a line curve.
|
interface |
Parabola
Represents a parabola curve.
|
interface |
Polyline
Represents a polyline curve.
|
interface |
Sketch
Represents a sketch
Use the SketchCollection class to create a sketch. |
interface |
Spline
Represents a spline curve.
|
Modifier and Type | Field and Description |
---|---|
IProfile |
Tip.MapEdgeData.dieEdge |
IProfile |
Tip.MapEdgeData.partEdge |
IProfile[] |
TrimTaskBuilder.TrimBoundsData.profileEntries
Profile entries that make up the
boundary of the trim task
|
IProfile[] |
SteelInsertBuilder.MainProfileData.profileEntries
profile entries
|
IProfile[] |
RotorBuilder.FlangeBendProfileData.profileEntries
The profile entries, will be curves, edges, faces, sketches or curve features.
|
IProfile[] |
RibChildBuilder.CenterlineData.profileEntries
The profile entries, will be curves, edges, faces, sketches or curve features.
|
IProfile[] |
PierceTaskBuilder.PierceBoundsData.profileEntries
Profile entries that make up the
boundary of the pierce task
|
IProfile[] |
PierceHoleChildBuilder.PierceHoleShapeData.profileEntries
profile entries
|
IProfile[] |
PadChildBuilder.ShapeData.profileEntries
The profile entries, will be curves, edges, faces, sketches or curve features.
|
IProfile[] |
FormTaskBuilder.RegionBoundsData.profileEntries
The profile entries, will be curves, edges, faces, sketches or curve features.
|
IProfile[] |
FlangeTaskBuilder.RegionBoundsData.profileEntries
Profile entries that make up the
boundary of the flange task
|
IProfile[] |
FillBuilder.RegionBoundsData.profileEntries
profile entries
|
IProfile[] |
DrawDiePunchBuilder.PunchProfileData.profileEntries
The profile entries, will be curves, edges, faces, sketches or curve features.
|
IProfile[] |
DeckParentBuilder.MainDeckData.profileEntries
The profile entries, will be curves, edges, faces, sketches or curve features.
|
IProfile[] |
ConnectProfileParentBuilder.ProfileData.profileEntries
profile entries
|
IProfile[] |
CastReliefParentBuilder.CastReliefData.profileEntries
The profile entries, will be curves, edges, faces, sketches or curve features.
|
Modifier and Type | Method and Description |
---|---|
IProfile[] |
PierceItemBuilder.getPierceObjects()
Gets the objects making up the hole to be pierced.
|
Modifier and Type | Method and Description |
---|---|
Tip.MapEdgeData |
Tip.mapEdge(IProfile inEdge)
Maps the edge to find the part and die position entity, either can be a null.
|
void |
DeckParentBuilder.setBaseFlange(DirectionOption direction,
IProfile[] profileEntries)
Sets the base flange profile of the draw die punch.
|
void |
DeckParentBuilder.setBinderEdge(DirectionOption direction,
IProfile[] profileEntries)
Sets the binder edge profile of the upper draw die deck.
|
void |
RibChildBuilder.setBottomEndByProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the bottom end limit geometry of the die rib using a profile.
|
void |
PierceHoleChildBuilder.setBreakerHoleShape(DirectionOption direction,
IProfile[] profileEntries)
Sets the breaker hole shape of the pierce hole
License requirements: ug_die_design ("Die Design") . |
void |
CastReliefParentBuilder.setCastRelief(DirectionOption direction,
IProfile[] profileEntries)
Sets the profile of the cast relief.
|
void |
RibChildBuilder.setCenterline(DirectionOption direction,
IProfile[] profileEntries)
Sets the centerline of the rib.
|
void |
RotorBuilder.setEndOfFlangeProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the end of flange profile of the die rotor casting.
|
void |
RotorBuilder.setFlangeBendProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the flange bend profile of the rotor casting.
|
void |
SteelInsertBuilder.setFlangeEndProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the flange end profile of the steel insert
License requirements: ug_die_design ("Die Design") . |
void |
DeckParentBuilder.setIntermediateDeck(DirectionOption direction,
IProfile[] profileEntries)
Sets the intermediate deck profile of the deck.
|
void |
DeckParentBuilder.setMainDeck(DirectionOption direction,
IProfile[] profileEntries)
Sets the main deck profile of the upper draw die deck.
|
void |
SteelInsertBuilder.setMainProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the main profile of the steel insert
License requirements: ug_die_design ("Die Design") . |
void |
DeckParentBuilder.setMainWallCenterline(DirectionOption direction,
IProfile[] profileEntries)
Sets the main wall centerline profile of the draw die punch.
|
void |
PierceTaskBuilder.setPierceBounds(DirectionOption direction,
IProfile[] profileEntries)
Sets the pierce bounds of the pierce task.
|
void |
PierceHoleChildBuilder.setPierceHoleShape(DirectionOption direction,
IProfile[] profileEntries)
Sets the shape of the pierce hole
License requirements: ug_die_design ("Die Design") . |
void |
PierceItemBuilder.setPierceObjects(IProfile[] objects)
Sets the objects making up the hole to be pierced.
|
void |
ConnectProfileParentBuilder.setProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the connecting profiles of the steel insert
License requirements: ug_die_design ("Die Design") . |
void |
DrawDiePunchBuilder.setPunchProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the punch profile of the draw die punch casting.
|
void |
FormTaskBuilder.setRegionBounds(DirectionOption direction,
IProfile[] profileEntries)
Sets the region bounds of the form task.
|
void |
FlangeTaskBuilder.setRegionBounds(DirectionOption direction,
IProfile[] profileEntries)
Sets the region bounds of the flange task
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
FillBuilder.setRegionBounds(DirectionOption direction,
IProfile[] profileEntries)
Sets the region bounds of the area fill
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
PadChildBuilder.setShape(DirectionOption direction,
IProfile[] profileEntries)
Sets the shape profile of the die pad.
|
void |
FormTaskBuilder.setShapeDetailByProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the shape detail of the form task using a profile.
|
void |
FlangeTaskBuilder.setShapeDetailByProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the shape detail of the flange task for profiles
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
PierceHoleChildBuilder.setSlugHoleShape(DirectionOption direction,
IProfile[] profileEntries)
Sets the slug hole shape of the pierce hole
License requirements: ug_die_design ("Die Design") . |
void |
RibChildBuilder.setStartByProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the start limit geometry of the die rib using a profile.
|
void |
RibChildBuilder.setTopEndByProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the top end limit geometry of the die rib using a profile.
|
void |
TrimTaskBuilder.setTrimBounds(DirectionOption direction,
IProfile[] profileEntries)
Sets the trim bounds of the trim task.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ArcSegment
Represents a arc segment.
|
interface |
GapArcSegment
Represents a gap arc segment.
|
interface |
LineSegment
Represents a line segment.
|
interface |
SplineSegment
Represents a spline segment.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Instantiation
Represents an User Defined Template Instantiation object
To create or edit an instance of this class, use InstantiationBuilder Created in NX10.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.