See: Description
Interface | Description |
---|---|
Collection |
Represents a collection of user defined template
To obtain an instance of this class, refer to Part Created in NX10.0.0 |
Instantiation |
Represents an User Defined Template Instantiation object
To create or edit an instance of this class, use InstantiationBuilder Created in NX10.0.0 |
InstantiationBuilder |
Represents a
InstantiationBuilder
To create a new instance of this class, use Collection.createInstantiationBuilder(nxopen.userdefinedtemplate.Instantiation) Created in NX10.0.0 |
Class | Description |
---|---|
InstantiationBuilder.JaUserdefinedtemplateLayerOption |
Output layer options
|
InstantiationBuilder.MatchedExpressionData |
This class holds the data returned from
InstantiationBuilder.getMatchedExpression(nxopen.Expression) |
InstantiationBuilder.MatchedReferenceData |
This class holds the data returned from
InstantiationBuilder.getMatchedReference(nxopen.NXObject) |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.