Interface | Description |
---|---|
Override |
Represents a
Override object. |
OverrideBuilder |
Represents a
Override builder To create a new instance of this class, use ResultObject.createOverrideBuilder(nxopen.validate.Override) Default values. |
Parser |
Represents a NX
Parser . |
Requirement |
Represents a
Requirement object. |
RequirementBuilder |
Represents a
Requirement builder To create a new instance of this class, use RequirementCollection.createRequirementBuilder(nxopen.validate.Requirement) Default values. |
RequirementCheck |
Represents an NX
RequirementCheck object. |
RequirementCheckCollection |
Represents an NX
RequirementCheckCollection object. |
RequirementCollection |
Represents an NX
RequirementCollection object. |
ResultObject |
Represents a check-mate result object.
|
ValidationManager |
Represents an object that manages validator and parser associated instance objects.
|
Validator |
Represents a NX
Validator . |
ValidatorOptions |
Contains information about run options of check-mate checking process.
|
XmlComparator |
Provides a generic comparator for finding differences between two XML
format files.
|
Class | Description |
---|---|
OverrideBuilder.DecisionActions |
Represents the override request decision action
|
OverrideBuilder.RequestTypes |
Represents the override request type
|
OverrideBuilder.ToStates |
Represents the override request to state
|
Parser.DataSourceTypes |
The data source type of check result.
|
RequirementBuilder.DataTypeOptions |
This enum represents the data type of the value in requirement
|
RequirementBuilder.DefinitionMethodOptions |
This enum represents the type of requirement definition method
|
RequirementBuilder.RelationalOperatorOptions |
This enum represents the relational operator for comparing values
|
RequirementBuilder.SeverityOptions |
This enum represents the severity level when a requirement is not satisfied
|
RequirementCheck.SaveResultsToTeamcenterOptions |
This enum represents the Save Results to Teamcenter option
|
RequirementCollection.SourceTypeOptions |
This enum represents the type of external source where requirement is defined
|
ResultObject.ResultTypes |
The type of check result
|
ValidatorOptions.LogModeTypes |
The log mode type.
|
ValidatorOptions.ResultsDisplayModeTypes |
The results display mode type.
|
ValidatorOptions.SaveModeTypes |
The save mode type.
|
XmlComparator.Options |
Represents config options in comparison For example: case 1: Defines filter file to control what nodes will be compared; generates comparison report and log; ignores CDATA and processing instruction nodes. |
XmlComparator.Result |
Specifies result of the comparison
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.