public interface CastReliefParentBuilder
Modifier and Type | Interface and Description |
---|---|
static class |
CastReliefParentBuilder.CastReliefData
This class holds the data returned from
getCastRelief() |
Modifier and Type | Method and Description |
---|---|
DieBuildStatusOption |
buildStatus()
Returns the build status of cast relief.
|
boolean |
designStatus()
Returns the design status of cast relief, if true the cast relief will be built into the model, if false it will not.
|
boolean |
displayStatus()
Returns the display status of cast relief, if true input data to the cast relief will be displayed, if false the input data will not be displayed.
|
CastReliefParentBuilder.CastReliefData |
getCastRelief()
Gets the profile of the cast relief.
|
double |
reliefDepth()
Returns the relief depth of cast relief.
|
Body |
reliefSheet()
Returns the relief sheet of cast relief.
|
void |
setCastRelief(DirectionOption direction,
IProfile[] profileEntries)
Sets the profile of the cast relief.
|
void |
setDesignStatus(boolean designStatus)
Sets the design status of cast relief, if true the cast relief will be built into the model, if false it will not.
|
void |
setDisplayStatus(boolean displayStatus)
Sets the display status of cast relief, if true input data to the cast relief will be displayed, if false the input data will not be displayed.
|
void |
setReliefDepth(double reliefDepth)
Sets the relief depth of cast relief.
|
void |
setReliefSheet(Body reliefSheet)
Sets the relief sheet of cast relief.
|
void setCastRelief(DirectionOption direction, IProfile[] profileEntries) throws NXException, RemoteException
direction
- Profile direction.profileEntries
- The profile entries, can be curves, edges, faces, sketches or curve features.NXException
RemoteException
CastReliefParentBuilder.CastReliefData getCastRelief() throws NXException, RemoteException
NXException
RemoteException
void setReliefSheet(Body reliefSheet) throws NXException, RemoteException
reliefSheet
- NXException
RemoteException
Body reliefSheet() throws NXException, RemoteException
NXException
RemoteException
void setReliefDepth(double reliefDepth) throws NXException, RemoteException
reliefDepth
- NXException
RemoteException
double reliefDepth() throws NXException, RemoteException
NXException
RemoteException
void setDesignStatus(boolean designStatus) throws NXException, RemoteException
designStatus
- NXException
RemoteException
boolean designStatus() throws NXException, RemoteException
NXException
RemoteException
DieBuildStatusOption buildStatus() throws NXException, RemoteException
NXException
RemoteException
void setDisplayStatus(boolean displayStatus) throws NXException, RemoteException
displayStatus
- NXException
RemoteException
boolean displayStatus() throws NXException, RemoteException
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.