See: Description
Interface | Description |
---|---|
AddendumSectionBuilder |
Represents a
AddendumSectionBuilder which is used to create or edit an addendum section. |
AddendumSectionUserDefinedBuilder |
Represents a
AddendumSectionUserDefinedBuilder builder used to select a previously
defined section or a string of objects to define the section shape. |
AddSurfBuilder |
Represents a
AddSurfBuilder builder
To create a new instance of this class, use DieCollection.createAddSurfBuilder(nxopen.features.Feature) Created in NX6.0.0 |
CastRelief |
Represents a cast relief feature
To create or edit an instance of this class, use CastReliefBuilder Created in NX6.0.0 |
CastReliefBuilder |
Represents a
CastReliefBuilder builder
To create a new instance of this class, use DieCollection.castRelief(nxopen.die.CastRelief) Default values. |
CastReliefParentBuilder |
Represents a Die Cast Relief sub feature.
|
ClampingSlot |
Represents a clamping slot feature
To create or edit an instance of this class, use ClampingSlotBuilder Created in NX6.0.0 |
ClampingSlotBuilder |
Represents a Clamping Slot feature builder
To create a new instance of this class, use DieCollection.clampingSlot(nxopen.die.ClampingSlot) Default values. |
Clearance |
Represents a die design clearance feature.
|
ClearanceBuilder |
Represents a builder that is used to create or edit a
Clearance feature. |
CompensateRoughDataBuilder |
Represents a
CompensateRoughDataBuilder . |
ConnectProfileParentBuilder |
Represents a Die Connecting Profile sub feature.
|
DeckParentBuilder |
Represents a Die Deck Feature sub feature.
|
DieAssistantFlangeProfile | |
DieAssistantFlangeProfileList |
Represents a list of objects.
|
DieAssistantTrimProfile | |
DieAssistantTrimProfileList |
Represents a list of objects.
|
DieAttributesBuilder |
Represents a
DieAttributesBuilder . |
DieBooleanBuilder |
Represents a
DieBooleanBuilder . |
DieBooleanBuilderList |
Represents a list of objects.
|
DieCollection |
Represents a Die Engineering/Design feature builder.
|
DieDirectionBuilder |
Represents a
DieDirectionBuilder . |
DieLimitsBuilder |
Limits a path to a segment of the path.
|
DieLimitsBuilderList |
Represents a list of objects.
|
DieLocationBuilderList |
Represents a list of objects.
|
DieLocationsBuilder |
Represents a
DieLocationsBuilder . |
DiePlaneBuilder |
Represents a
DiePlaneBuilder . |
DieShoe |
Represents a die shoe feature
To create or edit an instance of this class, use DieShoeBuilder Created in NX6.0.0 |
DieShoeBuilder |
Represents a Die Shoe feature builder.
|
DieSimCollection |
Represents a collection of Die Simulation - Press Models
To obtain an instance of this class, refer to Part Created in NX6.0.0 |
DrawBead |
Represents a draw bead feature.
|
DrawBeadBuilder |
Represents a builder that is used to create or edit a
DrawBead feature. |
DrawBeadSegmentBuilder |
Segment builder for Die Engineering draw bead.
|
DrawBeadSegmentBuilderList |
Represents a list of objects.
|
DrawBeadTaperBuilder |
Taper definition for the end of the Die Engineering Draw Bead.
|
DrawDiePunchBuilder |
Represents a Draw Die Punch feature builder.
|
DrawDiePunchSectionBuilder |
Represents a Draw Die Punch Section sub feature.
|
FillArea |
Represents a die design fill area feature.
|
FillAreaBuilder |
Represents a builder that is used to create or edit a
FillArea feature. |
FillBuilder |
Represents an Area Fill feature
To create a new instance of this class, use DieCollection.fill(nxopen.features.Feature) Created in NX4.0.0 |
FingerClearanceNotch |
Represents a die design finger clearance notch feature.
|
FingerClearanceNotchBuilder |
Represents a builder that is used to create or edit a
FingerClearanceNotch feature. |
FlangeSteelRibChildBuilder |
Represents a Die Flange Steel Rib Child sub feature.
|
FlangeSteelRibParentBuilder |
Represents a Die Flange Steel Rib Parent sub feature.
|
FlangeTaskBuilder |
Represents a Flange Task feature builder.
|
FormTaskBuilder |
Represents a Form Task feature builder.
|
HandlingCore |
Represents a die design handling core feature.
|
HandlingCoreBuilder |
Represents a builder that is used to create or edit a
HandlingCore feature. |
HandlingCoreChildBuilder |
Represents a Die Handling Core Child sub feature.
|
HandlingCoreParentBuilder |
Represents a Die Handling Core Parent sub feature.
|
Heelpost |
Represents a heelpost feature
To create or edit an instance of this class, use HeelpostBuilder Created in NX6.0.0 |
HeelpostBuilder |
Represents a
HeelpostBuilder builder
To create a new instance of this class, use DieCollection.heelpost(nxopen.die.Heelpost) Default values. |
HoleChildBuilder |
Represents a Die Hole Child sub feature.
|
HoleParentBuilder |
Represents a Die Hole Parent sub feature.
|
Keyway |
Represents a keyway feature
To create or edit an instance of this class, use KeywayBuilder Created in NX6.0.0 |
KeywayBuilder |
Represents a
KeywayBuilder builder
To create a new instance of this class, use DieCollection.keyway(nxopen.die.Keyway) Default values. |
KeywayChildBuilder |
Represents a Die Keyway Child sub feature.
|
KeywayParentBuilder |
Represents a Die Keyway Parent sub feature.
|
LineupBuilder |
Represents a Lineup feature builder
To create a new instance of this class, use DieCollection.lineup(nxopen.features.Feature) Created in NX4.0.0 |
MachineRelief |
Represents a die design machine relief feature.
|
MachineReliefBuilder |
Represents a builder that is used to create or edit a
MachineRelief feature. |
OutputCurvesBuilder |
Represents an output curves feature builder.
|
PadChildBuilder |
Represents a Die Pad Child sub feature.
|
PadParentBuilder |
Represents a Die Pad Parent sub feature.
|
PierceHoleChildBuilder |
Represents a Pierce Hole Child sub feature.
|
PierceHoleParentBuilder |
Represents a Pierce Hole Parent sub feature.
|
PierceItemBuilder | |
PierceItemBuilderList |
Represents a list of objects.
|
PierceTaskBuilder |
Represents a Pierce Task feature builder
To create a new instance of this class, use DieCollection.pierceTask(nxopen.features.Feature) Created in NX4.0.0 |
PointChildBuilder |
Represents a Die Point Child sub feature.
|
PointParentBuilder |
Represents a Die Point Parent sub feature.
|
PressModel |
Represents a Die Simulation - Press Model .
|
PressModelRoot |
Represents a Die Simulation - Press Model Root.
|
PressureSystemChildBuilder |
Represents a Die Pressure System Child sub feature.
|
PressureSystemParentBuilder |
Represents a Die Pressure System Parent sub feature.
|
QuickBinderBuilder |
Represents a
QuickBinderBuilder builder which builds a developable binder sheet
body by adding cones, cylinders, or planes to an approximated face. |
QuickBinderWrapBuilder |
Represents a
QuickBinderWrapBuilder builder
This is an abstract class, and cannot be created. |
RibChildBuilder |
Represents a Die Rib Child sub feature.
|
RibParentBuilder |
Represents a Die Rib Parent sub feature.
|
RotorBuilder |
Represents a CAM Rotor feature builder.
|
RotorSectionBuilder |
Represents a Rotor Section sub feature.
|
SpringbackCompensation |
Represents a springback compensation feature.
|
SpringbackCompensationBuilder |
Used to create or edit a
SpringbackCompensation feature. |
SteelInsertBuilder |
Represents a Steel Insert feature builder.
|
SteelInsertSectionBuilder |
Represents a Steel Insert Section sub feature.
|
SteelInsertSegmentChildBuilder |
Represents a Steel Insert Segment Child sub feature.
|
SteelInsertSegmentParentBuilder |
Represents a Steel Insert Segment Parent sub feature.
|
ThroatChildBuilder |
Represents a Die Throat Child sub feature.
|
ThroatParentBuilder |
Represents a Die Throat Parent sub feature.
|
Tip |
Represents a Tip feature.
|
TrimFlangeDieAssistant |
Represents a trim/flange die assistant
To create or edit an instance of this class, use TrimFlangeDieAssistantBuilder Created in NX5.0.0 |
TrimFlangeDieAssistantBuilder |
Represents a
TrimFlangeDieAssistantBuilder
To create a new instance of this class, use DieCollection.trimFlangeDieAssistant(nxopen.features.Feature) Created in NX5.0.0 |
TrimLineDevelopmentBuilder |
Represents a
TrimLineDevelopment builder
To create a new instance of this class, use DieCollection.createTrimLineDevelopmentBuilder(nxopen.features.Feature) Created in NX6.0.0 |
TrimTaskBuilder |
Represents a Trim Task feature builder.
|
UncutRegionsBuilder |
Calculates the uncut regions of a curve given a radius value for the cut tool.
|
WearPlateLocChildBuilder |
Represents a Die Wear Plate Locator sub feature.
|
WearPlateLocParentBuilder |
Represents a Die Wear Plate Locator sub feature.
|
Class | Description |
---|---|
AddendumSectionBuilder.SectionLocationType |
The settings indicating the location of the section being created.
|
AddendumSectionBuilder.SectionOrientationType |
The settings to indicate the section orientation.
|
AddendumSectionBuilder.SectionShapeType |
The settings to indicate the section shape.
|
AddendumSectionBuilder.SegmentParameterType |
The settings to indicate which parameter of the segment to lock.
|
AddendumSectionBuilder.SegmentType |
The settings to indicate the segment type to update.
|
AddendumSectionBuilder.SurfaceBuildType |
The settings to indicate the surface type.
|
AddSurfBuilder.Methods |
Settings for the type of addendum surface being created.
|
CastReliefParentBuilder.CastReliefData |
This class holds the data returned from
CastReliefParentBuilder.getCastRelief() |
ClampingSlotBuilder.Types |
Clamping slot types
|
ClearanceBuilder.ClearanceGeometryTypes |
Identifies which type of input defines the clearance.
|
ClearanceBuilder.Types |
Identifies which clearance type is being created in the casting.
|
CompensateRoughDataBuilder.ApproximationType |
Settings for the amount of approximation to perform.
|
CompensateRoughDataBuilder.Types |
Settings for the type of data being compensated.
|
ConnectProfileParentBuilder.ProfileData |
This class holds the data returned from
ConnectProfileParentBuilder.getProfile() |
DeckParentBuilder.MainDeckData |
This class holds the data returned from
DeckParentBuilder.getMainDeck() |
DieAssistantFlangeProfileType |
Settings for the flange type.
|
DieBooleanBuilder.BooleanType |
boolean type to apply to the selected solids
|
DieBuildStatusOption |
Settings for the build status of the die design sub features.
|
DieDirectionBuilder.DirectionType |
the options available for defining the direction
|
DiePlaneBuilder.PlaneType |
the options available for defining the plane
|
DirectionOption |
Settings for the profile direction.
|
DrawBeadBuilder.FemaleDepthTypes |
Specifies how the female depth is calculated or defined.
|
DrawBeadBuilder.FemaleWidthTypes |
Specifies how the feamle width is calcualted or defined.
|
DrawBeadBuilder.MaleBeadPositionTypes |
Identifes which casting the male bead is created in.
|
DrawBeadBuilder.OrientationTypes |
Identifies the orientation of the base parameters to the sheet metal.
|
DrawBeadBuilder.OrientSectionToDrawTypes |
Specifies if the segment height section parameter should be oriented to the draw direction or the sheet metal normal at the section location.
|
DrawBeadBuilder.OutputTypes |
Specifies what type of output is desired for the feature creation.
|
DrawBeadBuilder.ProjectionDirectionTypes |
Identifes how the centerline should be projected to the placement face during processing.
|
DrawBeadBuilder.TransitionDefinitionTypes |
Specifies how the transition area should be determined from segment to segment within a single bead.
|
DrawBeadSegmentBuilder.MaleBeadWidthTypes |
value for how the male width is specified.
|
DrawBeadTaperBuilder.TaperTypes |
Taper types to define how the slope is created for the bead end.
|
DrawDiePunchBuilder.PunchProfileData |
This class holds the data returned from
DrawDiePunchBuilder.getPunchProfile() |
DrawDiePunchSectionBuilder.FormingAttributesData |
This class holds the data returned from
DrawDiePunchSectionBuilder.getFormingAttributes() |
DrawDiePunchSectionBuilder.PunchProfileAttributesData |
This class holds the data returned from
DrawDiePunchSectionBuilder.getPunchProfileAttributes() |
FillAreaBuilder.Types |
Identifies the area of the casting the fill is targeted for.
|
FillAreaBuilder.UpperLimitTypes |
Specifies how the upper limit of the fill area is defined.
|
FillBuilder.RegionBoundsData |
This class holds the data returned from
FillBuilder.getRegionBounds() |
FingerClearanceNotchBuilder.Types |
Specifies what type of base geometry to build the finger clearance notch from.
|
FlangeTaskBuilder.CameraLayerAndXmlpData |
This class holds the data returned from
FlangeTaskBuilder.getCameraLayerAndXmlp() |
FlangeTaskBuilder.CamTypes |
Settings for the cam type of the flange task.
|
FlangeTaskBuilder.PierceTypes |
Settings for the pierce type of the flange task.
|
FlangeTaskBuilder.RegionBoundsData |
This class holds the data returned from
FlangeTaskBuilder.getRegionBounds() |
FlangeTaskBuilder.SpringbackTypes |
Settings for the springback type of the flange task.
|
FormTaskBuilder.RegionBoundsData |
This class holds the data returned from
FormTaskBuilder.getRegionBounds() |
HandlingCoreBuilder.Types |
Identifies how the handling Core is located in space.
|
HeelpostBuilder.Types |
Heelpost types
|
HoleChildBuilder.HoleAttributesData |
This class holds the data returned from
HoleChildBuilder.getHoleAttributes() |
HoleChildBuilder.PadAttributesData |
This class holds the data returned from
HoleChildBuilder.getPadAttributes() |
HoleParentBuilder.HoleAttributesData |
This class holds the data returned from
HoleParentBuilder.getHoleAttributes() |
HoleParentBuilder.PadAttributesData |
This class holds the data returned from
HoleParentBuilder.getPadAttributes() |
KeywayBuilder.LocationType |
Keyway location direction relative to the die centerline coordinate system
|
KeywayBuilder.Types |
Keyway runoff types
|
KeywayChildBuilder.LocationOption |
Settings for the location of the keyway.
|
KeywayChildBuilder.RunoffTypeOption |
Settings for the runoff type of the keyway.
|
KeywayChildBuilder.SlotAttributesData |
This class holds the data returned from
KeywayChildBuilder.getSlotAttributes() |
KeywayParentBuilder.RunoffTypeOption |
Settings for the runoff type of the keyway.
|
KeywayParentBuilder.SlotAttributesData |
This class holds the data returned from
KeywayParentBuilder.getSlotAttributes() |
MachineReliefBuilder.MainProfileTypes |
Specifies that the profile is for an exterior or interior profile.
|
MachineReliefBuilder.TrimSheetTypes |
Specifies what the trimming surface is defined by.
|
MachineReliefBuilder.Types |
Identifies the type of structure to be added, or subtracted, to the casting.
|
OutputCurvesBuilder.SmoothTypes |
Settings for the curve smoothing type.
|
OutputCurvesBuilder.TrimCurveCreateTypes |
Settings for the trim curve creation type.
|
OutputCurvesBuilder.TrimCurveTypes |
Settings for the trim curve type.
|
OutputCurvesBuilder.TrimOutputCurveTypes |
Settings for the trim curve output type.
|
PadChildBuilder.HoleAttributesData |
This class holds the data returned from
PadChildBuilder.getHoleAttributes() |
PadChildBuilder.PadAttributesData |
This class holds the data returned from
PadChildBuilder.getPadAttributes() |
PadChildBuilder.ShapeData |
This class holds the data returned from
PadChildBuilder.getShape() |
PadChildBuilder.ShapeTypeOption |
Settings for the shape type of the die pad.
|
PadParentBuilder.HoleAttributesData |
This class holds the data returned from
PadParentBuilder.getHoleAttributes() |
PadParentBuilder.PadAttributesData |
This class holds the data returned from
PadParentBuilder.getPadAttributes() |
PadParentBuilder.ShapeTypeOption |
Settings for the shape type of the die pads.
|
PierceHoleChildBuilder.HoleAttributesData |
This class holds the data returned from
PierceHoleChildBuilder.getHoleAttributes() |
PierceHoleChildBuilder.PierceHoleShapeData |
This class holds the data returned from
PierceHoleChildBuilder.getPierceHoleShape() |
PierceHoleChildBuilder.ShapeTypeOption |
Settings for the shape type of the pierce hole.
|
PierceHoleParentBuilder.HoleAttributesData |
This class holds the data returned from
PierceHoleParentBuilder.getHoleAttributes() |
PierceItemBuilder.HoleShapeType |
Settings for the hole shape of individual pierces.
|
PierceItemBuilder.SizingMethodOption |
Settings for the sizing method of individual pierces.
|
PierceTaskBuilder.CameraLayerAndXmlpData |
This class holds the data returned from
PierceTaskBuilder.getCameraLayerAndXmlp() |
PierceTaskBuilder.CamTypes |
Settings for the cam type of the pierce task.
|
PierceTaskBuilder.CenterPointOptionTypes |
Settings for the center point output options of the pierce task.
|
PierceTaskBuilder.PierceBoundsData |
This class holds the data returned from
PierceTaskBuilder.getPierceBounds() |
PierceTaskBuilder.PrecisionTypes |
Settings for the precistion type of the pierce task.
|
QuickBinderBuilder.EdgesOfFaceData |
This class holds the data returned from
QuickBinderBuilder.getEdgesOfFace(int) |
QuickBinderBuilder.EditTypes |
The type of edit to be performed on the face.
|
QuickBinderBuilder.Types |
The method used to approximate the product faces.
|
QuickBinderWrapBuilder.EditSizeType |
Settings for the edit size type.
|
QuickBinderWrapBuilder.Types |
Settings for the binder wrap sheet body type.
|
RibChildBuilder.CenterlineData |
This class holds the data returned from
RibChildBuilder.getCenterline() |
RotorBuilder.FlangeBendProfileData |
This class holds the data returned from
RotorBuilder.getFlangeBendProfile() |
RotorSectionBuilder.RotorAttributesData |
This class holds the data returned from
RotorSectionBuilder.getRotorAttributes() |
SpringbackCompensationBuilder.DefinedByType |
The type of input data that defines the compensation.
|
SpringbackCompensationBuilder.DegreeType |
The polynomial degree type.
|
SpringbackCompensationBuilder.ResultSheetType |
The type of sheet body you would like created as output.
|
SteelInsertBuilder.HoleGridOrientationData |
This class holds the data returned from
SteelInsertBuilder.getHoleGridOrientation() |
SteelInsertBuilder.InsertTypeOption |
Settings for the insert type.
|
SteelInsertBuilder.MainProfileData |
This class holds the data returned from
SteelInsertBuilder.getMainProfile() |
SteelInsertSectionBuilder.ExtensionTypeOption |
Settings for the extension type.
|
SteelInsertSectionBuilder.FormingAttributesData |
This class holds the data returned from
SteelInsertSectionBuilder.getFormingAttributes() |
SteelInsertSegmentChildBuilder.ExtensionTypeOption |
Settings for the extension type.
|
SteelInsertSegmentChildBuilder.InsertTypeOption |
Settings for the insert type.
|
SteelInsertSegmentParentBuilder.ExtensionTypeOption |
Settings for the extension type.
|
SteelInsertSegmentParentBuilder.InsertTypeOption |
Settings for the insert type.
|
ThroatChildBuilder.ExtensionAttributesData |
This class holds the data returned from
ThroatChildBuilder.getExtensionAttributes() |
ThroatChildBuilder.TypeOption |
Settings for the type of the throat section.
|
ThroatParentBuilder.ExtensionAttributesData |
This class holds the data returned from
ThroatParentBuilder.getExtensionAttributes() |
ThroatParentBuilder.TypeOption |
Settings for the type of the throat section.
|
Tip.MapEdgeData |
This class holds the data returned from
Tip.mapEdge(nxopen.IProfile) |
TrimLineDevelopmentBuilder.Convergency |
The solver convergency level of onestep unform.
|
TrimLineDevelopmentBuilder.MaterialTypeName |
Indicates type of material
|
TrimLineDevelopmentBuilder.MeshElement |
The 2-D mesh element type of onestep unform.
|
TrimLineDevelopmentBuilder.OutputMethodName |
Indicates which trim curves to output
|
TrimLineDevelopmentBuilder.SmoothingName |
Indicates type of curve smoothing
|
TrimLineDevelopmentBuilder.Surface |
The surface types of onestep unform.
|
TrimTaskBuilder.CameraLayerAndXmlpData |
This class holds the data returned from
TrimTaskBuilder.getCameraLayerAndXmlp() |
TrimTaskBuilder.CamTypes |
Settings for the cam type of the trim task.
|
TrimTaskBuilder.CheckAndMovePlanesData |
This class holds the data returned from
TrimTaskBuilder.checkAndMovePlanes(nxopen.features.Feature, nxopen.features.Feature, nxopen.ISurface, nxopen.ISurface) |
TrimTaskBuilder.MatchCutTypes |
Settings for the match cut type of the trim task.
|
TrimTaskBuilder.TrimBoundsData |
This class holds the data returned from
TrimTaskBuilder.getTrimBounds() |
UncutRegionsBuilder.ResultsType |
Indicates which side of curve to check
|
WearPlateLocChildBuilder.PadAttributesData |
This class holds the data returned from
WearPlateLocChildBuilder.getPadAttributes() |
WearPlateLocChildBuilder.PositionType |
Settings for the positioning of the locator relative to the wear plate.
|
WearPlateLocParentBuilder.PadAttributesData |
This class holds the data returned from
WearPlateLocParentBuilder.getPadAttributes() |
WearPlateLocParentBuilder.PositionType |
Settings for the positioning of the locator relative to the wear plate.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.