Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.pdm |
Provides classes and interfaces for PDM.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
nxopen.validate |
Provides classes and interfaces for Validation Utilities.
|
Modifier and Type | Method and Description |
---|---|
ErrorList |
IAttributeSourceObjectBuilder.autoAssignAttributes(NXObject[] objects)
Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
|
ErrorList |
Sketch.deleteObjects(NXObject[] objects)
Deletes objects from the sketch
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
ErrorList |
Update.errorList()
Returns the list of all the errors that the Update module has encountered
since the last time that the list was cleared.
|
ErrorList |
Session.newErrorList()
Creates a new error list.
|
Modifier and Type | Field and Description |
---|---|
ErrorList |
ComponentAssembly.RestructureComponentsData.errorList
Any errors that occurred during the restructure
|
ErrorList |
ComponentAssembly.CheckoutAllModifiedObjectsData.errorList
Any errors that occurred during checking out of objects
|
Modifier and Type | Method and Description |
---|---|
ErrorList |
ComponentAssembly.checkinComponents(Component[] partOccs,
ComponentAssembly.CheckinCheckoutOption checkinInputOption)
Checks in array of components as per the option
ComponentAssembly.CheckinCheckoutOption . |
ErrorList |
PositioningTask.checkInPositioningGroups(PositioningGroup[] positioningGroups)
Checks in the specified
nxopen.assemblies.PositioningGroup s which must be
associated with this positioning task. |
ErrorList |
ComponentAssembly.checkinWorkset()
Checks in workset.
|
ErrorList |
ComponentAssembly.checkoutComponents(Component[] partOccs,
ComponentAssembly.CheckinCheckoutOption checkoutInputOption)
Checks out array of components as per the option
ComponentAssembly.CheckinCheckoutOption . |
ErrorList |
PositioningTask.checkOutPositioningGroups(PositioningGroup[] positioningGroups)
Checks out the specified
nxopen.assemblies.PositioningGroup s which must be
associated with this positioning task. |
ErrorList |
ComponentAssembly.checkoutWorkset()
Checks out workset.
|
ErrorList |
Component.displayComponentsExact(Component[] components)
Sets an array of components to display using the exact representation.
|
ErrorList |
Component.displayComponentsLightweight(Component[] components)
Sets an array of components to display using the lightweight representation.
|
ErrorList |
ReplaceComponentBuilder.getErrorList()
Get the list of components that failed to replace with their corresponding error codes.
|
ErrorList |
DesignElementBuilder.getOperationFailures()
Returns design element operation failures
License requirements: None. |
ErrorList |
ComponentAssembly.releaseSuppression(Component[] components)
Release control of the suppression state of an array of components.
|
ErrorList |
ComponentAssembly.releaseSuppression(Component[] components,
Arrangement[] arrangements)
Release control of the suppression state of an array of components.
|
ErrorList |
ComponentAssembly.replaceReferenceSetInOwners(String newReferenceSet,
Component[] components)
Sets the reference set used to represent each component in an array.
|
ErrorList |
Component.suppress(Component[] components)
Suppresses an array of components in the ComponentAssembly that contains their
controlling Arrangement.
|
ErrorList |
ComponentAssembly.suppressComponents(Component[] components)
Suppresses an array of components in all
Arrangement s in this ComponentAssembly
License requirements: assemblies ("ASSEMBLIES MODULE") Created in NX3.0.0 |
ErrorList |
ComponentAssembly.suppressComponents(Component[] components,
Arrangement[] arrangements)
Suppresses an array of components
License requirements: assemblies ("ASSEMBLIES MODULE") . |
ErrorList |
ComponentAssembly.suppressComponents(Component[] components,
Arrangement[] arrangements,
String expression)
Suppresses an array of components in all
Arrangement s in this ComponentAssembly
License requirements: assemblies ("ASSEMBLIES MODULE") Created in NX5.0.1 |
ErrorList |
Component.unsuppress(Component[] components)
Unsuppresses an array of components in the ComponentAssembly that contains their
controlling Arrangement.
|
ErrorList |
ComponentAssembly.unsuppressComponents(Component[] components)
Unsuppresses an array of components in all
Arrangement s in this ComponentAssembly
License requirements: assemblies ("ASSEMBLIES MODULE") Created in NX3.0.0 |
ErrorList |
ComponentAssembly.unsuppressComponents(Component[] components,
Arrangement[] arrangements)
Unsuppresses an array of components in this ComponentAssembly
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Modifier and Type | Method and Description |
---|---|
ErrorList |
AssemblyCutBuilder.getOperationFailures()
Gets the list of errors encountered in the Assembly cut operation.
|
Modifier and Type | Method and Description |
---|---|
ErrorList |
CopyPasteNewBuilder.getOperationFailures()
Gets the operation failure error list object
License requirements: nx_ship_detail ("Ship Detail Design") . |
Modifier and Type | Method and Description |
---|---|
ErrorList |
PartOperationBuilder.getOperationFailures()
Returns part operation failures
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
ErrorList |
QuickPathBuilder.pathErrors()
Returns the errors associated with this path.
|
Modifier and Type | Field and Description |
---|---|
ErrorList |
ElectricalStockDeviceCollection.AutoRouteConnectionsData.errorList
Any errors that occurred during Automatic Routing.
|
Modifier and Type | Method and Description |
---|---|
ErrorList |
Parser.deleteResultObject(ResultObject resultObject)
Deletes result object, return error list
License requirements: None. |
ErrorList |
Validator.getLastErrorListFromCommit()
Return the list of errors happened during last
Validator.commit() . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.