Interface | Description |
---|---|
AlternateIdManager |
This class is responsible for setting and getting NX Manager database attribute.
|
AttributeGroupDescription |
Represents an attribute group type.
|
AttributeGroupDescriptionCollection |
Represents a collection of attribute group description objects.
|
AttributeGroupReviseBuilder |
Represents an attribute group revise builder.
|
CaeCloneManager | Deprecated
Deprecated in NX10.0.0.
|
CAEFileContainer |
This class is a File Container class for uploading JT files created by NX CAE Post Processing to Teamcenter.
|
ConfigurationContextBuilder |
Represents a
ConfigurationContextBuilder builder To create a new instance of this class, use ConfigurationManager.createConfigurationContextBuilder() Created in NX9.0.0 |
ConfigurationManager |
Represents Configuration Manager
Use Session.configurationManager() to get the instance of this class. |
DatabaseAttributeManager |
This class is responsible for setting and getting NX Manager database attribute.
|
DesignElementRevision |
Represents the design element revision in the database.
|
DesignFeatureRevision |
Represents the design feature revision in the database.
|
DesignSubordinateRevision |
Represents the design subordinate revision in the database.
|
EffectivityAttributePropertiesBuilder |
Represents an
EffectivityAttributePropertiesBuilder to be used for creating effectivity attributes. |
EffectivityTableRow |
Represents the class that contains effectivity parameters.
|
FileManagement |
This class is responsible for Teamcenter file management related activities.
|
GenericObjectAttributeHolder |
Represents the class that contains database business logic or pre-creation information for the objects.
|
IAttributeGroupOwner |
An interface class for objects that own attribute groups.
|
ListOfValues |
Represents list of values to be used in search query .
|
LogicalObject |
Represents the class that contains database business logic or pre-creation information for the objects.
|
ModelElementRevision |
Represents a base class that provides common methods for various model elements in a
CollaborativeDesign . |
NativePartLogicalObject |
Represents the class that contains information for the objects participating in import operation.
|
ObjectCreateBuilder |
Represents a builder class that perofrms create operation
To create a new instance of this class, use PdmSession.createObjectCreateBuilder(java.lang.String[], java.lang.String[]) Created in NX10.0.0 |
OperationErrors |
Represents Operation Errors to be returned in TCIN related operations .
|
PartBuilder |
This class serves as the base class for NX Manager part builders.
|
PartCreationObject |
This class is a proxy for a to-be-created part prior to the part being created.
|
PartCreationObjectAttributePropertiesBuilder | Deprecated
Deprecated in NX8.5.0.
|
PartFromPartBuilder |
This class provides the methods necessary to create a new part in NX Manager
from an existing part.
|
PartFromTemplateBuilder |
This class provides the methods necessary to create a new part in NX Manager
from a template part.
|
PartManager |
This class contains methods to create and manage parts in NX Manager mode.
|
PartOperationAttributePropertiesBuilder |
Represents an
PartOperationAttributePropertiesBuilder to be used for
creating attributes in part operation. |
PartOperationBuilder |
Represents a builder class that performs various design element operations.
|
PartOperationCopyBuilder |
Represents a builder class that performs various Save As operations.
|
PartOperationCreateBuilder |
Represents a builder class that performs Create operations
To create a new instance of this class, use PdmSession.createCreateOperationBuilder(nxopen.pdm.PartOperationBuilder.OperationType) Created in NX10.0.0 |
PartOperationImportCallbackData |
JA interface for PartOperationImportCallbackData object
This cannot be created . |
PartOperationImportObserver |
This class is responsible for invoking registered callbacks at different stages in import operation.
|
PartOperationImportObserver.InitializeCb |
User defined Initialize callback that is called during initialization of import builder
|
PartOperationImportObserver.PostCommitCb |
User defined PostCommit callback that is called after commit of import operation
|
PartOperationImportObserver.PreAutoassignCb |
User defined PreAutoAssign callback that is called before auto-assigning attributes
|
PartOperationImportObserver.PreCommitCb |
User defined PreCommit callback that is called before commit of import operation
|
PartOperationImportObserver.TerminateCb |
User defined Terminate callback that is called during destruction of import builder
|
PartOperationMakeUniqueBuilder |
Represents a
PartOperationMakeUniqueBuilder builder To create a new instance of this class, use PdmSession.createMakeUniqueOperationBuilder(nxopen.BasePart) Created in NX10.0.0 |
PartOperationValidationPropertiesBuilder |
Represents an
PartOperationValidationPropertiesBuilder to be used
for overriding the default validation parameters for a part in import operation. |
PdmPart |
This class serves as a gateway to part-specific tools for NX Manager mode.
|
PdmSearch |
Represents search query .
|
PdmSearchManager |
Represents search manager class
Use Session.pdmSearchManager() to get the instance of this class. |
PdmSession |
Represents the NX Manager session
To obtain an instance of this class, refer to Session Created in NX7.5.0 |
PendingComponentsManager |
This class is used for managing a part's pending components, that
is, those that have been added within Teamcenter but are not yet
present in NX.
|
PersistentSettings |
Persistently held settings for a Teamcenter user account.
|
RequirementUtils |
Collection of PDM utility methods
To obtain an instance of this class, refer to Session Created in NX6.0.3 |
SearchResult |
Represents search query .
|
SessionSettings |
Values for the settings that affect the current Teamcenter session.
|
SoaQuery |
Represents search soa query to perform Teamcenter search .
|
TracelinkQuery |
Represents the Trace link query
To obtain an instance of this class use RequirementUtils Created in NX6.0.3 |
VariantConfigurationBuilder |
Represents a builder class that performs variant rule configuration.
|
Class | Description |
---|---|
AlternateIdManager.AlternateIdsData |
Contains alternate Ids data
|
AlternateIdManager.AssignAlternateIdData |
This class holds the data returned from
AlternateIdManager.assignAlternateId() |
AlternateIdManager.AssignAlternateRevData |
Contains alternate Revision Id data
|
CaeCloneManager.CloneOption |
Option for creation of part builder for CAE Clone
|
ConfigurationContextBuilder.ConfigContextMode |
configuration mode
|
ConfigurationContextBuilder.ConfigContextType |
configuration type
|
ConfigurationContextBuilder.ConfigurationDetail |
configuration detail
|
DesignElementRevision.DesignElementCategory |
Represents the category for this design element revision.
|
DesignElementRevision.TransformData |
This class holds the data returned from
DesignElementRevision.getTransform() |
FileManagement.ExportFilesData | |
ModelElementRevision.PositioningStatus |
Represents the positioning status of a design element
|
PartBuilder.Operation |
Tokens identifying every possible UG/Manager part selection dialog.
|
PartBuilder.PartFileNameData |
Contains part file name information
|
PartBuilder.PartNumberData |
Contains part number information.
|
PartBuilder.PartRevisionData |
Contains part revision information
|
PartFromPartBuilder.FileSaveAs |
This enum is used to specify which non-master parts and dependent files
should be saved during the save as operation.
|
PartOperationBuilder.DependentFileSaveAs | Deprecated
Deprecated in NX10.0.0.
|
PartOperationBuilder.NonMasterSaveAs | Deprecated
Deprecated in NX10.0.0.
|
PartOperationBuilder.OperationType |
Represents an operation type that can be performed on a part .
|
PartOperationCopyBuilder.CopyDependentFiles |
This enum is used to specify which dependent files
should be copied to new part during the save as operation.
|
PartOperationCopyBuilder.CopyNonMasterParts |
This enum is used to specify which non-master parts
should be copied to new part during the save as operation.
|
PartOperationCopyBuilder.OperationSubType |
Represents an operation sub type for copying a part
|
PartOperationCreateBuilder.OperationSubType |
Represents an operation sub type for creating a part
|
PdmPart.CheckinInput |
Reservation check-in input struct
|
PdmPart.CheckoutInput |
Reservation check-out input struct
|
PdmSession.SsoSettingsData |
This class holds the data returned from
PdmSession.getSsoSettings() |
PdmSession.TcserverSettingsData |
This class holds the data returned from
PdmSession.getTcserverSettings() |
PdmSoaqueryNxmgrfielddatatype |
NX Manager search field data type
|
PendingComponentsManager.AddComponentData |
This class holds the data returned from
PendingComponentsManager.addComponent(java.lang.String) |
VariantConfigurationBuilder.VariantRuleTableInformationData |
This class holds the data returned from
VariantConfigurationBuilder.getVariantRuleTableInformation() |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.