StudioXformBuilderEx Class¶
-
class
NXOpen.Features.
StudioXformBuilderEx
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.StudioXform
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateStudioXformBuilderEx
Default values.
Property Value AdvancedMethodOption AdvancedOff CanUseFaceFinder 0 CurveRange.AnchorPosition Start DegreesAndSegmentsOrPatches.Degree 3 DegreesAndSegmentsOrPatches.SegmentsOrPatches 1 DegreesAndSegmentsOrPatches.UDegree 5 DegreesAndSegmentsOrPatches.UPatches 1 DegreesAndSegmentsOrPatches.VDegree 5 DegreesAndSegmentsOrPatches.VPatches 1 ExtractMethod Original FaceFinder.CoaxialEnabled 0 FaceFinder.CoplanarAxesEnabled 0 FaceFinder.CoplanarEnabled 0 FaceFinder.EqualDiameterEnabled 0 FaceFinder.OffsetEnabled 0 FaceFinder.ParallelEnabled 0 FaceFinder.PerpendicularEnabled 0 FaceFinder.SymmetricEnabled 0 FaceFinder.TangentEnabled 0 FaceFinder.ThicknessChainEnabled 0 FaceFinder.UseFaceBrowse 1 FallOffScale 0 FeatureSaveMethod Relative InsertKnotDirection UDirection InsertKnotParameter 20 IsSingleSelection 1 KeepAllContinuity 0 LockPoles 1 LockRegionUEndFlexibility 0 LockRegionUStartFlexibility 0 LockRegionVEndFlexibility 0 LockRegionVStartFlexibility 0 MovementMethod View PlanarizeDirection U PlanarizeMethod AtPlaneLocation PlanarizeProjectionPlane YZ PrincipalMovementDirection Z PrincipalRotatingAxis Z PrincipalScalingDirection X ProportionalAllU 1 ProportionalAllV 1 ProportionalFallOffScale (deprecated) 0.5 ProportionalMoveAfterU 0 ProportionalMoveAfterV 0 ProportionalMoveBeforeU 0 ProportionalMoveBeforeV 0 RotatingAxis WCS ScalingDirection View SurfaceRange.AnchorPosition Vertex1 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AdvancedMethod | Returns or sets the advanced method |
AdvancedMethodOption | Returns or sets the advanced method |
CanUseFaceFinder | Returns or sets the using face finder flag |
ContinuityUMax | Returns the continuity at U maximum |
ContinuityUMin | Returns the continuity at U minimum |
ContinuityVMax | Returns the continuity at V maximum |
ContinuityVMin | Returns the continuity at V minimum |
ControlPoleManager | Returns the control pole manager |
CurveRange | Returns the curve range |
DegreesAndSegmentsOrPatches | Returns the degrees and segments or patches |
ExtractMethod | Returns or sets the b-surface extraction method |
ExtractTolerance | Returns or sets the value indicating a tolerance to be used to extract a b-surface from a selection face |
FaceFinder | Returns the face finder |
FallOffScale | Returns or sets the fall off scale |
FeatureSaveMethod | Returns or sets the feature save method |
InsertKnotDirection | Returns or sets the insert knot direction |
InsertKnotParameter | Returns or sets the parameter where to insert knots |
IsSingleSelection | Returns or sets the single selection flag |
KeepAllContinuity | Returns or sets a value indicating whether to keep all continuity |
LockPoles | Returns or sets a value indicating whether to lock poles in boundary constraints |
LockRegionUEndFlexibility | Returns or sets the lock region flexibility at U end |
LockRegionUStartFlexibility | Returns or sets the lock region flexibility at U start |
LockRegionVEndFlexibility | Returns or sets the lock region flexibility at V end |
LockRegionVStartFlexibility | Returns or sets the lock region flexibility at V start |
MovementArbitraryPlane | Returns or sets the movement arbitrary plane |
MovementArbitraryVector | Returns or sets the movement arbitrary vector |
MovementMethod | Returns or sets the movement method |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlanarizeArbitraryPlane | Returns or sets the planarize arbitrary plane |
PlanarizeDirection | Returns or sets the planarize direction |
PlanarizeMethod | Returns or sets the planarize method |
PlanarizeProjectionPlane | Returns or sets the planarize projection plane |
PrincipalMovementDirection | Returns or sets the principal movement direction |
PrincipalRotatingAxis | Returns or sets the principal rotating axis |
PrincipalScalingDirection | Returns or sets the principal scaling direction |
ProportionalAllU | Returns or sets a value indicating whether to use all poles in U direction during the proportional movement |
ProportionalAllV | Returns or sets a value indicating whether to use all poles in V direction during the proportional movement |
ProportionalFallOffScale | Returns or sets the proportional fall off scale |
ProportionalMoveAfterU | Returns or sets a value indicating the pole number after u to participate in the proportional movement |
ProportionalMoveAfterV | Returns or sets a value indicating the pole number after v to participate in the proportional movement |
ProportionalMoveBeforeU | Returns or sets a value indicating the pole number before u to participate in the proportional movement |
ProportionalMoveBeforeV | Returns or sets a value indicating the pole number before v to participate in the proportional movement |
ProportionalPoleControlOption | Returns or sets the proportional pole control type |
RotatingArbitraryPlane | Returns or sets the rotating arbitrary plane |
RotatingArbitraryVector | Returns or sets the rotating arbitrary vector |
RotatingAxis | Returns or sets the rotating axis |
RotatingPivot | Returns or sets the rotating pivot |
RotatingPivotPoint | Returns or sets the rotating pivot point |
ScalingArbitraryPlane | Returns or sets the scaling arbitrary plane |
ScalingArbitraryVector | Returns or sets the scaling arbitrary vector |
ScalingCenter | Returns or sets the scaling center |
ScalingCenterPoint | Returns or sets the scaling center point |
ScalingDirection | Returns or sets the scaling direction |
SurfaceRange | Returns the surface range |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the editing type |
XformOX | Returns the orient express object |
XformObjects | Returns the object to be transformed. |
Methods¶
Method | Description |
---|---|
ChangeDegree | Changes degree of the selected xform object |
ChangeDegreeWithParameters | Changes degree of the selected xform object with desired parameters |
ChangeFlexibility | Changes flexibility of the selected xform object |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
ConvertParameters | Converts parameters of the feature that owns selected xform object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EndLockRegion | End Lock Region operation to the selected xform object |
FallOffReset | Reset the fall off scale |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
InsertKnot | Inserts knot in the selected xform object |
InsertKnots | Insert knots |
InsertPole | Inserts a pole in the selected xform object |
LockRegionNextObject | Move to next object in Lock Region method when more than one objected are in editing |
ProportionalReset | Reset the proportional scale |
RebaseOriginalGeometry | Replaces the original geometry data of an entity with the current deformed geometry data |
RemovePole | Inserts a pole in the selected xform object |
RestoreParentFace | Restore the parent face of a selection face |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetPoleEditType | Update pole status of the selected BSpine curve |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpdateLockRegionGeometry | Update lock region geometry with current geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AdvancedMethod¶
-
StudioXformBuilderEx.
AdvancedMethod
¶ Returns or sets the advanced method
-------------------------------------
Getter Method
Signature
AdvancedMethod()
Returns: Return type: NXOpen.Features.StudioXformBuilderExAdvancedMethodType
New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Features.StudioXformBuilderEx.AdvancedMethodOption
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
AdvancedMethod(advancedMethod)
Parameters: advancedMethod ( NXOpen.Features.StudioXformBuilderExAdvancedMethodType
) –New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Features.StudioXformBuilderEx.AdvancedMethodOption
instead.License requirements: studio_free_form (“STUDIO FREE FORM”)
AdvancedMethodOption¶
-
StudioXformBuilderEx.
AdvancedMethodOption
¶ Returns or sets the advanced method
-------------------------------------
Getter Method
Signature
AdvancedMethodOption()
Returns: Return type: NXOpen.Features.StudioXformBuilderExAdvancedMethodOptionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvancedMethodOption(advancedMethod)
Parameters: advancedMethod ( NXOpen.Features.StudioXformBuilderExAdvancedMethodOptionType
) –New in version NX8.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CanUseFaceFinder¶
-
StudioXformBuilderEx.
CanUseFaceFinder
¶ Returns or sets the using face finder flag
-------------------------------------
Getter Method
Signature
CanUseFaceFinder()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanUseFaceFinder(canUseFaceFinder)
Parameters: canUseFaceFinder (bool) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ContinuityUMax¶
-
StudioXformBuilderEx.
ContinuityUMax
¶ Returns the continuity at U maximum
-------------------------------------
Getter Method
Signature
ContinuityUMax()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ContinuityUMin¶
-
StudioXformBuilderEx.
ContinuityUMin
¶ Returns the continuity at U minimum
-------------------------------------
Getter Method
Signature
ContinuityUMin()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ContinuityVMax¶
-
StudioXformBuilderEx.
ContinuityVMax
¶ Returns the continuity at V maximum
-------------------------------------
Getter Method
Signature
ContinuityVMax()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ContinuityVMin¶
-
StudioXformBuilderEx.
ContinuityVMin
¶ Returns the continuity at V minimum
-------------------------------------
Getter Method
Signature
ContinuityVMin()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ControlPoleManager¶
-
StudioXformBuilderEx.
ControlPoleManager
¶ Returns the control pole manager
-------------------------------------
Getter Method
Signature
ControlPoleManager()
Returns: Return type: NXOpen.GeometricUtilities.ControlPoleManagerData
New in version NX6.0.0.
License requirements: None.
CurveRange¶
-
StudioXformBuilderEx.
CurveRange
¶ Returns the curve range
-------------------------------------
Getter Method
Signature
CurveRange()
Returns: Return type: NXOpen.GeometricUtilities.CurveRangeBuilder
New in version NX6.0.0.
License requirements: None.
DegreesAndSegmentsOrPatches¶
-
StudioXformBuilderEx.
DegreesAndSegmentsOrPatches
¶ Returns the degrees and segments or patches
-------------------------------------
Getter Method
Signature
DegreesAndSegmentsOrPatches()
Returns: Return type: NXOpen.GeometricUtilities.DegreesAndSegmentsOrPatchesBuilder
New in version NX6.0.0.
License requirements: None.
ExtractMethod¶
-
StudioXformBuilderEx.
ExtractMethod
¶ Returns or sets the b-surface extraction method
-------------------------------------
Getter Method
Signature
ExtractMethod()
Returns: Return type: NXOpen.Features.StudioXformBuilderExExtrationMethodType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtractMethod(extractMethod)
Parameters: extractMethod ( NXOpen.Features.StudioXformBuilderExExtrationMethodType
) –New in version NX8.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ExtractTolerance¶
-
StudioXformBuilderEx.
ExtractTolerance
¶ Returns or sets the value indicating a tolerance to be used to extract a b-surface from a selection face
-------------------------------------
Getter Method
Signature
ExtractTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtractTolerance(extractTolerance)
Parameters: extractTolerance (float) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FaceFinder¶
-
StudioXformBuilderEx.
FaceFinder
¶ Returns the face finder
-------------------------------------
Getter Method
Signature
FaceFinder()
Returns: Return type: NXOpen.Features.FaceRecognitionBuilder
New in version NX7.5.0.
License requirements: None.
FallOffScale¶
-
StudioXformBuilderEx.
FallOffScale
¶ Returns or sets the fall off scale
-------------------------------------
Getter Method
Signature
FallOffScale()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FallOffScale(fallOffScale)
Parameters: fallOffScale (float) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FeatureSaveMethod¶
-
StudioXformBuilderEx.
FeatureSaveMethod
¶ Returns or sets the feature save method
-------------------------------------
Getter Method
Signature
FeatureSaveMethod()
Returns: Return type: NXOpen.Features.StudioXformBuilderExFeatureType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureSaveMethod(featureSaveMethod)
Parameters: featureSaveMethod ( NXOpen.Features.StudioXformBuilderExFeatureType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertKnotDirection¶
-
StudioXformBuilderEx.
InsertKnotDirection
¶ Returns or sets the insert knot direction
-------------------------------------
Getter Method
Signature
InsertKnotDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderExInsertKnotDirectionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsertKnotDirection(insertKnotDirection)
Parameters: insertKnotDirection ( NXOpen.Features.StudioXformBuilderExInsertKnotDirectionType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertKnotParameter¶
-
StudioXformBuilderEx.
InsertKnotParameter
¶ Returns or sets the parameter where to insert knots
-------------------------------------
Getter Method
Signature
InsertKnotParameter()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsertKnotParameter(insertKnotSlider)
Parameters: insertKnotSlider (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
IsSingleSelection¶
-
StudioXformBuilderEx.
IsSingleSelection
¶ Returns or sets the single selection flag
-------------------------------------
Getter Method
Signature
IsSingleSelection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSingleSelection(singleSelectionFlag)
Parameters: singleSelectionFlag (bool) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
KeepAllContinuity¶
-
StudioXformBuilderEx.
KeepAllContinuity
¶ Returns or sets a value indicating whether to keep all continuity
-------------------------------------
Getter Method
Signature
KeepAllContinuity()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepAllContinuity(keepAllContinuity)
Parameters: keepAllContinuity (bool) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LockPoles¶
-
StudioXformBuilderEx.
LockPoles
¶ Returns or sets a value indicating whether to lock poles in boundary constraints
-------------------------------------
Getter Method
Signature
LockPoles()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockPoles(lockPoles)
Parameters: lockPoles (bool) – New in version NX8.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LockRegionUEndFlexibility¶
-
StudioXformBuilderEx.
LockRegionUEndFlexibility
¶ Returns or sets the lock region flexibility at U end
-------------------------------------
Getter Method
Signature
LockRegionUEndFlexibility()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockRegionUEndFlexibility(lockRegionUEndFlexibility)
Parameters: lockRegionUEndFlexibility (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LockRegionUStartFlexibility¶
-
StudioXformBuilderEx.
LockRegionUStartFlexibility
¶ Returns or sets the lock region flexibility at U start
-------------------------------------
Getter Method
Signature
LockRegionUStartFlexibility()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockRegionUStartFlexibility(lockRegionUStartFlexibility)
Parameters: lockRegionUStartFlexibility (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LockRegionVEndFlexibility¶
-
StudioXformBuilderEx.
LockRegionVEndFlexibility
¶ Returns or sets the lock region flexibility at V end
-------------------------------------
Getter Method
Signature
LockRegionVEndFlexibility()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockRegionVEndFlexibility(lockRegionVEndFlexibility)
Parameters: lockRegionVEndFlexibility (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LockRegionVStartFlexibility¶
-
StudioXformBuilderEx.
LockRegionVStartFlexibility
¶ Returns or sets the lock region flexibility at V start
-------------------------------------
Getter Method
Signature
LockRegionVStartFlexibility()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockRegionVStartFlexibility(lockRegionVStartFlexibility)
Parameters: lockRegionVStartFlexibility (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
MovementArbitraryPlane¶
-
StudioXformBuilderEx.
MovementArbitraryPlane
¶ Returns or sets the movement arbitrary plane
-------------------------------------
Getter Method
Signature
MovementArbitraryPlane()
Returns: Return type: NXOpen.Plane
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MovementArbitraryPlane(movementArbitraryPlane)
Parameters: movementArbitraryPlane ( NXOpen.Plane
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
MovementArbitraryVector¶
-
StudioXformBuilderEx.
MovementArbitraryVector
¶ Returns or sets the movement arbitrary vector
-------------------------------------
Getter Method
Signature
MovementArbitraryVector()
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MovementArbitraryVector(movementArbitraryVector)
Parameters: movementArbitraryVector ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
MovementMethod¶
-
StudioXformBuilderEx.
MovementMethod
¶ Returns or sets the movement method
-------------------------------------
Getter Method
Signature
MovementMethod()
Returns: Return type: NXOpen.Features.StudioXformBuilderExMovementMethodType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MovementMethod(movementMethod)
Parameters: movementMethod ( NXOpen.Features.StudioXformBuilderExMovementMethodType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PlanarizeArbitraryPlane¶
-
StudioXformBuilderEx.
PlanarizeArbitraryPlane
¶ Returns or sets the planarize arbitrary plane
-------------------------------------
Getter Method
Signature
PlanarizeArbitraryPlane()
Returns: Return type: NXOpen.Plane
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlanarizeArbitraryPlane(planarizeArbitraryPlane)
Parameters: planarizeArbitraryPlane ( NXOpen.Plane
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PlanarizeDirection¶
-
StudioXformBuilderEx.
PlanarizeDirection
¶ Returns or sets the planarize direction
-------------------------------------
Getter Method
Signature
PlanarizeDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderExPlanarizeDirectionType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlanarizeDirection(planarizeDirection)
Parameters: planarizeDirection ( NXOpen.Features.StudioXformBuilderExPlanarizeDirectionType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PlanarizeMethod¶
-
StudioXformBuilderEx.
PlanarizeMethod
¶ Returns or sets the planarize method
-------------------------------------
Getter Method
Signature
PlanarizeMethod()
Returns: Return type: NXOpen.Features.StudioXformBuilderExPlanarizeMethodType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlanarizeMethod(planarizeMethod)
Parameters: planarizeMethod ( NXOpen.Features.StudioXformBuilderExPlanarizeMethodType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PlanarizeProjectionPlane¶
-
StudioXformBuilderEx.
PlanarizeProjectionPlane
¶ Returns or sets the planarize projection plane
-------------------------------------
Getter Method
Signature
PlanarizeProjectionPlane()
Returns: Return type: NXOpen.Features.StudioXformBuilderExPlanarizeProjectionPlaneType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlanarizeProjectionPlane(planarizeProjectionPlane)
Parameters: planarizeProjectionPlane ( NXOpen.Features.StudioXformBuilderExPlanarizeProjectionPlaneType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PrincipalMovementDirection¶
-
StudioXformBuilderEx.
PrincipalMovementDirection
¶ Returns or sets the principal movement direction
-------------------------------------
Getter Method
Signature
PrincipalMovementDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderExPrincipalMovementDirectionType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrincipalMovementDirection(principalMovementDirection)
Parameters: principalMovementDirection ( NXOpen.Features.StudioXformBuilderExPrincipalMovementDirectionType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PrincipalRotatingAxis¶
-
StudioXformBuilderEx.
PrincipalRotatingAxis
¶ Returns or sets the principal rotating axis
-------------------------------------
Getter Method
Signature
PrincipalRotatingAxis()
Returns: Return type: NXOpen.Features.StudioXformBuilderExPrincipalRotatingAxisType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrincipalRotatingAxis(principalRotatingAxis)
Parameters: principalRotatingAxis ( NXOpen.Features.StudioXformBuilderExPrincipalRotatingAxisType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PrincipalScalingDirection¶
-
StudioXformBuilderEx.
PrincipalScalingDirection
¶ Returns or sets the principal scaling direction
-------------------------------------
Getter Method
Signature
PrincipalScalingDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderExPrincipalScalingDirectionType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrincipalScalingDirection(principalScalingDirection)
Parameters: principalScalingDirection ( NXOpen.Features.StudioXformBuilderExPrincipalScalingDirectionType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalAllU¶
-
StudioXformBuilderEx.
ProportionalAllU
¶ Returns or sets a value indicating whether to use all poles in U direction during the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalAllU()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalAllU(proportionalAllU)
Parameters: proportionalAllU (bool) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalAllV¶
-
StudioXformBuilderEx.
ProportionalAllV
¶ Returns or sets a value indicating whether to use all poles in V direction during the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalAllV()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalAllV(proportionalAllV)
Parameters: proportionalAllV (bool) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalFallOffScale¶
-
StudioXformBuilderEx.
ProportionalFallOffScale
¶ Returns or sets the proportional fall off scale
-------------------------------------
Getter Method
Signature
ProportionalFallOffScale()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Features.StudioXformBuilderEx.FallOffScale
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalFallOffScale(proportionalFallOffScale)
Parameters: proportionalFallOffScale (float) – New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Features.StudioXformBuilderEx.FallOffScale
instead.License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalMoveAfterU¶
-
StudioXformBuilderEx.
ProportionalMoveAfterU
¶ Returns or sets a value indicating the pole number after u to participate in the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalMoveAfterU()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalMoveAfterU(proportionalMoveAfterU)
Parameters: proportionalMoveAfterU (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalMoveAfterV¶
-
StudioXformBuilderEx.
ProportionalMoveAfterV
¶ Returns or sets a value indicating the pole number after v to participate in the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalMoveAfterV()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalMoveAfterV(proportionalMoveAfterV)
Parameters: proportionalMoveAfterV (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalMoveBeforeU¶
-
StudioXformBuilderEx.
ProportionalMoveBeforeU
¶ Returns or sets a value indicating the pole number before u to participate in the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalMoveBeforeU()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalMoveBeforeU(proportionalMoveBeforeU)
Parameters: proportionalMoveBeforeU (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalMoveBeforeV¶
-
StudioXformBuilderEx.
ProportionalMoveBeforeV
¶ Returns or sets a value indicating the pole number before v to participate in the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalMoveBeforeV()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalMoveBeforeV(proportionalMoveBeforeV)
Parameters: proportionalMoveBeforeV (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalPoleControlOption¶
-
StudioXformBuilderEx.
ProportionalPoleControlOption
¶ Returns or sets the proportional pole control type
-------------------------------------
Getter Method
Signature
ProportionalPoleControlOption()
Returns: Return type: NXOpen.Features.StudioXformBuilderExProportionalPoleControlType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalPoleControlOption(poleControlOption)
Parameters: poleControlOption ( NXOpen.Features.StudioXformBuilderExProportionalPoleControlType
) –New in version NX8.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RotatingArbitraryPlane¶
-
StudioXformBuilderEx.
RotatingArbitraryPlane
¶ Returns or sets the rotating arbitrary plane
-------------------------------------
Getter Method
Signature
RotatingArbitraryPlane()
Returns: Return type: NXOpen.Plane
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotatingArbitraryPlane(rotatingArbitraryPlane)
Parameters: rotatingArbitraryPlane ( NXOpen.Plane
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RotatingArbitraryVector¶
-
StudioXformBuilderEx.
RotatingArbitraryVector
¶ Returns or sets the rotating arbitrary vector
-------------------------------------
Getter Method
Signature
RotatingArbitraryVector()
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotatingArbitraryVector(rotatingArbitraryVector)
Parameters: rotatingArbitraryVector ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RotatingAxis¶
-
StudioXformBuilderEx.
RotatingAxis
¶ Returns or sets the rotating axis
-------------------------------------
Getter Method
Signature
RotatingAxis()
Returns: Return type: NXOpen.Features.StudioXformBuilderExRotatingAxisType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotatingAxis(rotatingAxis)
Parameters: rotatingAxis ( NXOpen.Features.StudioXformBuilderExRotatingAxisType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RotatingPivot¶
-
StudioXformBuilderEx.
RotatingPivot
¶ Returns or sets the rotating pivot
-------------------------------------
Getter Method
Signature
RotatingPivot()
Returns: Return type: NXOpen.Features.StudioXformBuilderExRotatingPivotType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotatingPivot(rotatingPivot)
Parameters: rotatingPivot ( NXOpen.Features.StudioXformBuilderExRotatingPivotType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RotatingPivotPoint¶
-
StudioXformBuilderEx.
RotatingPivotPoint
¶ Returns or sets the rotating pivot point
-------------------------------------
Getter Method
Signature
RotatingPivotPoint()
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotatingPivotPoint(rotatingPivotPoint)
Parameters: rotatingPivotPoint ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ScalingArbitraryPlane¶
-
StudioXformBuilderEx.
ScalingArbitraryPlane
¶ Returns or sets the scaling arbitrary plane
-------------------------------------
Getter Method
Signature
ScalingArbitraryPlane()
Returns: Return type: NXOpen.Plane
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingArbitraryPlane(scalingArbitraryPlane)
Parameters: scalingArbitraryPlane ( NXOpen.Plane
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ScalingArbitraryVector¶
-
StudioXformBuilderEx.
ScalingArbitraryVector
¶ Returns or sets the scaling arbitrary vector
-------------------------------------
Getter Method
Signature
ScalingArbitraryVector()
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingArbitraryVector(scalingArbitraryVector)
Parameters: scalingArbitraryVector ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ScalingCenter¶
-
StudioXformBuilderEx.
ScalingCenter
¶ Returns or sets the scaling center
-------------------------------------
Getter Method
Signature
ScalingCenter()
Returns: Return type: NXOpen.Features.StudioXformBuilderExScalingCenterType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingCenter(scalingCenter)
Parameters: scalingCenter ( NXOpen.Features.StudioXformBuilderExScalingCenterType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ScalingCenterPoint¶
-
StudioXformBuilderEx.
ScalingCenterPoint
¶ Returns or sets the scaling center point
-------------------------------------
Getter Method
Signature
ScalingCenterPoint()
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingCenterPoint(scalingCenterPoint)
Parameters: scalingCenterPoint ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ScalingDirection¶
-
StudioXformBuilderEx.
ScalingDirection
¶ Returns or sets the scaling direction
-------------------------------------
Getter Method
Signature
ScalingDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderExScalingDirectionType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingDirection(scalingDirection)
Parameters: scalingDirection ( NXOpen.Features.StudioXformBuilderExScalingDirectionType
) –New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SurfaceRange¶
-
StudioXformBuilderEx.
SurfaceRange
¶ Returns the surface range
-------------------------------------
Getter Method
Signature
SurfaceRange()
Returns: Return type: NXOpen.GeometricUtilities.SurfaceRangeBuilder
New in version NX6.0.0.
License requirements: None.
Type¶
-
StudioXformBuilderEx.
Type
¶ Returns or sets the editing type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.StudioXformBuilderExTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.StudioXformBuilderExTypes
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
XformOX¶
-
StudioXformBuilderEx.
XformOX
¶ Returns the orient express object
-------------------------------------
Getter Method
Signature
XformOX()
Returns: Return type: NXOpen.GeometricUtilities.OrientXpressBuilder
New in version NX7.0.0.
License requirements: None.
XformObjects¶
-
StudioXformBuilderEx.
XformObjects
¶ Returns the object to be transformed.
Any face having b-surface type geometry or curve having b-curve geometry can be transformed.
-------------------------------------
Getter Method
Signature
XformObjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
ChangeDegree¶
-
StudioXformBuilderEx.
ChangeDegree
¶ Changes degree of the selected xform object
Signature
ChangeDegree(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to change degree ofNew in version NX6.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Features.StudioXformBuilderEx.ChangeDegreeWithParameters
instead.License requirements: studio_free_form (“STUDIO FREE FORM”)
ChangeDegreeWithParameters¶
-
StudioXformBuilderEx.
ChangeDegreeWithParameters
¶ Changes degree of the selected xform object with desired parameters
Signature
ChangeDegreeWithParameters(xformObject, uDegree, vDegree, uPatch, vPatch)
Parameters: - xformObject (
NXOpen.NXObject
) – the selected face or curve to change degree of - uDegree (int) – the U degree to change to, valid range is [1, 24]
- vDegree (int) – the V degree to change to, valid range is [1, 24]
- uPatch (int) – the U patch to change to, valid value is greater than 1
- vPatch (int) – the V patch to change to, valid value is greater than 1
New in version NX8.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
- xformObject (
ChangeFlexibility¶
-
StudioXformBuilderEx.
ChangeFlexibility
¶ Changes flexibility of the selected xform object
Signature
ChangeFlexibility(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to change flexibility ofNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ConvertParameters¶
-
StudioXformBuilderEx.
ConvertParameters
¶ Converts parameters of the feature that owns selected xform object.
Converts through points studio spline feature to by poles feature, otherwise removes parameters of the feature.
Signature
ConvertParameters(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to convert pameters fromNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
EndLockRegion¶
-
StudioXformBuilderEx.
EndLockRegion
¶ End Lock Region operation to the selected xform object
Signature
EndLockRegion(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to end Lock Region operation ofNew in version NX8.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FallOffReset¶
-
StudioXformBuilderEx.
FallOffReset
¶ Reset the fall off scale
Signature
FallOffReset()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertKnot¶
-
StudioXformBuilderEx.
InsertKnot
¶ Inserts knot in the selected xform object
Signature
InsertKnot(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to insert knot inNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertKnots¶
-
StudioXformBuilderEx.
InsertKnots
¶ Insert knots
Signature
InsertKnots()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertPole¶
-
StudioXformBuilderEx.
InsertPole
¶ Inserts a pole in the selected xform object
Signature
InsertPole(xformObject, poleIndex, insertType, direction, location)
Parameters: - xformObject (
NXOpen.NXObject
) – the selected face or curve to insert pole to - poleIndex (int) – which pole index to begin insert to
- insertType (
NXOpen.Features.StudioXformBuilderExInsertPoleType
) – Insert type - direction (
NXOpen.Features.StudioXformBuilderExSurfaceDirectionType
) – U or V direction a pole row on a surface is inserted, pass U direction for a curve - location (float) – a point between 2 poles to indicate where a pole should be inserted, express as %
New in version NX8.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
- xformObject (
LockRegionNextObject¶
-
StudioXformBuilderEx.
LockRegionNextObject
¶ Move to next object in Lock Region method when more than one objected are in editing
Signature
LockRegionNextObject()
New in version NX8.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalReset¶
-
StudioXformBuilderEx.
ProportionalReset
¶ Reset the proportional scale
Signature
ProportionalReset()
New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Features.StudioXformBuilderEx.FallOffReset
instead.License requirements: studio_free_form (“STUDIO FREE FORM”)
RebaseOriginalGeometry¶
-
StudioXformBuilderEx.
RebaseOriginalGeometry
¶ Replaces the original geometry data of an entity with the current deformed geometry data
Signature
RebaseOriginalGeometry(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to rebase the geometry data ofNew in version NX8.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RemovePole¶
-
StudioXformBuilderEx.
RemovePole
¶ Inserts a pole in the selected xform object
Signature
RemovePole(xformObject, poleIndex, direction)
Parameters: - xformObject (
NXOpen.NXObject
) – the selected face or curve to remove pole from - poleIndex (int) – which pole index to remove
- direction (
NXOpen.Features.StudioXformBuilderExSurfaceDirectionType
) – U or V direction a pole row on a surface is removed, pass U direction for a curve
New in version NX8.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
- xformObject (
RestoreParentFace¶
-
StudioXformBuilderEx.
RestoreParentFace
¶ Restore the parent face of a selection face
Signature
RestoreParentFace()
New in version NX7.5.2.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetPoleEditType¶
-
StudioXformBuilderEx.
SetPoleEditType
¶ Update pole status of the selected BSpine curve
Signature
SetPoleEditType(xformObject, index, poleEditType)
Parameters: - xformObject (
NXOpen.NXObject
) – spline being edited - index (int) – index of a pole being edited
- poleEditType (
NXOpen.Features.StudioXformBuilderExPoleEditType
) – the pole edit type
New in version NX7.5.4.
License requirements: studio_free_form (“STUDIO FREE FORM”)
- xformObject (
UpdateLockRegionGeometry¶
-
StudioXformBuilderEx.
UpdateLockRegionGeometry
¶ Update lock region geometry with current geometry
Signature
UpdateLockRegionGeometry(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to change flexibility ofNew in version NX6.0.2.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
StudioXformBuilderEx.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.