SurfaceRangeBuilder Class¶
-
class
NXOpen.GeometricUtilities.
SurfaceRangeBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the surface range and anchor builder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AnchorPosition | Returns or sets the anchor position |
Tag | Returns the Tag for this object. |
UEnd | Returns the u end |
UStart | Returns the u start |
VEnd | Returns the v end |
VStart | Returns the v start |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SurfaceRangeBuilderAnchorPositionType Enumeration | Represents the anchor position type |
Property Detail¶
AnchorPosition¶
-
SurfaceRangeBuilder.
AnchorPosition
¶ Returns or sets the anchor position
-------------------------------------
Getter Method
Signature
AnchorPosition()
Returns: Return type: NXOpen.GeometricUtilities.SurfaceRangeBuilderAnchorPositionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnchorPosition(anchorPosition)
Parameters: anchorPosition ( NXOpen.GeometricUtilities.SurfaceRangeBuilderAnchorPositionType
) –New in version NX6.0.0.
License requirements: None.
UEnd¶
-
SurfaceRangeBuilder.
UEnd
¶ Returns the u end
-------------------------------------
Getter Method
Signature
UEnd()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: None.
UStart¶
-
SurfaceRangeBuilder.
UStart
¶ Returns the u start
-------------------------------------
Getter Method
Signature
UStart()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: None.
VEnd¶
-
SurfaceRangeBuilder.
VEnd
¶ Returns the v end
-------------------------------------
Getter Method
Signature
VEnd()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: None.
VStart¶
-
SurfaceRangeBuilder.
VStart
¶ Returns the v start
-------------------------------------
Getter Method
Signature
VStart()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SurfaceRangeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.