SurfaceRangeBuilderAnchorPositionType Enumeration¶
NXOpen.GeometricUtilities.SurfaceRangeBuilder.AnchorPositionType is an alias for NXOpen.GeometricUtilities.SurfaceRangeBuilderAnchorPositionType
-
class
NXOpen.GeometricUtilities.
SurfaceRangeBuilderAnchorPositionType
¶ Bases:
object
Represents the anchor position type
Enum Members
Enum Member Enum Member Description Center Anchor at the center of the surfaceVertex1 Anchor at the first corner of the surfaceVertex2 Anchor at the second corner of the surfaceVertex3 Anchor at the third corner of the surfaceVertex4 Anchor at the fourth corner of the surface-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-