StudioXformBuilderExPlanarizeProjectionPlaneType Enumeration¶
NXOpen.Features.StudioXformBuilderEx.PlanarizeProjectionPlaneType is an alias for NXOpen.Features.StudioXformBuilderExPlanarizeProjectionPlaneType
-
class
NXOpen.Features.
StudioXformBuilderExPlanarizeProjectionPlaneType
¶ Bases:
object
Represents the planarize projection plane type
Enum Members
Enum Member Enum Member Description YZ On Y-Z plane when planarizeXZ On X-Z plane when planarizeXY On X-Y plane when planarizePlane On arbitrary plane when planarize-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-