StudioXformBuilderExInsertPoleType Enumeration¶
NXOpen.Features.StudioXformBuilderEx.InsertPoleType is an alias for NXOpen.Features.StudioXformBuilderExInsertPoleType
-
class
NXOpen.Features.
StudioXformBuilderExInsertPoleType
¶ Bases:
object
Represents the insert pole type
Enum Members
Enum Member Enum Member Description Next Insert pole next to the selected polePrevious Insert pole previous to the selected pole-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-