Diagram editor overview
Polarion provides the Diagram Editor tool for creating and editing diagrams. You can use it to create and edit diagrams in:
The text of LiveDoc Documents
Work Items contained in Documents
The Description field of Work Items in the Table view of the Work Items topic of the portal
Rich Text type custom fields of Work Items
After inserting a new diagram, you can insert a caption above of below it. The Diagram Editor provides an extensive library of shapes and symbols that can be using to create a wide variety of diagram types.
The main capabilities and features of the Diagram Editor include: