Create a new diagram
Create a new diagram in a LiveDoc Document
Open the project containing the Document, and in Navigation browse to the space and Document, clicking on the Document to open it in the Document Editor.
Alternatively, you can use the Search box in Navigation to search for the desired Document.
In the Document, create a new line at the place you want to insert a new diagram. If you want to place the diagram inside a Work Item, place the caret inside the Work Item and use the Insert menu on the Work Item icon in the Document's left margin to add a new line above or below the current caret position.
On the Diagram Editor toolbar, click on the Insert drop-down menu and choose Diagram.
Insert a diagram in the Table view of Work Items
In the project containing the Work Item, select Work Items in Navigation to open the Work Item Tracker. If the Table view is not the current view when the page opens, select that view.
Browse or query Work Items, and in the upper pane of the Table view select the item in which you want to insert a diagram.
Scroll the lower pane of the Table view until you can see the Description field of the selected Work Item.
Click on the header to open the field for editing.
On the Description field toolbar, click the Insert Diagram button.
Table view. |
Description field. |
You can also create and edit diagrams in custom fields of the Rich Text type. Such fields have a formatting toolbar like that of the Description field.