Print a diagram
The File menu of the Diagram Editor includes the Page Setup command and the Print command. Use these to set up printing of the current diagram and print it to any accessible local or network printer. Only the currently open diagram is printed, not the Document that contains it.