Captions
You can add a caption to several types of content in Polarion.
Images (in Documents, Work Items, table cells)
Tables (in Documents, Work Items)
Diagrams (in Documents, Work Items, table cells)
To add a caption, click on the item, then click Add Caption on the pop-up menu. In the Add Caption dialog box, you can:
Enter caption text in the Caption field.
Select whether the caption should appear above or below the item by clicking the appropriate icon in Show At.
Select a label that describes the item type, or add a new label. The value set in this field is prefixed to the value in the Caption field.
You can optionally add a new label and apply it when captioning images, diagrams or tables. For example, you might create a label mamed Citation and specify it when adding a caption to some items. You could then insert a Table of Citations in your Document. Note that tables of figures, tables of tables, and tables of custom-labeled items appear only in documents generated by export to PDF and Round-trip for Microsoft Word. A placeholder appears in your Polarion Document.
A custom caption label appears in the Label list when the Document contains a caption that uses it. To remove a custom label, remove all captions that use it and refresh your browser.
Captions and On-demand Work Item loading
When on-demand Work Item loading is enabled by administrators in the system configuration it affects captions as follows:
If the Document's Work Item Presentation configuration is set up for Test Steps or rich-text type Custom Fields to be visible, then all caption numbers appear as a hash mark (#). They are replaced with the correct numbers when exported.
If the Document's Work Item Presentation configuration does not contain Test Steps or Custom Fields as outlined above, then caption numbers will display, even with on-demand Work Item loading enabled.
Visible caption numbers will display correctly even if previous captions from the same sequence have not finished loading.
When on-demand Work Item loading is disabled, then all caption numbers will appear in the Document, but they may take a while to load if the Document is a large one with many Work Items and/or captioned content.
Image |
Table |
Diagram |
There are two default caption label values: Table and Figure. These values determine if a caption is included in a Table of Figures or a Table of Tables, if these are inserted into a Document.