Edit a Diagram
When you edit a Document or a Work Item field containing a diagram, the diagram is not automatically editable. An additional action is required to open the diagram in the Diagram Editor. However, you can resize the diagram without opening it in the Diagram Editor.
Edit an existing diagram in a Work Item's Description field
Click the field header to open the field for editing.
In field, click anywhere on the diagram.
Click the Edit button that appears on the diagram to launch the Diagram Editor.
Edit an existing diagram in a Document
Click anywhere on the diagram.
Click the Edit button that appears on the diagram to launch the Diagram Editor.
Resize a Diagram
To resize an existing diagram, follow the same steps as for editing, except click the Resize button.
Enter the new pixel dimensions in the Resize Image dialog. Note that the aspect ratio is automatically maintained unless you toggle off the Keep Aspect Ratio button.