Tab Statistics (material flow objects)
The material flow objects show the most important statistical data on the tab Statistics when you select the check box Resource statistics and click Apply. Note that the values for Waiting, Working, Blocked, Setting-Up, Failed, Powering up/down, Stopped, Paused, and Unplanned should add up to 100 percent.
Working | Shows the portion of the statistics collection period during which the object was Working. | |
Setting-up | Shows the portion of the statistics collection period during which the object was Setting-Up. | |
Waiting | Shows the portion of the statistics collection period during which the object was Waiting. | |
Blocked | Shows the portion of the statistics collection period during which the object was Blocked. | |
Powering up/down | Shows the portion of the statistics collection period during which the object was Powering up/down. | |
Failed | Shows the portion of the statistics collection period during which the object was Failed. | |
Stopped | Shows the portion of the statistics collection period during which the object was Stopped by a LockoutZone. | |
Paused | Shows the portion of the statistics collection period during which the object was Paused. | |
Unplanned | Shows the portion of the statistics collection period during which the object was Unplanned, i.e., is not scheduled to work to the statistics collection period. | |
Relative occupation | Shows the sum of all dwelling times of all MUs during the statistics collection period during which the object was not paused and not failed. This sum is then divided by the capacity and the entire statistics collection period without pauses and failures. | |
Relatively empty | Shows the portion of the statistics collection period during which the object was Empty in relation to the time during which the object was available. | |
Relatively full | Shows the portion of the statistics collection period during which all temporary storage places of the Buffer were occupied in relation to the time during which the object was available. | |
Contents | Shows the number of MUs, which are located on the object. When a part enters the object, it only counts the part itself, not its contents: When a Container transporting several parts enters the object, the number of entries increases by 1, not by the number of parts located on the Container! | |
Minimum contents | Shows the minimum number of MUs that was located on the object. When a part enters the object, it only counts the part itself, not its contents: When a Container several parts enters the object, the number of entries increases by 1, not by the number of parts located on the Container! | |
Maximum contents | Shows the maximum number of MUs that was located on the object. When a part enters the object, it only counts the part itself, not its contents: When a Container transporting several parts enters the object, the number of entries increases by 1, not by the number of parts located on the Container! | |
Entries | Shows the number of MUs that entered the object. When a part enters the object, it only counts the part itself, not its contents: When a Container transporting several parts enters the object, the number of entries increases by 1, not by the number of parts located on the Container! | |
Exits | Shows the number of MUs that exited the object. When a part exits the object, it only counts the part itself, not its contents: When a Transporter transporting several MUs leaves the object, the number of exits increases by 1, not by the number of MUs which the Transporter transports! |
To view more detailed statistics of the material flow object in the Statistics Report, click the object in the Frame, and press F6 (Show Statistics Report), or click Show Statistics Report on the Home ribbon tab.
You can also click the object in the Frame with the right mouse button and select Show Statistics Report on the context menu.
You can also show energy statistics values by clicking Energy Statistics .
Related Topics
Methods for Accessing Statistics of the Material Flow Objects |