Unplanned (general description)
A material flow resource is unplanned, when you did not enter a time in the ShiftCalendar during which it is going to work.
Note:
Plant Simulation only increments the counter for pauses and unplanned times when the duration of the pause or shift pause is not 0.
Note:
When a Worker/Exporter is brokered to the paused station, it remains brokered to the station while it is paused. Statistics of the Worker/Exporter does not count this time as waiting.
The LED of an unplanned station is light blue .
SimTalk
Related Topics