Waiting (described)
A material flow resource is waiting when:
It is not Paused.
It is not Failed.
It is not Stopped.
It is not fully occupied.
An occupied station is not working, for example, when it is waiting for an Exporter.
It is not Setting-Up.
Note:The read-only attribute ResWaiting returns the state waiting of the resource.
The LED of a station that is waiting for an Exporter/Worker is orange .
The Statistics Report shows the Waiting Time below Resource Statistics of Stationary Resources.
SimTalk
Related Topics