Statistics Report (described)
To open the statistics report, which shows Resource Statistics data of the selected object or class, select View > Show Statistics Report in the dialog of the object.
You can also right-click the object in the Frame and select Show Statistics Report or you can press F6 in the Frame.
To show statistics data of several objects, select them (Shift+click, or drag a marquee over them) in the Frame and press F6. To add one or several objects to an open report, select it/them and press F6. The report adds the statistics of the objects, which you selected to the drop-down list. To jump to any of the topics in the report, which interest you, select that topic from the drop-down list:
The report then shows that topic by itself on the page. To print just this page, click the button Print This Page. To show all topics in the display window, click Show All. To print the entire report, click Print.
To show a Tooltip with the name of the respective read-only attribute for this statistics value, drag the mouse over the column header.
To save the report as an HTML file (*.htm or *.html) or as a text file (*.txt) click Save. Enter a name for the file and select the folder into which you want to save it.
To update the report with the current values, click Refresh.
To show the name of the statistics method , which matches the value shown in a column of a table, as at tooltip, drag the mouse over the column header and leave it there.
The report can show:
The individual material flow objects also show the most important statistics values on the Tab Statistics.
Also compare Viewing the Statistics Report in the Step-by-Step Help.
Related Topic
Methods for Accessing Statistics of the Material Flow Objects