Energy Statistics - Energy Statistics
This topic provides details about Energy Statistics of the material flow object(s).
The energy states of the material flow objects differ from the resource states with the same name. The values for the resource states refer to the statistics collection period, while the values for the energy states refer to the total energy consumption.
A bar with this color in the Statistics Report and the Chart | Looks like this | Means that the object is |
---|---|---|
green | working | |
brown | setting-up | |
yellow | operational | |
red | failed | |
light gray | on standby | |
dark gray | off |
The column | Shows | Read-only attribute |
---|---|---|
Total consumption | the sum of the total energy consumption. | |
Working | the portion of the total energy consumption during which the object was working. | |
Setting-up | the portion of the total energy consumption during which the object was setting-up. | |
Operational | the portion of the total energy consumption during which the object was operational. | |
Failed | the portion of the total energy consumption during which the object was failed. | |
Standby | the portion of the total energy consumption during which the object was on standby. | |
Off | the portion of the total energy consumption during which the object was off. |