Show Statistics Report (in Frame)
To show the statistics of the selected object in the Statistics Report, select this command or press F6.
To show the statistics of several objects, select them (Shift+click or drag a marquee over them) and press F6.
To add one or several objects to an open report, select it/them and press F6.
The report adds the statistics of the objects, which you selected to the drop-down list. To jump to any of the topics, which interest you, select that topic from the drop-down list:
Note that then the report just shows the page with this topic in the display window.
To save the report as an HTML file (*.htm or *.html) or as a text file (*.txt) click Save. Enter a name for the file and select the folder into which you want to save it.
To update the report with the current values, click Refresh.
To print the report, click Print.
Instead, you can also select View > Statistics Report in the dialog of the objects.
Related Topics
Related Topics
Context Menu of the Selected Object in the FrameArrange Icons (Frame)
Calculate Angles
Controls (in Frame)
Create Sensor (in Frame)
Create Tugger Train
Delete Sensor
Disable
Down One Level
Edit Display Panel (in Frame)
Edit Dialog (in Frame)
Edit Icons (in Frame)
Edit User-defined Attributes (in Frame)
Enable (in Frame)
Next Icon (in Frame)
Open (in Frame)
Open Class (in Frame)
Open Comment Window
Open Debugger
Open External Connections List
Open Origin (in Frame)
Open Sensor
Open Values Table
Open Without Control
Previous Icon (in Frame)
Rename (in Frame)
Reorder Successors
Reset Simulation (in Frame)
Run (Method)
Show (in Frame)
Show Assigned Objects (on context menu)
Show Attributes and Methods (in Frame)
Show Dialog (in Frame)
Show Exported Services
Show External Connected Objects
Show Structure (in Frame)
Start/Stop Simulation (button in Frame)
Start without Animation (in Frame)
Statistics Wizard
Type Info (in Frame)