Open External Connections List
To open the list, which shows the paths of the external connections in the Frame in which you inserted the Interface object, select this command.
Column 1 shows the Connector at the exit of the Frame, column 2 the name of the succeeding object.
Instead, you can also select View > External Connections in the dialog of the Interface.
Related Topics
Context Menu of the Selected Object in the FrameArrange Icons (Frame)
Calculate Angles
Controls (in Frame)
Create Sensor (in Frame)
Create Tugger Train
Delete Sensor
Disable
Down One Level
Edit Display Panel (in Frame)
Edit Dialog (in Frame)
Edit Icons (in Frame)
Edit User-defined Attributes (in Frame)
Enable (in Frame)
Next Icon (in Frame)
Open (in Frame)
Open Class (in Frame)
Open Comment Window
Open Debugger
Open Origin (in Frame)
Open Sensor
Open Values Table
Open Without Control
Previous Icon (in Frame)
Rename (in Frame)
Reorder Successors
Reset Simulation (in Frame)
Run (Method)
Show (in Frame)
Show Assigned Objects (on context menu)
Show Attributes and Methods (in Frame)
Show Dialog (in Frame)
Show Exported Services
Show External Connected Objects
Show Statistics Report (in Frame)
Show Structure (in Frame)
Start/Stop Simulation (button in Frame)
Start without Animation (in Frame)
Statistics Wizard
Type Info (in Frame)