Show Assigned Objects (on context menu)
To select the objects which are assigned to the LockoutZone or to the ShiftCalendar as resources in the Frame, select Show Assigned Objects.
Instead, you can also select View > Show Assigned Objects in the dialog of the LockoutZone.
Related Topics
Context Menu of the Selected Object in the FrameArrange Icons (Frame)
Calculate Angles
Controls (in Frame)
Create Sensor (in Frame)
Create Tugger Train
Delete Sensor
Disable
Down One Level
Edit Display Panel (in Frame)
Edit Dialog (in Frame)
Edit Icons (in Frame)
Edit User-defined Attributes (in Frame)
Enable (in Frame)
Next Icon (in Frame)
Open (in Frame)
Open Class (in Frame)
Open Comment Window
Open Debugger
Open External Connections List
Open Origin (in Frame)
Open Sensor
Open Values Table
Open Without Control
Previous Icon (in Frame)
Rename (in Frame)
Reorder Successors
Reset Simulation (in Frame)
Run (Method)
Show (in Frame)
Show Attributes and Methods (in Frame)
Show Dialog (in Frame)
Show Exported Services
Show External Connected Objects
Show Statistics Report (in Frame)
Show Structure (in Frame)
Start/Stop Simulation (button in Frame)
Start without Animation (in Frame)
Statistics Wizard
Type Info (in Frame)