Create Sensor (in Frame)
To create a new sensor on the length-oriented object, click at the rough position at which you would like to insert the sensor with the right mouse button and select this command. Enter the precise position and the remaining data defining to the sensor into the dialog that opens.
To open the sensor at a later point in time, click it with the right mouse button and select Open Sensor.
To delete the sensor at a later point in time, click it with the right mouse button and select Delete Sensor. To delete the sensor in 3D, press the Del key on your keyboard.
Instead, you can also click Sensors in the dialog of the object.
Related Topics
Context Menu of the Selected Object in the FrameArrange Icons (Frame)
Calculate Angles
Controls (in Frame)
Create Tugger Train
Delete Sensor
Disable
Down One Level
Edit Display Panel (in Frame)
Edit Dialog (in Frame)
Edit Icons (in Frame)
Edit User-defined Attributes (in Frame)
Enable (in Frame)
Next Icon (in Frame)
Open (in Frame)
Open Class (in Frame)
Open Comment Window
Open Debugger
Open External Connections List
Open Origin (in Frame)
Open Sensor
Open Values Table
Open Without Control
Previous Icon (in Frame)
Rename (in Frame)
Reorder Successors
Reset Simulation (in Frame)
Run (Method)
Show (in Frame)
Show Assigned Objects (on context menu)
Show Attributes and Methods (in Frame)
Show Dialog (in Frame)
Show Exported Services
Show External Connected Objects
Show Statistics Report (in Frame)
Show Structure (in Frame)
Start/Stop Simulation (button in Frame)
Start without Animation (in Frame)
Statistics Wizard
Type Info (in Frame)