Blocked
A material flow resource is blocked, when:
It is fully occupied.
It is not Paused.
It is not Failed.
It is not Stopped.
All of its stations are not Working.
All of its stations are not Setting-Up.
Note:The read-only attribute ResBlocked returns the state blocked of the resource.
The LED of a blocked station is yellow .
The Statistics Report shows the Blocked Time below Resource Statistics of Stationary Resources
SimTalk
Related Topics
Related Topics
Resource Statistics (material flow objects)Working (general description)
Setting-Up (general description)
Waiting (described)
Powering up/down
Failed (resource statistics)
Stopped (material flow object, state)
Paused (material flow objects)
Unplanned (general description)
Empty
Relative Occupation