Working (general description)
The definition of working depends on the object that processes the MU:
The object | Is working when |
---|---|
Station, ParallelStation, AssemblyStation, DismantleStation, PlaceBuffer, Drain | it processes at least one MU |
at least one MU is moving on it | |
its current speed is not 0. It can also be working when it is moving and when it does not transport any part | |
it has a speed or when it is rotating, no matter if it moves a part or not | |
has a speed or when the moving time is running | |
it is rotating, no matter if it moves a part or not or when it picks a part up or deposits a part | |
— | |
— The processing time is identical with the sorting time, i.e., it is always zero. This means the sorting takes place instantaneously. Even though the processing time is zero, each sorting action counts as a processing procedure. | |
material flows | |
when materials are mixed | |
when the is transformed into an MU | |
when the MU is transformed into a material |
The read-only attribute ResWorking, returns the state working of the resource.
The LED of a station that is processing parts is green .
The Statistics Report shows the Working Time below Resource Statistics of Stationary Resources.
SimTalk
Related Topics