BookPos
Syntax
<MU-Path>.BookPos → real |
The read-only attribute BookPos returns the position of the booking point of the MU according to the current ConveyingDirection on the object, designated by <MU-Path>, on which it is located. You can only get the attribute, you cannot set it.
Return Value
The return value has the data type real.
Note:
The attribute only returns the position, when the active MU is located on a length-oriented object! For point-oriented objects the return value always is 0.
Example
print@.BookPos |