BlockingStarttime
Syntax
<MU-Path>.BlockingStarttime → time |
The read-only attribute BlockingStarttime returns the point in time at which the blocking time of the MU designated by <MU-Path> started.
The BlockingStarttime also applies to the Sorter and to the FlowControl, i.e., to the objects that can appear in a blocking list.
Return Value
The attribute returns a value of data type time.
You can also view the remaining processing time in the dialog Show Attributes and Methods of the object.
Example
print .MUs.Part:872564.BlockingStarttime |
Related Topics