Cont (MUs)
Syntax
<MU-Path>.Cont → object |
The read-only attribute Cont returns the MU, which is located on the loading space of the MU designated by <MU-Path>. You can also use Cont to access any location on the loading space by its position in the matrix.
Parameters
The parameter X of data type integer designates the x-position of the MU.
The parameter Y of data type integer designates the y-position of the MU.
Return Value
The return value has the data type object.
Example
@.Cont.move(Station) |
Related Topics
Contents, menu command
Statistics Values, of the Transporter